Amazon Sidewalk Version 2.8.2 - Release Notes (May 4, 2026)#
Amazon Sidewalk is a secure, low-bandwidth, long-range wireless protocol designed to connect smart devices and extend their range beyond standard Wi-Fi or Bluetooth. It enables seamless connectivity for IoT devices in homes and neighborhoods, supporting features like device tracking, smart lighting, and sensor networks.
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Added in 2.8.2#
New WPK mainboard (BRD4002B) support for OOB. Support for Simplicity SDK 2025.12.3.
Added in 2.8.1#
Support for Simplicity SDK 2025.12.2.
Added in 2.8.0#
Support for Simplicity SDK 2025.12.0.
Support for RAIL 3.0.
API Changes#
None.
Bug Fixes#
Fixed in 2.8.1#
DMP BLE app migration fix.
Minor location app fixes.
Fixed in 2.8.0#
DULT related bug fixes.
KG100S Software component fixes.
Chip Enablement#
Added in 2.8.1#
xg29 board support.
Added in 2.8.0#
None.
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
New Features#
None.
Enhancements#
None.
Removed Features#
None.
Deprecated Features#
None.
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
None.
Modified APIs#
None.
Removed APIs#
None.
Deprecated APIs#
None.
Bug Fixes#
Fixed in 2.8.1#
None.
Fixed in 2.8.0#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1512585 | DULT - Handle stopped BLE stack. | None. |
|
| 1528095 | Semtech component not added automatically with KG100S Software component. | None. |
|
| 1563086 | Qualification app freezes after FSK initialization. | None. |
|
| 1468643 | Rework DMP application to fit Simplicity Connect mobile application update to prevent freeze of DMP. | None. |
|
Chip Enablement#
None.
Application Example Changes#
New Examples | Modified Examples | Removed Examples | Deprecated Examples
Added in 2.7.0
New Location Sample Application
New Examples#
| Example Name | Description | Supported Software Variants (if applicable) | Supported Modes | Supported Board(s) | Supported Host Interfaces |
|---|---|---|---|---|---|
| Amazon Sidewalk - SoC Location | The Location sample application leverages the Amazon Sidewalk protocol to provide and demonstrate location services. | Amazon Sidewalk with enabled Location Services | SoC | None | N/A |
Modified Examples#
None.
Removed Examples#
None.
Deprecated Examples#
None.
Known Issues and Limitations#
None.
Impact of Release Changes#
Impact Statements | Migration Guide
Impact Statements#
None.
Migration Guide#
None.
Using This Release#
What's in the Release? | Compatible Software | Installation and Use | Help and Feedback
What's in the Release?#
The Sidewalk MCU SDK v2.8.0 release introduces mainly support for the latest SiSDK 2025.12.0 and stability improvements. RAIL 3.0 support is available with this release.
Compatible Software#
| Software | Compatible Version or Variant |
|---|---|
| Simplicity SDK | Simplicity SDK 2025.12.3 |
| Amazon Sidewalk SDK | 1.19.1 |
Installation and Use#
To run your first demo, see our Getting Started Guides.
To kick start your development, see our Developer's Guide.
For information about Secure Vault Integration, see Secure Vault.
To review Security and Software Advisory notifications and manage your notification preferences:
Log in with your account credentials.
Click your profile icon in the upper-right corner of the page.
Select Notifications from the dropdown menu.
In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications
To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.
For recommended settings, configurations, and usage guidelines, see our Developer's Guide.
To learn more about the software in this release, dive into our online documentation.
Help and Feedback#
Contact Silicon Labs Support.
To use our Ask AI tool to get answers, see the search field at the top of this page.
Note: Ask AI is experimental.
Get help from our developer community.
Feature Matrix#
Unsupported Features#
Sidewalk Bulk Data Transfer (SBDT): Sidewalk BLE integrated OTA mechanism is available in our Sidewalk alpha repository, as it is not publicly accessible on the Amazon AWS side.
Switched Multiprotocol (SMP): Sidewalk, BLE, Z-Wave SMP PoC are available in our alpha repository.
SDK Release and Maintenance Policy#
See our SDK Release and Maintenance Policy.