RAIL Library Version 3.0.4 - Release Notes (Nov 4, 2026)#
Silicon Labs RAIL (Radio Abstraction Interface Layer) provides an intuitive and easily-customizable radio interface that is designed to support proprietary or standards-based wireless protocols.
Click here for earlier releases.
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Added in 3.0.4#
None.
Added in 3.0.3#
None.
Added in 3.0.2#
None.
Added in 3.0.1#
None.
Added in 3.0.0#
Added RAIL support for MGM270SC22SNA and BGM270SC22SNA modules.
API Changes#
Changed in 3.0.4#
None.
Changed in 3.0.3#
None.
Changed in 3.0.2#
None.
Changed in 3.0.1#
None.
Changed in 3.0.0#
RAIL APIs have been updated to 3.0, which brings several improvements in the areas of RAIL initialization, RX FIFOs and companion Packet Queues, TX FIFOs, and TX power management. Refer RAIL 3.0 Migration guide for more details.
Bug Fixes#
Fixed in 3.0.4#
Targeted quality improvements and bug fixes.
Fixed in 3.0.3#
Targeted quality improvements and bug fixes.
Fixed in 3.0.2#
Targeted quality improvements and bug fixes.
Fixed in 3.0.1#
Targeted quality improvements and bug fixes.
Fixed in 3.0.0#
Targeted quality improvements and bug fixes.
Chip Enablement#
None.
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
New Features#
Added in 3.0.4#
None.
Added in 3.0.3#
None.
Added in 3.0.2#
None.
Added in 3.0.1#
None.
Added in 3.0.0#
Added RAIL support for MGM270SC22SNA and BGM270SC22SNA modules.
Updated the entries in the power setting table to include PA submode for the SiXG301 part.
The RAIL Utility, RSSI Internal component can now store and retrieve the chip RSSI offset from NVM3 persistent storage.
In RAIL 3.0,
sl_rail_set_tx_fifo()now supports configuring a transmit FIFO whose size is not a power-of-2. Such a FIFO is usable only in TXSL_RAIL_DATA_METHOD_PACKET_MODEand not TXSL_RAIL_DATA_METHOD_FIFO_MODE. In RAIL 2.x,RAIL_SetTxFifo()does not support this; its functionality remains unchanged.Added a callback
sl_railcb_convert_ddbm_to_power_setting_entrywhich provides register settings for requested deci-dBm power. This replaces the now-deprecated RAIL 2.xRAIL_ConvertDbmToRaw()API.Added
sl_rail_ieee802154_config_signal_identifier()andsl_rail_ble_config_signal_identifier()APIs to the configure signal identifier for IEEE 802.15.4 and BLE protocols, respectively.Provided ability to adjust the RAIL default high and low RF Sense sensitivity thresholds.
Added RAIL Utility, IEEE802.15.4 Fast Channel Switching and RAIL Utility, IEEE802.15.4 Duty Cycling components to be used with RAIL Utility, IEEE802.15.4 PHY Configuration on the SiXG301 part.
Added
sl_rail_abort_rx_incoming_packet()allowing an application to abort an incoming packet during its reception.Added a new API
sl_rail_ble_config_channels()to load any BLE channel configuration.Added a new RAIL library variation that uses secure peripheral addresses.
Enhancements#
Added in 3.0.4#
None.
Added in 3.0.3#
None.
Added in 3.0.2#
None.
Added in 3.0.1#
None.
Added in 3.0.0#
The
RAIL_ConfigData()API has been split into two RAIL 3 functions,sl_rail_config_rx_data()andsl_rail_config_tx_data(), to allow independent control of Rx and Tx data configuration, respectively.Renamed
ver.htorail_version.handver_def.htorail_version_def.h.Updated the railtest and new
sl_rail_testapps to usememory_manager (sl_malloc/free())component rather thansilabs_core_memory_manager. Due to this change, code size increases and interrupt latency may also increase a negligible amount.
Removed Features#
None.
Deprecated Features#
Deprecated in 3.0.3#
None.
Deprecated in 3.0.3#
None.
Deprecated in 3.0.2#
None.
Deprecated in 3.0.1#
None.
Deprecated in 3.0.0#
RAIL 2.x APIs are now deprecated in this release. Refer to Deprecated APIs for more details.
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
Added in 3.0.3#
None.
Added in 3.0.3#
None.
Added in 3.0.2#
None.
Added in 3.0.1#
None.
Added in 3.0.0#
For all the new APIs that are added in this release, see New APIs.
Modified APIs#
Modified in 3.0.3#
None.
Modified in 3.0.3#
None.
Modified in 3.0.2#
None.
Modified in 3.0.1#
None.
Modified in 3.0.0#
For all the new APIs that are modified in this release, see Modified APIs.
Removed APIs#
None.
Deprecated APIs#
Deprecated in 3.0.3#
None.
Deprecated in 3.0.3#
None.
Deprecated in 3.0.2#
None.
Deprecated in 3.0.1#
None.
Deprecated in 3.0.0#
Complete list of the deprecated APIs can be found here.
Bug Fixes#
Fixed in 3.0.4#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1683434 | Fixed a Z-Wave issue with sl_rail_zwave_perform_ir_cal() which was mistakenly attempting to calibrate a nonexistent beam channel, returning an error. Also eliminated issuing superfluous SL_RAIL_EVENT_CAL_NEEDED events during sl_rail_zwave_perform_ir_cal() operation as well as with sl_rail_zwave_init() prior to establishing a region. | None |
|
| 1784015 | Fixed an issue on the EFR32xG24 where the IEEE 802.15.4 2.4 GHz antenna diversity PHY could lose about 6 dB of RX sensitivity when configured for a fixed antenna (ANTENNA0/ANTENNA1) instead of AUTO. Also updated AGC settings on the IEEE 802.15.4 OQPSK production and diversity production PHYs to reduce gain recovery time for improved Wi-Fi coexistence. | None |
|
| 1852374 | Fixed an issue on the SixG301 part where, with Fast Channel Switching enabled, the radio would not receive valid packets when the die temperature exceeded approximately 90 deg C. | None |
|
Fixed in 3.0.3#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1627182 | Fixed a race condition that could cause a channel-hopping packet received soon after a transmit to report an incorrect sl_rail_rx_packet_details_t::channel_hopping_channel_index (while sl_rail_rx_packet_details_t::channel is correct). | None |
|
| 1629254 | Fixed an issue on the EFR32xG25 part, where writing to an empty TX FIFO during a transmit could cause data corruption (first added byte sent twice), with a greater chance of occurring with OFDM or SUN OQPSK PHYs. | None |
|
Fixed in 3.0.2#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1563479 | Optimized some recent changes that regressed RX-to-RX-with-channel-change timing vs. Simplicity SDK 2025.6.0 release. | None |
|
| 1565641 | Eliminated a race condition on the SiXG301 part where Fast Channel Switching could impact CSMA transmits. | 00335449 |
|
| 1572298 | Fixed an issue where calling sl_rail_ieee802154_config_gb863_mhz_radio() or sl_rail_ieee802154_config_gb915_mhz_radio() no longer implicitly enabled SL_RAIL_IEEE802154_G_OPTION_GB868. It had to be enabled by calling sl_rail_ieee802154_config_g_options() later. | None |
|
| 1576544 | Fixed an issue on the SiXG301 part where SL_RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND was not generated for the IEEE 802.15.4 stack when Fast Channel Switching is enabled. | 00335936 |
|
| 1579915 | Fixed an issue on the SIxG301 part, where the radio would not receive packets when switching protocols in a Dynamic Multiprotocol applications. | None |
|
| 1581066 | Fixed an issue where changing radio configurations while frame detection is disabled due to RX overflow or SL_RAIL_RX_OPTION_DISABLE_FRAME_DETECTION would silently re-enable frame detection. | None |
|
Fixed in 3.0.1#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1586903 | Fixed an issue where the power-restriction limits were incorrect for the MGM270SC22SNA and BGM270SC22SNA modules. | None |
|
Fixed in 3.0.0#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 233012 | Fixed an issue with coexistence and CSMA transmits where Request could be improperly de-asserted on CCAs (clear channel assessments) with zero backoff preventing that CCA from seeing a clear channel to permit transmit. | None | All chips |
| 1309208 | Fixed a minor issue on the EFR32xG21 where the TX-to-RX turnaround timing could be slightly longer than specified. | None | EFR32xG21 |
| 1434510 | Fixed an issue on the SiXG301 where a ramp time of more than 1000us would trigger an assert; the maximum ramp time is now limited to 1000us. | None | SiXG301 |
| 1470529 | Fixed an issue with coexistence where some CSMA transmit CCAs (clear channel assessments) provided no advance warning to assert Request and be Granted in time for the CCA to see a clear channel and permit transmit. | None | All chips |
| 1474636 | Fixed an issue where a very small packet (1-2 bytes) with a very fast PHY (>= 2mbps) can be improperly dropped or trigger SL_RAIL_ASSERT_FAILED_UNEXPECTED_STATE_RX_FIFO. On EFR32xG2x platforms it is still possible such packets will not properly respect an RX transition to TX, e.g., for autoAck. | None | EFR32xG2x |
| 1478786 | Fixed an issue where the BGM260PB32VNA module failed to build due to incorrect signatures. | None | BGM260PB32VNA |
| 1490308 | Fixed an issue where RAIL_ConfigData() or sl_rail_config_rx_data() would mistakenly return success if the RX buffer write offset is not properly aligned for the requested RX source to function properly. Also clarified documentation around these function's alignment requirements. | None | All chips |
| 1496415 | Expanded the fix for issue 1470529 to cover fixed and 0-backoff CSMA/LBT operations and issue SL_RAIL_EVENT_TX_CCA_ACTIVATED when LBT is actually started and not sooner. | None | All chips |
| 1499282 | Fixed an issue where RAIL could hang in its idle code path when switching from the IEEE 802.15.4 High Data Rate (HDR) PHY to the normal 802.15.4 PHY. | None |
|
| 1503687 | Fixed sl_rail_get_rx_time_preamble_start() and sl_rail_get_rx_time_sync_word_end() on the EFR32xG25 part for OFDM and OQPSK modulations. | None | EFR32xG25 |
| 1514841 | RAIL libraries are now built to avoid instructions or optimizations that might cause an unaligned access trap, should one be enabled on Cortex M platforms. | None | Cortex M platforms |
| 1518333 | Fixed an issue on the EFR32xG25 where the radio could not receive any frame after the radio is idled while OFDM frame detection is ongoing. | None | EFR32xG25 |
| 1523880 | Fixed an issue on the EFE32xG25, where the radio could get a sync detect event without a completion event when sl_rail_idle() was called just before the frame detection. | None | EFE32xG25 |
| 1524998 | Fixed an issue with Concurrent RX Channel Switching on EFR32xG2x platforms which could cause transmit to lock up and never complete. | None | EFR32xG2x |
| 1530983 | Fixed an issue with BLE on EFR32xG27 and EFR32xG29 where RX overflow could render the protocol deaf. | None |
|
| 1531433 | In RAIL 3.0, Modules are not yet supported by the new sl_rail_util_pa plugin. This is fixed by adding a sl_rail_util_compatible_pa component that will pull in the correct PA plugin depending on whether building for modules or SoC's. | None | All chips |
| 1542463 | Fixed a race condition on the EFR32xG25 with OFDM-FSK concurrent PHYs where idling the radio during a SL_RAIL_EVENT_RX_PREAMBLE_LOST event would not idle the software modem. | None | EFR32xG25 |
| 1557444 | Fixed a Channel Sounding issue on the EFR32xG24 platform where the device would transmit a tone longer than expected on Phase-Based Ranging steps. | None | EFR32xG24 |
Chip Enablement#
Added support for the xG2D device family.
Application Example Changes#
New Examples | Modified Examples | Removed Examples | Deprecated Examples
New Examples#
None.
Modified Examples#
None.
Removed Examples#
None.
Deprecated Examples#
None.
Known Issues and Limitations#
| ID | Issue or Limitation Description | GitHub / Salesforce Reference (if any) | Workaround (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|---|
| 1581310 | There is a known issue on the EFR32xG24 part with a BLE sleepy app using AoX antenna switching where a transmit completion event isn't generated for a packet that contains AoA connectionless CTE. This locks up BLE. | The current workaround is to configure the app not to sleep lower than EM1. | None |
|
| 1458845 | When running Channel Sounding RTT with a non-BG24 CS device, RTT has an error of +/- 12.5 ns depending on CS role. Precision is not affected. BG24 to BG24 RTT is not affected. | None | None |
|
Impact of Release Changes#
Impact Statements | Migration Guide
Impact Statements#
None.
Migration Guide#
RAIL APIs have been updated to 3.0 bringing several improvements in the areas of RAIL initialization, RX FIFOs and companion Packet Queues, TX FIFOs, and TX power management. Refer to RAIL 3.0 Migration guide for more details.
Using This Release#
What's in the Release? | Compatible Software | Installation and Use | Help and Feedback
What's in the Release?#
RAIL Library packages and plugins.
Compatible Software#
None.
Installation and Use#
For information about Secure Vault Integration, see Secure Vault.
To review Security and Software Advisory notifications and manage your notification preferences:
Log in with your account credentials.
Click your profile icon in the upper-right corner of the page.
Select Notifications from the dropdown menu.
In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications
To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.
Help and Feedback#
Contact Silicon Labs Support.
To use our Ask AI tool to get answers, see the search field at the top of this page.
Note: Ask AI is experimental.
Get help from our developer community.
Unsupported Features#
None.
SDK Release and Maintenance Policy#
See our SDK Release and Maintenance Policy.