Edit

Simplicity Connect Mobile App Version 3.2.2 - Release Notes (May 4, 2026)#

These release notes cover Simplicity Connect for Android and iOS.

Click here for earlier releases.

Simplicity Connect App includes simple demos to teach you how to get started with Simplicity Connect and all Silicon Labs development tools.

Release Summary#

Key Features | API Changes | Bug Fixes | Chip Enablement

Key Features#

Added in 3.2.2#

None.

Added in 3.2.1#

None.

Added in 3.2.0#

  • Added the Battery-less Asset Tagging Demo.

  • Added the Channel Sounding Demo (Android).

  • Added the Smart lock Demo.

  • Added the Matter EVSE Demo.

API Changes#

None.

Bug Fixes#

Fixed in 3.2.2#

  • Fixed the mobile app attempting to connect after the IOP test had completed.

  • Fixed missing cleanup notes popup during the IOP test.

  • Fixed device filtering to correctly support RSSI and Complete Local Name fields in advertisement data.

  • Improved IOP test UI text for better clarity and usability.

  • Fixed incorrect failure status being reported before the IOP test completed.

Fixed in 3.2.1#

  • Support for WPA3 Transition Mode Security.

  • IOP Tests OTA Update Failures During Reboot.

Fixed in 3.2.0#

  • Fixed Simplicity Connect app v3.1.1 RSSI Graph freeze after 3 seconds.

  • Fixed missing button at the write new value.

Chip Enablement#

None.

Key Features#

New Features | Enhancements | Removed Features | Deprecated Features

Note: See Feature Matrix for a list of any applicable APIs, examples, software variants, modes, hardware, and host interfaces applicable for each feature.

New Features#

Added in 3.2.2#

None.

Added in 3.2.1#

None.

Added in 3.2.0#

  • Battery-less Asset Tagging Demo.

  • Channel Sounding Demo (Android).

  • Smart lock Demo.

  • Matter EVSE Demo.

Enhancements#

Added in 3.2.2#

None.

Added in 3.2.1#

None.

Added in 3.2.0#

  • Matter EVSE Demo.

  • Connected Device (DMP) Demo.

Removed Features#

None.

Deprecated Features#

None.

API Changes#

None.

Bug Fixes#

Fixed in 3.2.2#

ID Issue Description GitHub / Salesforce Reference Affected Software Variants, Hardware, Modes, Host Interfaces
1618025 Simplicity Connect mobile app attempts to connect after the IOP test has completed on Android. None. None.
1617893 Cleanup notes popup is not displayed during the IOP test on Android. None. None.
1617902 Device filtering by RSSI and Complete Local Name in advertisement data is not functioning correctly on iOS and Android. None. None.
1617901 IOP test UI text is unclear and lacks meaningful descriptions on iOS and Android. None. None.
1617894 IOP test is marked as failed before the test is completed on iOS mobile. None. None.

Fixed in 3.2.1#

ID Issue Description GitHub / Salesforce Reference Affected Software Variants, Hardware, Modes, Host Interfaces
1579539 Support for WPA3 Transition Mode Security. None. None.
1582664 IOP Tests OTA Update Failures During Reboot. None. None.

Fixed in 3.2.0#

ID Issue Description GitHub / Salesforce Reference Affected Software Variants, Hardware, Modes, Host Interfaces
1524422 Simplicity Connect app v3.1.1 RSSI Graph froze after 3 seconds. None. None.
1525534 Missing button at the write new value. None. None.
1412458 Bluetooth connection interval has been modified by the Simplicity Connect v3.0.1. None. None.

Chip Enablement#

None.

Application Example Changes#

New Examples | Modified Examples | Removed Examples | Deprecated Examples

New Examples#

Added in 3.2.2#

None.

Added in 3.2.1#

None.

Added in 3.2.0#

Example Name Description Supported Software Variants Supported Modes Supported OPNs / Boards / OPN Combinations Supported Host Interfaces

Smart Lock

User Guide
The Smart Lock demo showcases how to control a smart lock using Bluetooth Low Energy (BLE) and Amazon Web Services (AWS). The SiWx91x Development Kit (Dev Kit) functions as the smart lock device. Users can control the smart lock device locally via BLE or remotely via AWS. SoC SiWx917 UART UART

Battery-less Asset Tagging Demo

User Guide
This demo showcases a battery-less asset tracking system based on the principle of energy harvesting. N/A BRD2710A and BRD8201A UART UART

Channel Sounding

User Guide
Measure distance using Bluetooth channel sounding between a mobile device and an EFR32xG24. N/A BRD2606A UART UART

Matter EVSE

User Guide
The user can commission, get status, change mode of charging and control the EVSE Matter device. N/A SiWx917 UART UART

Modified Examples#

Added in 3.2.2#

None.

Added in 3.2.1#

None.

Added in 3.2.0#

Example Name Changes Supported Software Variants Supported Modes Supported OPNs / Boards / OPN Combinations Supported Host Interfaces

Connected Device

User Guide

Users can control a Dynamic Multiprotocol application of a connected device. N/A SoC
  • EFR32xG24 (Thread)
  • SiWx917 (Wi-Fi)
N/A

Removed Examples#

None.

Deprecated Examples#

None.

Known Issues and Limitations#

None.

Impact of Release Changes#

None.

Using This Release#

What's in the Release?#

Added in 3.2.2#

None.

Added in 3.2.1#

None.

Added in 3.2.0#

  • Battery-less Asset Tagging.

  • Channel Sounding Demo (Android).

  • Smart lock Demo.

  • Matter EVSE Demo.

  • Connected Device (DMP) Demo.

Compatible Software#

Software

Compatible version or variant

Simplicity Connect App

3.2.2

WiSeConnect

4.0.2

Silicon Labs Matter

2.8.1 - 1.5

Installation and Use#

To upgrade your application with this release, download from Google Play Store or Apple App Store.

Source code can be found on GitHub iOS Android.

To run your first demo, see our Getting Started Guides.

To kick start your development, see our Developer's Guide.

For information about Secure Vault Integration, see Secure Vault.

To review Security and Software Advisory notifications and manage your notification preferences:

  1. Go to https://community.silabs.com/.

  2. Log in with your account credentials.

  3. Click your profile icon in the upper-right corner of the page.

  4. Select Notifications from the dropdown menu.

  5. In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications

  6. To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.

  • To learn more about the software in this release, dive into our online documentation.

Help and Feedback#

Feature Matrix#

Supported Features#

Feature Name Description Quality Related API Name(S) Supported Software Variant(s) Supported Mode(s) Supported OPN(s) / Board(s) / OPN Combination(s) Supported Host Interface(s) Application Examples
Health Thermometer Reading data from Health Thermometer Service Sample Demo N/A Secure connectivity firmware for BLE SoC EFR32xG24 N/A Bluetooth - SoC Thermometer example from Simplicity Studio
Connected Device Control application of connected light and switches Sample Demo N/A Secure connectivity firmware for BLE SoC EFR32xG24 N/A rail_soc_light & rail_soc_switch example from Simplicity Studio
Blinky Control LED and Receive button press Sample Demo N/A Secure connectivity firmware for BLE SoC EFR32xG24 N/A Bluetooth - SoC Blinky  example from Simplicity Studio
Range Test Evaluate the link budget and range of EFR32 Sample Demo N/A Secure connectivity firmware for BLE SoC EFR32xG24 N/A RAIL - SoC Range Test example from Simplicity Studio
BLE Throughput Measure the TP between mobile device and EFR32 Sample Demo N/A Secure connectivity firmware for BLE SoC EFR32xG24 N/A Bluetooth - SoC Throughput example from Simplicity Studio
Motion Control a 3D render of Dev Kit Sample Demo N/A Secure connectivity firmware for BLE SoC EFR32xG24 N/A bt_soc_thunderboard example from Simplicity Studio
Environment Read and display the data from the Dev Kit Sample Demo N/A Secure connectivity firmware for BLE SoC EFR32xG24 N/A bt_soc_thunderboard example from Simplicity Studio
Wi-Fi Commissioning Wi-Fi Commissioning over BLE Sample Demo N/A Standard connectivity firmware for Wi-Fi SoC SiWx917 N/A Out of Box Demo (SoC) example from Simplicity Studio
ESL Add/commission the ESL tag by scanning QR Code Sample Demo N/A Secure connectivity firmware for BLE SoC and NCP EFR32xG22 (SoC), EFR32BG22 (NCP) UART Bluetooth - NCP ESL Access Point &  Bluetooth ESL tag example from Simplicity Studio
Matter Add/commission the Matter tags by scanning QR Code Sample Demo N/A Secure connectivity firmware for BLE and Standard connectivity firmware for Wi-Fi SoC EFR32xG24 (Thread), SiWx917 ( Wi-Fi) UART Matter - SoC Lighting over Wi-Fi/THREAD from Simplicity Studio
Wi-Fi OTA Control OTA FW update over Wi-Fi Sample Demo N/A Standard connectivity firmware for Wi-Fi SoC SiWx917 UART Wi-Fi - M4 Firmware Update via TCP example from Simplicity Studio
Wi-Fi Sensor Read and display the sensor data from the dev Kit Sample Demo N/A Standard connectivity firmware for Wi-Fi SoC SiWx917 UART Wi-Fi - SiWx917 Dev Kit (BRD2605A) example from Simplicity Studio
Wi-Fi Throughput Measure Wi-Fi TP between mobile device and SiWx917 Sample Demo N/A Standard connectivity firmware for Wi-Fi SoC SiWx917 UART Wi-Fi - Throughput (SoC) example from Simplicity Studio
Wi-Fi Provisioning Wi-Fi Provisioning over Wi-Fi Sample Demo N/A Standard connectivity firmware for Wi-Fi SoC SiWx917 UART Wi-Fi - Provisioning via Access Point (SoC) example from Simplicity Studio
Amazon AWS IoT Cloud Add/commission/read and control device over AWS IoT Sample Demo N/A Standard connectivity firmware for Wi-Fi SoC SiWx917 UART Wi-Fi Coex - Wi-Fi Client BLE Provisioning with AWS (SoC) example from Simplicity Studio
Smart Lock Add/commission smart lock and read/control it over bluetooth and AWS IoT Cloud. Sample Demo N/A Standard connectivity firmware for Wi-Fi SoC SiWx917 UART Smart Lock example from Simplicity Studio
Battery-less Asset Tagging This will show energy harvesting by devices. Sample Demo N/A Standard connectivity firmware for Wi-Fi SoC BRD2710A and BRD8201A UART Bluetooth - SoC Energy Harvesting Sensor example from Simplicity Studio
Channel Sounding Demo (Android) This will show energy harvesting by devices. Sample Demo N/A Standard connectivity firmware for BLE SoC BRD2606A UART Bluetooth - SoC Energy Harvesting Sensor example from Simplicity Studio

Unsupported Features#

None.

SDK Release and Maintenance Policy#

See here for our SDK release and maintenance policy.