Simplicity SDK Platform - CPC Version 4.7.2 (September 24, 2025) - Release Notes#

Simplicity SDK Platform Version 5.2.2

Simplicity SDK Version 2025.6.2

The Co-Processor Communication (CPC) framework enables secure and efficient data exchange between two processors over a shared serial link, acting as a multiplexer to support multiple applications simultaneously. Designed with a Linux host (CPC daemon) as the primary device and an EFR(M) device as the secondary, CPC ensures reliable, in-order, error-free communication over encrypted UART or SPI connections.

Release Summary#

Key Features | API Changes | Bug Fixes | Chip Enablement

Key Features#

Added in 4.7.2#

  • Added option in cpcd to disable Multicast; applications attempting to open a Multicast endpoint will now fail as expected.

  • Added support in cpcd for higher speed option on UART.

Added in 4.7.1#

None.

Added in 4.7.0#

  • Added permanent memory allocation initialization for CPC, for Series 3.

  • Improved SPI bitrate configuration to default to 1 MHz when unspecified.

  • Added support for GCC Link Time Optimization (LTO).

API Changes#

Added in 4.7.2#

None.

Added in 4.7.1#

None.

Added in 4.7.0#

Introduced sl_cpc_init_permanent_allocations API for permanent memory allocation initialization; sl_cpc_init() continues to handle this for Series 2.

Bug Fixes#

Fixed in 4.7.2#

Fixed CPC Secondary to allow a minimum of 3 RX buffers when using the UART driver without HWFC.

Fixed in 4.7.1#

None.

Fixed in 4.7.0#

  • Resolved race condition in UART code causing buffer errors.

  • Improved SPI bitrate configuration to make it optional; CPCd.

  • Corrected nonce overflow detection logic in CPC protocol; Protocol bump required.

  • Fixed link time warnings in GCC LTO compilation for CPC sample apps.

  • Addressed xmodem bootloader (UART) detection causing CPCd hang.

  • Fixed SPI driver PRS signal initialization; incorrect define was used but had no effect on existing devices.

Chip Enablement#

None.

Key Features#

New Features | Enhancements | Removed Features | Deprecated Features

New Features#

Added in 4.7.2#

None.

Added in 4.7.1#

None.

Added in 4.7.0#

  • Added permanent memory allocation initialization for CPC in preparation for Series 3. sl_cpc_init_permanent_allocations; sl_cpc_init() continues to handle this for Series 2.

  • Added support for GCC Link Time Optimization (LTO).

Enhancements#

Added in 4.7.2#

  • Added option in cpcd to disable Multicast; applications attempting to open a Multicast endpoint will now fail as expected.

  • Added support in cpcd for higher speed option on UART.

Added in 4.7.1#

  • Improved SPI driver compatibility for Series 2 and 3 devices.

  • Added preprocessor validation for UART RX buffer size without hardware flow control.

Added in 4.7.0#

None.

Removed Features#

None.

Deprecated Features#

None.

API Changes#

New APIs | Modified APIs | Removed APIs | Deprecated APIs

New APIs#

Added in 4.7.2#

None.

Added in 4.7.1#

None.

Added in 4.7.0#

New API Signature

Deprecated API replaced by this (if any)

sl_status_t sl_cpc_init_permanent_allocations(void)

None

Modified APIs#

None.

Removed APIs#

None.

Deprecated APIs#

None.

Bug Fixes#

Fixed in 4.7.2#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1487613 Fixed CPC Secondary to allow a minimum of 3 RX buffers when using the UART driver without HWFC. None All

Fixed in 4.7.1#

None.

Fixed in 4.7.0#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1430454 Resolved race condition in UART code causing buffer errors. None All
1411410 Improved SPI bitrate configuration to make it optional. None All
1410876 Corrected nonce overflow detection logic in CPC protocol. None All
1375701 Fixed link time warnings in GCC LTO compilation for CPC sample apps. None All
1281660 Addressed xmodem bootloader detection causing CPCd hang. None All

Chip Enablement#

None.

Application Example Changes#

New Examples#

None.

Modified Examples#

None.

Removed Examples#

None.

Deprecated Examples#

None.

Known Issues and Limitations#

None.