Simplicity SDK Platform - CPC Version 4.9.1 - Release Notes (Jul 29, 2026)#
Simplicity SDK Platform Version 6.1.1
The Co-Processor Communication (CPC) framework enables secure and efficient data exchange between two processors over a shared serial link, acting as a multiplexer to support multiple applications simultaneously. Designed with a Linux host (CPC daemon) as the primary device and an EFR(M) device as the secondary, CPC ensures reliable, in-order, error-free communication over encrypted UART or SPI connections.
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Added LLVM compiler support for CPC applications.
API Changes#
Added in 4.9.1#
Added a CPC service endpoint for the Matter stack,
SL_CPC_ENDPOINT_MATTER(18). For Silicon Labs internal use only.
Bug Fixes#
Fixed in 4.9.0#
Fixed a threading issue where a CPC endpoint opened in one thread could report an inconsistent state after being closed from another thread.
Fixed compile errors that prevented Secondary SPI projects from building after switching from the UART recommended interface to the SPI recommended interface.
Chip Enablement#
None.
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
New Features#
Added LLVM compiler support for CPC applications.
Enhancements#
None.
Removed Features#
None.
Deprecated Features#
None.
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
None.
Modified APIs#
Added in 4.9.1#
Added a CPC service endpoint for the Matter stack,
SL_CPC_ENDPOINT_MATTER(18). For Silicon Labs internal use only.
Removed APIs#
None.
Deprecated APIs#
None.
Bug Fixes#
Fixed in 4.9.0#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| Services | |||
| 1568519 | cpc: Fixed a threading issue where a CPC endpoint opened in one thread could appear in an inconsistent state to the opening thread when closed from another thread. | None | Software: CPC Secondary; Mode: Multi-threaded applications |
| Secondary (MCU) | |||
| 1571482 | cpc: Fixed compile errors that prevented Secondary SPI projects from building after switching from the UART recommended interface to the SPI recommended interface. | None | Software: CPC Secondary SPI |
Chip Enablement#
None.
Application Example Changes#
New Examples#
None.
Modified Examples#
None.
Removed Examples#
None.
Deprecated Examples#
None.
Known Issues and Limitations#
None.