Silicon Labs MVP Math Library Version 6.0.0 - Release Notes (Jun 23, 2026)#
Silicon Labs AI/ML Version 3.0.0
Simplicity SDK Version 2026.6.0
MVP Math Library includes Real and Complex Matrix and Vector operations using the Matrix Vector Processor available on EFR32xG24/6/8 and SiWG917. The library is an alternative to CMSIS-DSP for Matrix and Vector math operations.
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
MVP Math Library release notes moved from Platform to AI/ML.
NN kernels moved from MVP Math Library to AI/ML SDK.
Renamed "MVP Math Demo" sample application to "Compute - SoC Math MVP EFR32".
API Changes#
None.
Bug Fixes#
None.
Chip Enablement#
None.
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
Note: See Feature Matrix for a list of any applicable APIs, examples, software variants, modes, hardware, and host interfaces for each feature.
New Features#
None.
Enhancements#
Package relocation: MVP Math Library is now delivered as part of the AI/ML SDK extension instead of the Platform SDK. Release notes are published under AI/ML instead of Platform.
Sample application rename: Renamed "MVP Math Demo" to "Compute - SoC Math MVP EFR32" in Simplicity Studio.
Removed Features#
Removed Feature | Was Deprecated? |
|---|---|
NN kernels (moved to AI/ML SDK) | No |
Neural network kernels previously provided by the MVP Math Library are now part of the AI/ML SDK. Applications that used NN kernels from the MVP Math Library should use the AI/ML SDK components instead.
Deprecated Features#
None.
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
None.
Modified APIs#
None.
Removed APIs#
Removed API / Feature | Was Deprecated? |
|---|---|
NN kernels in MVP Math Library | No |
Deprecated APIs#
None.
Bug Fixes#
None.
Chip Enablements#
None.
Application Example Changes#
New Examples | Modified Examples | Removed Examples | Deprecated Examples
New Examples#
None.
Modified Examples#
Example Name | Changes |
|---|---|
Compute - SoC Math MVP EFR32 | Renamed from "MVP Math Demo". |
Removed Examples#
None.
Deprecated Examples#
None.
Known Issues and Limitations#
None.