You are viewing documentation for version:
PDFSimplicity SDK Version 2026.6.0 - Release Notes (Jun 23, 2026)#
The primary tool for the Silicon Labs IoT software development ecosystem, combining wireless software development kits (SDKs) and platform into a single, integrated package.
Release Announcement#
Beginning with the 2026.6 release, Simplicity SDK releases follow a predictable biannual release model with two release types:
June Long-Term Support (LTS) release: The recommended baseline for production programs. During the 30-month standard maintenance window, an LTS release may receive maintenance patches and is eligible for technical support.
December Interim release: A shorter-maintained release for prototyping, early feature access, and development work that will move to a later LTS release. The December Interim release receives 6 months of standard maintenance and support.
Simplicity SDK releases prior to 2026.6 provide 18 months of maintenance and support.
Gecko SDK 4.5 LTS provides on-going support and maintenance for active Series 0 and 1 devices.
Customers who need to remain on a specific SDK release beyond the standard maintenance window may use Silicon Labs' SDK Extended Maintenance Service to extend maintenance for that release.
Simplicity SDK Packaging and Distribution#
Starting with the 2025.12 release, the Simplicity SDK transitions from GitHub-based monolithic delivery to a modular, Conan-based package model.
To obtain and work with the Simplicity SDK 2025.12, customers must use Silicon Labs Tool (SLT) v1.1.0 or newer, available through:
This update also introduces a new directory structure organized by technology and functional domain, which may affect how SDKs are integrated, consumed, and automated in developer workflows.
Developer Guidance#
CLI development (Headless or CI/CD dev setups)#
Need to update scripts that rely on ‘git clone’ and integrate SLT to manage and automate the SDK delivery.
Any tooling, scripts, or manual workflows that rely on fixed SDK paths may need to be updated accordingly.
GUI development (Simplicity Studio 6)#
Resources#
Note: This Simplicity SDK release will be published on GitHub for reference purposes only, not recommended for development. Development should use the SDK packages delivered via SLT.
Release Summary#
| Release Item |
Version |
Release Date |
Key Features |
Chip Enablement |
Platform |
6.1.0 |
Jun 23, 2026 |
Platform MCU - Debug Logger: Logger support added (evaluation quality).
- Watchdog Manager: Watchdog manager support added (evaluation quality).
- sl_main: Added a new app_init_post_platform application hook in sl_main_second_stage_init, called after sl_platform_init, sl_driver_init, and sl_service_init complete and before sl_stack_init. This hook lets applications run initialization that depends on platform components, drivers, and services but must run before stacks are initialized.
- Linker: Added support for RAM-only execution for provisioning applications (GCC toolchain).
- Startup code: Added an assembly reset handler trampoline so safe code can execute before the C environment is loaded.
Security - Added support for NIST SP 800-108r1 key derivation, enabling PUF-based key derivation on xG27 devices
- Added new fine-grained SLC components for Mbed TLS X509, PK, SSL, and DTLS client/server APIs to reduce code size for specific use cases.
Bootloader - Added support for the BRD4419A evaluation board.
- Updated the default Series 3 bootloader clock configuration to use SoCPLL at 145 MHz sourced from HFRCO.
- Added support for dynamic application image selection in dual-application bootloaders using a flash-based switch mechanism.
Micrium OS
CPC
MVP Math Library |
Platform MCU - Added EFR32BG29/EFR32MG29 OPN and radio board support.
- Added EFR32FG2D and WPK Main Board (BRD4002B) support.
|
RAIL Library |
3.1.0 |
Jun 23, 2026 |
This release includes API updates for:
- Event/config visibility
- AF sensing and multiprotocol timing support
- TX PA interface refresh with migration toward newer power-table APIs
|
None |
RAIL SDK |
3.1.0 |
Jun 23, 2026 |
None |
None |
USB |
1.7.0 |
Jun 23, 2026 |
None |
None |
Wi-Fi 6 + BLE (WiSeConnect) |
4.1.0 |
Jun 23, 2026 |
Wi-Fi
- Multicast / broadcast filtering with IP allowlist and beacon-drop threshold
- WPA3 H2E SE
- BSS Max Idle
- Debug logging v2 (SL_DEBUG_LOG_V2) and Internal Buffer Manager
Network Stack
- Added support to configure the DNS timeout from host.
- Added Embedded MQTT password length support up to 512 bytes.
- Added support for graceful TCP FIN handshake closure.
- Upgraded the lwIP stack from v2.1.2 to v2.2.1.
SiWx91x Bluetooth LE
- Added support for dynamically enabling or disabling BLE.
- Added logging support for BLE.
- Added RC clock support for BLE.
- Added support for BLE stack bypass/offloading.
Multiprotocol
- Support for concurrent two BLE connections with advertising extensions and WLAN TCP TX data transfer in NCP.
- Support for concurrent operation of eight BLE peripheral connections, two BLE central devices, and WLAN MQTT data transfer in NCP mode.
SiWx91x Platform
- Added a Memory Manager Redirect component to redirect libc heap allocations to the CMSIS FreeRTOS heap_4 allocator by using heap wrappers.
- Upgraded GCC to 14.2 and enabled Link Time Optimization (LTO) for GCC-based builds.
- Updated SiWx91x platform code to Support BRD4002B Mainboard with EFR Driver Integration.
|
SoC: BRD4343C (SiW917Y-RB4343C) radio board for refreshed SiWG917Y SoC modules with external 32 kHz LP crystal pins; module OPNs SiWN917Y100LGAXA, SiWN917Y100LGNXA, SiWG917Y110LGNXA, SiWG917Y111MGNXA, SiWG917Y121MGNXA, SiWG917Y110LGAXA, SiWG917Y111MGAXA, SiWG917Y121MGAXA.
NCP: BRD4357C (SiW917Y-RB4357C) radio board for refreshed SiWN917Y NCP modules with external 32 kHz LP crystal pins; module OPNs SiWN917Y100LGAXA, SiWN917Y100LGNXA.
New boards: BRD4343C
New chip components (SiWx917Y / SiWN917Y modules) under components/device/silabs/si91x/mcu/core/chip/component/:
- siwg917y110lgaxa, siwg917y110lgnxa
- siwg917y111mgaxa, siwg917y111mgnxa
- siwg917y121mgnxa, siwg917y121mgaxa
- siwn917y100lgaxa, siwn917y100lgnxa (NCP refresh)
|
OpenThread |
3.1.0 |
Jun 23, 2026 |
- Added Thread 1.4 qualification support for OTBR in NCP mode.
- Continued Thread 1.4 qualification support for SoC and OTBR in RCP mode.
- Added Thread - SoC Empty sample applications.
- Added NAT64 and TREL support for Host / NCP configurations.
- OTBR support on Android 15 with CPC spinel proxy support.
- Standardized Simplicity SDK example app titles and descriptions.
- Silicon Labs standard logger integration.
|
None |
Zigbee |
9.1 |
Jun 23, 2026 |
- Configurable next RX channel for Green Power Device (GPD) bi-directional commissioning.
- Secure inter-PAN message fragmentation with APS link encryption after key establishment.
- Packet handoff post-incoming filter with per-packet link quality (RSSI, LQI, channel).
- Zigbee 4.0 gateway sample application.
- GCC and IAR toolchain upgrades (GCC 14.2.rel1 and IAR 9.70.4).
- Antenna calibration APIs for networking products.
- Configurable route table size in Zigbee Pro Stack Config.
|
None |
Bluetooth LE |
11.1.0 |
Jun 23, 2026 |
Example and Middleware - Added Serial Port Profile middleware through the new spp component and related configuration and GATT service content.
- Added new Bluetooth peer manager and peer security middleware components for central, peripheral, filter, common, and security flows.
Host Stack - New flag `SL_BT_PERIODIC_ADVERTISER_INCLUDE_ADVERTISING_DATA_INFORMATION` in `sl_bt_periodic_advertiser_flags` enables the inclusion of Advertising Data Information (ADI) in transmitted periodic advertising PDUs.
- New command `sl_bt_periodic_advertiser_refresh_data_id` enables refreshing the Advertising Data ID (DID) without the need to provide the same data again.
- New mode `sl_bt_sync_report_non_duplicate` in `sl_bt_sync_reporting_mode_t` enables filtering duplicate periodic advertisements.
- The `bluetooth_feature_linklayer_interface` component provides new commands `sl_bt_linklayer_get_hci_connection_handle` and `sl_bt_linklayer_get_bgapi_connection_handle` for converting between link layer HCI connection handles and the BGAPI host stack connection handles. The application needs to convert between handle types when it uses the linklayer class to access low-level link layer functionality that uses connection handles.
- The bluetooth_feature_connection_analyzer feature can now maintain synchronization to the analyzed connection even if connection parameters or channel map is updated. The LLCP events need to be passed from the Central device to the connection analyzer device by the application. Use the `bluetooth_feature_connection_analyzer_llcp_report` component and the `sl_bt_linklayer_event_info_reporting_enable` command to enable the LLCP reporting on the Central. Pass the corresponding LLCP events from `sl_bt_evt_linklayer_event_info_report` events to the connection analyzer device and use `sl_bt_connection_analyzer_process_llcp_event` to process the event.
- New command `sl_bt_gap_set_privacy_mode_with_rpa_randomization` enables configuring local privacy with separate minimum and maximum RPA rotation intervals. When the interval bounds differ, advertiser and central-side RPAs are refreshed at randomized times within the configured range. Keeping the interval bounds equal preserves deterministic rotation behavior.
- New events `sl_bt_evt_gap_random_address_refresh` and `sl_bt_evt_advertiser_random_address_refresh` notify the application when the scanner/initiator or a stack-managed advertiser starts using a new private address. The related privacy mode commands document these events.
- New command `sl_bt_resolving_list_read_peer_resolvable_address` reads the current peer resolvable private address tracked by the controller for a device in the Resolving List.
- The `bluetooth_feature_cs` component adds Channel Sounding (CS) handover commands and events to the cs BGAPI class. Use the `bluetooth_feature_cs_handover_leader` and `bluetooth_feature_cs_handover_follower` components to enable the corresponding controller-side handover roles. Retrieve CS procedure parameters from the CS Leader, pass them to the CS Follower, and use the handover commands and events to synchronize the Follower to the CS procedure and LE connection and to control scheduled CS procedure execution.
Controller - Added support for ADI in Periodic Advertising and Periodic Advertising with Responses, improving interoperability with devices expecting this capability.
- Added Channel Map Update Indication support for the Periodic Advertising advertiser, enabling Adaptive Frequency Hopping with Periodic Advertising for improved reliability in congested or noisy RF environments.
Multiprotocol CMP + BLE-RCP sample applications (Zigbee NCP + OpenThread RCP + Bluetooth RCP) - Added new Concurrent Multiprotocol (CMP) co-processor sample projects that run Zigbee NCP, OpenThread RCP, and Bluetooth RCP on one EFR device. The Bluetooth side exposes a BLE controller over CPC so a Linux host can use the Silicon Labs RCP with CPCd and a standard Bluetooth stack (i.e. BlueZ). Zigbee and OpenThread host applications use the same CPC multiplexer model as existing NCP / RCP designs.
|
Multiprotocol xG2B: Added Alpha software support for xG2B devices in Multiprotocol. |
Bluetooth Mesh |
11.0.0 |
Jun 23, 2026 |
- GCC and IAR compiler version updates
|
None |
Bluetooth Location Services |
11.0.0 |
Jun 23, 2026 |
Real-Time Locationing Service The RTL Service (`rtl_service`) is a new software component providing a unified API that works in both RTOS and bare-metal environments. - The service automatically adapts: in RTOS mode it runs a dedicated processing task; in bare-metal mode it processes within the application main-loop.
- All API functions can be called from any task or interrupt context. The service handles mutual exclusion internally.
- Submit CS or Ranging Service (RAS) procedure data and receive distance estimates asynchronously through a result callback.
RTL Library Version Function - A function `sl_rtl_get_lib_version()` was added to return the exact library version.
`
Algorithm Mode Enum Renaming The enum `sl_rtl_cs_algo_mode` field names have been renamed as follows: - `SL_RTL_CS_ALGO_MODE_REAL_TIME_BASIC` renamed to `SL_RTL_CS_ALGO_MODE_TRACKING_ACCURACY_OPTIMIZED`
- `SL_RTL_CS_ALGO_MODE_REAL_TIME_FAST` renamed to `SL_RTL_CS_ALGO_MODE_TRACKING_LATENCY_OPTIMIZED
- `SL_RTL_CS_ALGO_MODE_STATIC_HIGH_ACCURACY` renamed to `SL_RTL_CS_ALGO_MODE_STATIONARY`
|
|
Z-Wave |
8.1.0 |
Jun 23, 2026 |
|
None |
Wi-SUN |
2.12.0 |
Jun 23, 2026 |
- Added automatic connection parameter selection based on PAN size, with adaptation as the network grows or shrinks.
- Introduced an optional separate heap component for critical Wi-SUN stack and cryptographic allocations.
- Added Direct Connect client support with scanning, complementing the existing server role.
- Added First Breath mode for expedited upstream application data after a network outage.
- Added Last Gasp mode for a final burst of traffic before power loss.
- Expanded RF test component with dedicated TX and RX modes for production testing.
|
None |
Silicon Labs Matter |
2.9.0-1.5 |
Jun 25, 2026 |
- Quality-tested Matter 1.6 solution for Thread and Wi-Fi.
- Matter + AWS dual-stack support for 917 NCP boards.
|
|
Amazon Sidewalk |
2.9.0 |
Jun 23, 2026 |
- Cloud Light SoC Sample application.
- Supporting new Temperature sensor on WPK board.
- Application tab enablement in Sidewalk Assistant.
- Updated libraries to Amazon Stack 1.19.4.
- Stability improvements.
|
None |
Connect |
4.3.0 |
Jun 23, 2026 |
Transition to Common Manufacturing Tokens instead of Legacy Token handling |
EFR32FG2D |
Machine Learning |
3.0.0 |
Jun 23, 2026 |
- New DX for adding ML Models to new or existing projects.
- New APIs to initialize, execute, and de-initialize ML models.
- Project upgrades require manual effort. See the AI-assisted migration prompt.
- Multiple-Model feature to add and execute multiple ML models in a project.
|
Added support for EFM32 devices. |
Simplicity Connect Mobile App |
3.3.0 |
Jun 23, 2026 |
- Added Simplicity Connect rebranding.
- Added Matter demos for Oven and Range Hood.
- Added example app titles to the app and user guide.
- Added a proximity lock demo via channel sounding on Android.
|
None |
Note: Click here for earlier releases on GitHub.
Looking for older release notes? You can still access previous versions for both Simplicity SDK (prior to 2025.6.0) and Gecko SDK here.