Custom Board Debug Options#

Enabling debug support for a custom board has two stages. First, set up and configure the custom board in Simplicity Studio®. Then configure Visual Studio Code (VS Code) with the debugger settings and launch configurations you need for debug sessions on the target platform.

Configure Debugging for a Custom Board#

The following Silicon Labs debug adapters are supported for programming and debugging custom boards and hardware:

Debug Adapter

Debug Mode

Description

Wireless Starter Kit Mainboard (WSTK BRD4001A)

OUT

Uses the external debug connection for a custom board.

Wireless Pro Kit Mainboard (WPK BRD4002A, OPN: Si-MB4002A)

MINI

Uses the onboard mini-Simplicity connector.

Wireless Pro Kit Mainboard (WPK BRD4002A, OPN: Si-MB4002A)

OUT

Uses the debug connectors on the side of the board.

Simplicity Link Debugger (Si-DBG1015A)

OUT

Connects to the custom board through the mini-Simplicity connector or header pins by using jumper wires.

SEGGER J-Link Debug Probe

-

Connects to the custom board through a compatible debug connector.

Note: For either a WSTK or WPK configured for OUT mode, the recommended connection method is to use a Simplicity Debug Adapter Board (SLSDA001A). Insert the adapter board into the Debug Connector and Simplicity Connector, and then use a 10-pin ribbon cable to connect to the debug connector on the custom board.

Hardware Setup#

The following hardware configuration is used throughout this guide. Connect the custom board to the Wireless Pro Kit Mainboard (BRD4002A/B) using the mini-Simplicity (MINI) connector, and connect the mainboard to the host computer with a USB-C cable.

Hardware Set UpHardware Set Up

Configure the Debug Adapter#

  1. In Simplicity Studio, select DEVICES.

  2. In the Device tree, select the debug adapter you want to use for a custom board.

  3. In the General Information panel, select Change next to Debug Mode to open Simplicity Device Manager (SDM).

    Changing debug mode in the General Information panelChanging debug mode in the General Information panel

  4. In SDM, select the appropriate Debug Mode for the target device, and then apply the configuration.

    Changing debug mode in the General Information panelChanging debug mode in the General Information panel

  5. In the Device tree, under the selected debug adapter, select Detect Target Part to identify the target part on the custom board.

    Look for devices option in the Device treeLook for devices option in the Device tree

  6. For an SiWG917 device, select Check if your target board is based on SiWG917.

    Look for devices dialog for an SiWG917 deviceLook for devices dialog for an SiWG917 device

  7. Select Detect Target Part.

  8. After the target part (for example, EFR32MG24B310F1536IM48) is successfully detected, it appears the custom board debug adapter, as shown in the following figure.

    Custom board in Devices SectionCustom board in Devices Section

    The custom board configuration also appears in the Devices view of the Simplicity Studio for VS Code extension.

    Sld1119 Debug Vs CodeSld1119 Debug Vs Code

Note: To detect a different target device, right-click the detected target in the Device tree and select Configure Device Hardware. This action launches Simplicity Device Manager (SDM). In SDM, click Reset Adapter, and then run Look for Devices again to detect the target device.

Configure Debug Sessions in VS Code#

The VS Code extension automatically retrieves the debug adapter configuration from Simplicity Device Manager, so you typically do not need additional setup to flash and debug a custom board. The debug adapter configured for the custom board appears under Devices in the Simplicity VS Code extension.

If the default settings are not sufficient, use the project-specific Debug Configurator:

  1. Right-click on the project folder.

  2. Select Open Configurators 2.0.

    Open Configurators 2.0 from the project folderOpen Configurators 2.0 from the project folder

  3. Select Debug Configurator.

    The standard debug configuration fields are prefilled. Expand the bottom section of the dialog to view optional fields for the debug session, including configuration options for Real-Time Transfer (RTT) and Serial Wire Output (SWO) terminals.

    Optional RTT and SWO settings in Debug ConfiguratorOptional RTT and SWO settings in Debug Configurator

Common Settings#

  • Break after Reset: Stops code execution after a reset instead of running to main.

  • Run to entry point: Defaults to main, but you can change it for special debugging scenarios.

Enable the RTT Config or SWO Config sections (or both) to apply custom settings for those terminals. The default settings are typically sufficient.