USB Device Core API
Description
USB Device Core API.
Data Structures | |
struct | sl_usbd_device_config_t |
USB DEVICE CONFIGURATION DATA TYPE. | |
struct | sl_usbd_setup_req_t |
USB DEVICE MICROSOFT XTENDED PROPERTIES DATA TYPE. | |
struct | sl_usbd_class_driver_t |
INTERFACE CLASS DRIVER. |
Functions | |
sl_status_t | sl_usbd_core_init (void) |
Initialize the USB device stack. | |
sl_status_t | sl_usbd_core_start_device (void) |
Start the device stack. | |
sl_status_t | sl_usbd_core_stop_device (void) |
Stop the device stack. | |
sl_status_t | sl_usbd_core_get_device_state (sl_usbd_device_state_t *p_dev_state) |
Get the current device state. | |
sl_status_t | sl_usbd_core_get_device_speed (sl_usbd_device_speed_t *p_dev_speed) |
Get device speed. | |
sl_status_t | sl_usbd_core_set_device_self_power (bool self_pwr) |
Set the device's current power source. | |
sl_status_t | sl_usbd_core_get_device_configuration (sl_usbd_device_config_t **p_dev_cfg) |
Set the device's Microsoft vendor code. | |
sl_status_t | sl_usbd_core_get_device_frame_number (uint16_t *p_frame_nbr) |
Get the last frame number from the driver. | |
sl_status_t | sl_usbd_core_add_configuration (uint8_t attrib, uint16_t max_pwr, sl_usbd_device_speed_t spd, const char *p_name, uint8_t *p_cfg_nbr) |
Add a configuration attribute to the device. | |
sl_status_t | sl_usbd_core_add_interface (uint8_t cfg_nbr, sl_usbd_class_driver_t *p_class_drv, void *p_if_class_arg, void *p_if_alt_class_arg, uint8_t class_code, uint8_t class_sub_code, uint8_t class_protocol_code, const char *p_name, uint8_t *p_if_nbr) |
Associate a configuration with its alternative-speed counterpart. | |
sl_status_t | sl_usbd_core_add_alt_interface (uint8_t config_nbr, uint8_t if_nbr, void *p_class_arg, const char *p_name, uint8_t *p_if_alt_nbr) |
Add an alternate setting to a specific interface. | |
sl_status_t | sl_usbd_core_add_interface_group (uint8_t config_nbr, uint8_t class_code, uint8_t class_sub_code, uint8_t class_protocol_code, uint8_t if_start, uint8_t if_cnt, const char *p_name, uint8_t *p_if_grp_num) |
Create an interface group. | |
sl_status_t | sl_usbd_core_get_device_descriptor (uint8_t *p_buf, uint8_t max_len, uint8_t *p_desc_len) |
Get the device descriptor. | |
sl_status_t | sl_usbd_core_get_configuration_descriptor (uint8_t *p_buf, uint16_t max_len, uint8_t config_ix, uint16_t *p_desc_len) |
Get a configuration descriptor. | |
sl_status_t | sl_usbd_core_get_string_descriptor (uint8_t *p_buf, uint8_t max_len, uint8_t str_ix, uint8_t *p_desc_len) |
Get a string descriptor. | |
sl_status_t | sl_usbd_core_add_string (const char *p_str) |
Add string to USB device. | |
sl_status_t | sl_usbd_core_get_string_index (const char *p_str, uint8_t *p_str_ix) |
Get string index corresponding to a given string. | |
sl_status_t | sl_usbd_core_write_08b_to_descriptor_buf (uint8_t val) |
Write an 8-bit value to the descriptor buffer. | |
sl_status_t | sl_usbd_core_write_16b_to_descriptor_buf (uint16_t val) |
Write a 16-bit value in the descriptor buffer. | |
sl_status_t | sl_usbd_core_write_24b_to_descriptor_buf (uint32_t val) |
Write a 24-bit value to the descriptor buffer. | |
sl_status_t | sl_usbd_core_write_32b_to_descriptor_buf (uint32_t val) |
Write a 32-bit value to the descriptor buffer. | |
sl_status_t | sl_usbd_core_write_buf_to_descriptor_buf (const uint8_t *p_buf, uint16_t len) |
Write a buffer into the descriptor buffer. | |
sl_status_t | sl_usbd_core_write_control_sync (void *p_buf, uint32_t buf_len, uint16_t timeout_ms, bool end, uint32_t *p_xfer_len) |
Send data on the Control IN endpoint. | |
sl_status_t | sl_usbd_core_read_control_sync (void *p_buf, uint32_t buf_len, uint16_t timeout_ms, uint32_t *p_xfer_len) |
Receive data on the Control OUT endpoint. | |
sl_status_t | sl_usbd_core_add_bulk_endpoint (uint8_t config_nbr, uint8_t if_nbr, uint8_t if_alt_nbr, bool dir_in, uint16_t max_pkt_len, uint8_t *p_ep_addr) |
Add a bulk endpoint to alternate setting interface. | |
sl_status_t | sl_usbd_core_read_bulk_sync (uint8_t ep_addr, void *p_buf, uint32_t buf_len, uint16_t timeout_ms, uint32_t *p_xfer_len) |
Receive data on Bulk OUT endpoint. | |
sl_status_t | sl_usbd_core_read_bulk_async (uint8_t ep_addr, void *p_buf, uint32_t buf_len, sl_usbd_async_function_t async_fnct, void *p_async_arg) |
Receive data on Bulk OUT endpoint asynchronously. | |
sl_status_t | sl_usbd_core_write_bulk_sync (uint8_t ep_addr, void *p_buf, uint32_t buf_len, uint16_t timeout_ms, bool end, uint32_t *p_xfer_len) |
Send data on a Bulk IN endpoint. | |
sl_status_t | sl_usbd_core_write_bulk_async (uint8_t ep_addr, void *p_buf, uint32_t buf_len, sl_usbd_async_function_t async_fnct, void *p_async_arg, bool end) |
Send data on the Bulk IN endpoint asynchronously. | |
sl_status_t | sl_usbd_core_add_interrupt_endpoint (uint8_t config_nbr, uint8_t if_nbr, uint8_t if_alt_nbr, bool dir_in, uint16_t max_pkt_len, uint16_t interval, uint8_t *p_ep_addr) |
Add an interrupt endpoint to an alternate setting interface. | |
sl_status_t | sl_usbd_core_read_interrupt_sync (uint8_t ep_addr, void *p_buf, uint32_t buf_len, uint16_t timeout_ms, uint32_t *p_xfer_len) |
Receive data on the Interrupt OUT endpoint. | |
sl_status_t | sl_usbd_core_read_interrupt_async (uint8_t ep_addr, void *p_buf, uint32_t buf_len, sl_usbd_async_function_t async_fnct, void *p_async_arg) |
Receive data on Interrupt OUT endpoint asynchronously. | |
sl_status_t | sl_usbd_core_write_interrupt_sync (uint8_t ep_addr, void *p_buf, uint32_t buf_len, uint16_t timeout_ms, bool end, uint32_t *p_xfer_len) |
Send data on Interrupt IN endpoint. | |
sl_status_t | sl_usbd_core_write_interrupt_async (uint8_t ep_addr, void *p_buf, uint32_t buf_len, sl_usbd_async_function_t async_fnct, void *p_async_arg, bool end) |
Send data on the Interrupt IN endpoint asynchronously. | |
sl_status_t | sl_usbd_core_endpoint_write_zlp (uint8_t ep_addr, uint16_t timeout_ms) |
Add an isochronous endpoint to alternate setting interface. | |
sl_status_t | sl_usbd_core_endpoint_read_zlp (uint8_t ep_addr, uint16_t timeout_ms) |
Receive zero-length packet from the host. | |
sl_status_t | sl_usbd_core_abort_endpoint (uint8_t ep_addr) |
Abort I/O transfer on the endpoint. | |
sl_status_t | sl_usbd_core_endpoint_read_complete (uint8_t ep_log_nbr) |
Notify USB stack that packet receive has completed. | |
sl_status_t | sl_usbd_core_endpoint_write_complete (uint8_t ep_log_nbr) |
Notify USB stack that packet transmit has completed. | |
sl_status_t | sl_usbd_core_endpoint_write_complete_extended (uint8_t ep_log_nbr, sl_status_t xfer_err) |
Notify USB stack that packet transmit has completed (see Note #1). | |
sl_status_t | sl_usbd_core_stall_endpoint (uint8_t ep_addr, bool state) |
Stall the non-control endpoint. | |
sl_status_t | sl_usbd_core_is_endpoint_stalled (uint8_t ep_addr, bool *p_ep_stall) |
Get the stall status of a non-control endpoint. | |
sl_status_t | sl_usbd_core_get_max_endpoint_packet_size (uint8_t ep_addr, uint16_t *p_max_size) |
Retrieve the endpoint maximum packet size. | |
sl_status_t | sl_usbd_core_get_max_phy_endpoint_number (uint8_t *p_ep_phy_nbr) |
Get the maximum physical endpoint number. | |
sl_status_t | sl_usbd_core_get_max_open_endpoint_number (uint8_t *p_nbr_open) |
__WEAK void | sl_usbd_on_bus_event (sl_usbd_bus_event_t event) |
__WEAK void | sl_usbd_on_config_event (sl_usbd_config_event_t event, uint8_t config_nbr) |
Macros | |
#define | SL_USBD_FRAME_NBR_MAX 2047u |
#define | SL_USBD_FRAME_NBR_MASK 0b0000011111111111 |
#define | SL_USBD_MICROFRAME_NBR_MASK 0b0011100000000000 |
#define | SL_USBD_DEV_ATTRIB_SELF_POWERED 0x01u |
#define | SL_USBD_DEV_ATTRIB_REMOTE_WAKEUP 0x02u |
#define | SL_USBD_DESC_LEN_DEV 18u |
#define | SL_USBD_DESC_LEN_DEV_QUAL 10u |
#define | SL_USBD_DESC_LEN_HDR 2u |
#define | SL_USBD_DESC_LEN_CFG 9u |
#define | SL_USBD_DESC_LEN_OTHER_SPD_CFG 9u |
#define | SL_USBD_DESC_LEN_IF 9u |
#define | SL_USBD_DESC_LEN_IF_ASSOCIATION 8u |
#define | SL_USBD_DESC_LEN_EP 7u |
#define | SL_USBD_DESC_LEN_OTG 3u |
#define | SL_USBD_REQ_DIR_MASK 0x80u |
#define | SL_USBD_REQ_DIR_HOST_TO_DEVICE 0x00u |
#define | SL_USBD_REQ_DIR_DEVICE_TO_HOST 0x80u |
#define | SL_USBD_REQ_DIR_BIT 0x80u |
#define | SL_USBD_REQ_TYPE_MASK 0x60u |
#define | SL_USBD_REQ_TYPE_STANDARD 0x00u |
#define | SL_USBD_REQ_TYPE_CLASS 0x20u |
#define | SL_USBD_REQ_TYPE_VENDOR 0x40u |
#define | SL_USBD_REQ_TYPE_RESERVED 0x60u |
#define | SL_USBD_REQ_RECIPIENT_MASK 0x1Fu |
#define | SL_USBD_REQ_RECIPIENT_DEVICE 0x00u |
#define | SL_USBD_REQ_RECIPIENT_INTERFACE 0x01u |
#define | SL_USBD_REQ_RECIPIENT_ENDPOINT 0x02u |
#define | SL_USBD_REQ_RECIPIENT_OTHER 0x03u |
#define | SL_USBD_REQ_GET_STATUS 0u |
#define | SL_USBD_REQ_CLEAR_FEATURE 1u |
#define | SL_USBD_REQ_SET_FEATURE 3u |
#define | SL_USBD_REQ_SET_ADDRESS 5u |
#define | SL_USBD_REQ_GET_DESCRIPTOR 6u |
#define | SL_USBD_REQ_SET_DESCRIPTOR 7u |
#define | SL_USBD_REQ_GET_CONFIGURATION 8u |
#define | SL_USBD_REQ_SET_CONFIGURATION 9u |
#define | SL_USBD_REQ_GET_INTERFACE 10u |
#define | SL_USBD_REQ_SET_INTERFACE 11u |
#define | SL_USBD_REQ_SYNCH_FRAME 12u |
#define | SL_USBD_DESC_TYPE_DEVICE 1u |
#define | SL_USBD_DESC_TYPE_CONFIGURATION 2u |
#define | SL_USBD_DESC_TYPE_STRING 3u |
#define | SL_USBD_DESC_TYPE_INTERFACE 4u |
#define | SL_USBD_DESC_TYPE_ENDPOINT 5u |
#define | SL_USBD_DESC_TYPE_DEVICE_QUALIFIER 6u |
#define | SL_USBD_DESC_TYPE_OTHER_SPEED_CONFIGURATION 7u |
#define | SL_USBD_DESC_TYPE_INTERFACE_POWER 8u |
#define | SL_USBD_DESC_TYPE_OTG 9u |
#define | SL_USBD_DESC_TYPE_IAD 11u |
#define | SL_USBD_LANG_ID_ARABIC_SAUDI_ARABIA 0x0401u |
#define | SL_USBD_LANG_ID_CHINESE_TAIWAN 0x0404u |
#define | SL_USBD_LANG_ID_ENGLISH_US 0x0409u |
#define | SL_USBD_LANG_ID_ENGLISH_UK 0x0809u |
#define | SL_USBD_LANG_ID_FRENCH 0x040Cu |
#define | SL_USBD_LANG_ID_GERMAN 0x0407u |
#define | SL_USBD_LANG_ID_GREEK 0x0408u |
#define | SL_USBD_LANG_ID_ITALIAN 0x0410u |
#define | SL_USBD_LANG_ID_PORTUGUESE 0x0816u |
#define | SL_USBD_LANG_ID_SANSKRIT 0x044Fu |
#define | SL_USBD_CLASS_CODE_USE_IF_DESC 0x00u |
#define | SL_USBD_CLASS_CODE_AUDIO 0x01u |
#define | SL_USBD_CLASS_CODE_CDC_CONTROL 0x02u |
#define | SL_USBD_CLASS_CODE_HID 0x03u |
#define | SL_USBD_CLASS_CODE_PHYSICAL 0x05u |
#define | SL_USBD_CLASS_CODE_IMAGE 0x06u |
#define | SL_USBD_CLASS_CODE_PRINTER 0x07u |
#define | SL_USBD_CLASS_CODE_MASS_STORAGE 0x08u |
#define | SL_USBD_CLASS_CODE_HUB 0x09u |
#define | SL_USBD_CLASS_CODE_CDC_DATA 0x0Au |
#define | SL_USBD_CLASS_CODE_SMART_CARD 0x0Bu |
#define | SL_USBD_CLASS_CODE_CONTENT_SECURITY 0x0Du |
#define | SL_USBD_CLASS_CODE_VIDEO 0x0Eu |
#define | SL_USBD_CLASS_CODE_PERSONAL_HEALTHCARE 0x0Fu |
#define | SL_USBD_CLASS_CODE_DIAGNOSTIC_DEVICE 0xDCu |
#define | SL_USBD_CLASS_CODE_WIRELESS_CONTROLLER 0xE0u |
#define | SL_USBD_CLASS_CODE_MISCELLANEOUS 0xEFu |
#define | SL_USBD_CLASS_CODE_APPLICATION_SPECIFIC 0xFEu |
#define | SL_USBD_CLASS_CODE_VENDOR_SPECIFIC 0xFFu |
#define | SL_USBD_SUBCLASS_CODE_USE_IF_DESC 0x00u |
#define | SL_USBD_SUBCLASS_CODE_USE_COMMON_CLASS 0x02u |
#define | SL_USBD_SUBCLASS_CODE_VENDOR_SPECIFIC 0xFFu |
#define | SL_USBD_PROTOCOL_CODE_USE_IF_DESC 0x00u |
#define | SL_USBD_PROTOCOL_CODE_USE_IAD 0x01u |
#define | SL_USBD_PROTOCOL_CODE_VENDOR_SPECIFIC 0xFFu |
#define | SL_USBD_FEATURE_SEL_ENDPOINT_HALT 0u |
#define | SL_USBD_FEATURE_SEL_DEVICE_REMOTE_WAKEUP 1u |
#define | SL_USBD_FEATURE_SEL_TEST_MODE 2u |
#define | SL_USBD_MAX_BUS_PWR_LIMIT_mA 500u |
#define | SL_USBD_ENDPOINT_TYPE_MASK 0x03u |
#define | SL_USBD_ENDPOINT_TYPE_CTRL 0x00u |
#define | SL_USBD_ENDPOINT_TYPE_ISOC 0x01u |
#define | SL_USBD_ENDPOINT_TYPE_BULK 0x02u |
#define | SL_USBD_ENDPOINT_TYPE_INTR 0x03u |
#define | SL_USBD_ENDPOINT_TYPE_SYNC_MASK 0x0Cu |
#define | SL_USBD_ENDPOINT_TYPE_SYNC_NONE 0x00u |
#define | SL_USBD_ENDPOINT_TYPE_SYNC_ASYNC 0x04u |
#define | SL_USBD_ENDPOINT_TYPE_SYNC_ADAPTIVE 0x08u |
#define | SL_USBD_ENDPOINT_TYPE_SYNC_SYNC 0x0Cu |
#define | SL_USBD_ENDPOINT_TYPE_USAGE_MASK 0x30u |
#define | SL_USBD_ENDPOINT_TYPE_USAGE_DATA 0x00u |
#define | SL_USBD_ENDPOINT_TYPE_USAGE_FEEDBACK 0x10u |
#define | SL_USBD_ENDPOINT_TYPE_USAGE_IMPLICIT_FEEDBACK 0x20u |
#define | SL_USBD_ENDPOINT_NBR_MASK 0x0Fu |
#define | SL_USBD_ENDPOINT_MAX_NBR 32u |
#define | SL_USBD_ENDPOINT_DIR_MASK 0x80u |
#define | SL_USBD_ENDPOINT_DIR_BIT 0x80u |
#define | SL_USBD_ENDPOINT_DIR_OUT 0x00u |
#define | SL_USBD_ENDPOINT_DIR_IN 0x80u |
#define | SL_USBD_ENDPOINT_TRANSACTION_PER_UFRAME_1 1u |
#define | SL_USBD_ENDPOINT_TRANSACTION_PER_UFRAME_2 2u |
#define | SL_USBD_ENDPOINT_TRANSACTION_PER_UFRAME_3 3u |
#define | SL_USBD_ENDPOINT_MAX_INTERVAL_VAL 32768u |
#define | SL_USBD_MICROSOFT_COMPAT_ID_NULL 0u |
#define | SL_USBD_MICROSOFT_COMPAT_ID_RNDIS 1u |
#define | SL_USBD_MICROSOFT_COMPAT_ID_PTP 2u |
#define | SL_USBD_MICROSOFT_COMPAT_ID_MTP 3u |
#define | SL_USBD_MICROSOFT_COMPAT_ID_XUSB20 4u |
#define | SL_USBD_MICROSOFT_COMPAT_ID_BLUETOOTH 5u |
#define | SL_USBD_MICROSOFT_COMPAT_ID_WINUSB 6u |
#define | SL_USBD_MICROSOFT_COMPAT_ID_NONE 255u |
#define | SL_USBD_MICROSOFT_SUBCOMPAT_ID_NULL 0u |
#define | SL_USBD_MICROSOFT_SUBCOMPAT_ID_BLUETOOTH_1_1 1u |
#define | SL_USBD_MICROSOFT_SUBCOMPAT_ID_BLUETOOTH_1_2 2u |
#define | SL_USBD_MICROSOFT_SUBCOMPAT_ID_BLUETOOTH_EDR 3u |
#define | SL_USBD_MICROSOFT_PROPERTY_TYPE_REG_SZ 1u |
#define | SL_USBD_MICROSOFT_PROPERTY_TYPE_REG_EXPAND_SZ 2u |
#define | SL_USBD_MICROSOFT_PROPERTY_TYPE_REG_BINARY 3u |
#define | SL_USBD_MICROSOFT_PROPERTY_TYPE_REG_DWORD_LITTLE_ENDIAN 4u |
#define | SL_USBD_MICROSOFT_PROPERTY_TYPE_REG_DWORD_BIG_ENDIAN 5u |
#define | SL_USBD_MICROSOFT_PROPERTY_TYPE_REG_LINK 6u |
#define | SL_USBD_MICROSOFT_PROPERTY_TYPE_REG_MULTI_SZ 7u |
#define | SL_USBD_ENDPOINT_INFO_TYPE_CTRL 0x01u |
#define | SL_USBD_ENDPOINT_INFO_TYPE_ISOC 0x02u |
#define | SL_USBD_ENDPOINT_INFO_TYPE_BULK 0x04u |
#define | SL_USBD_ENDPOINT_INFO_TYPE_INTR 0x08u |
#define | SL_USBD_ENDPOINT_INFO_DIR_OUT 0x10u |
#define | SL_USBD_ENDPOINT_INFO_DIR_IN 0x20u |
#define | SL_USBD_CONFIG_NBR_NONE 255u |
#define | SL_USBD_CONFIG_NBR_SPD_BIT 0x80u |
#define | SL_USBD_INTERFACE_NBR_NONE 255u |
#define | SL_USBD_ALT_INTERFACE_NBR_NONE 255u |
#define | SL_USBD_INTERFACE_GROUP_NBR_NONE 255u |
#define | SL_USBD_ENDPOINT_ADDR_NONE 255u |
#define | SL_USBD_ENDPOINT_PHY_NONE 255u |
#define | SL_USBD_ENDPOINT_NBR_NONE 255u |
#define | SL_USBD_CLASS_NBR_NONE 255u |
#define | USBD_CFG_STR_EN 1 |
#define | USBD_CFG_MS_OS_DESC_EN 0 |
#define | USBD_CFG_URB_EXTRA_EN 0 |
#define | SL_USBD_URB_MAX_NBR SL_USBD_OPEN_ENDPOINTS_QUANTITY |
#define | SL_USBD_CORE_EVENT_BUS_NBR 7u |
#define | SL_USBD_CORE_EVENT_BUS_NBR_TOTAL (SL_USBD_CORE_EVENT_BUS_NBR * SL_USBD_DEVICE_QUANTITY) |
#define | SL_USBD_CORE_EVENT_ASYNC_NBR ((SL_USBD_OPEN_ENDPOINTS_QUANTITY * SL_USBD_DEVICE_QUANTITY) + SL_USBD_EXTRA_URB_QUANTITY) |
#define | SL_USBD_CORE_EVENT_NBR_TOTAL (SL_USBD_CORE_EVENT_BUS_NBR_TOTAL + SL_USBD_CORE_EVENT_ASYNC_NBR) |
#define | SL_USBD_FRAME_NBR_GET(frame_nbr) ((frame_nbr) & SL_USBD_FRAME_NBR_MASK) |
#define | SL_USBD_MICROFRAME_NBR_GET(microframe_nbr) ((microframe_nbr) >> 11u) |
#define | SL_USBD_FRAME_NBR_DIFF_GET(frame_nbr1, frame_nbr2) |
#define | SL_USBD_ENDPOINT_PHY_TO_ADDR(ep_phy_nbr) |
#define | SL_USBD_ENDPOINT_ADDR_TO_PHY(ep_addr) |
#define | SL_USBD_ENDPOINT_ADDR_TO_LOG(ep_addr) (uint8_t)((ep_addr) & SL_USBD_ENDPOINT_NBR_MASK) |
#define | SL_USBD_ENDPOINT_PHY_TO_LOG(ep_phy_nbr) (ep_phy_nbr / 2u) |
#define | SL_USBD_ENDPOINT_LOG_TO_ADDR_IN(ep_log_nbr) ((ep_log_nbr) | SL_USBD_ENDPOINT_DIR_IN) |
#define | SL_USBD_ENDPOINT_LOG_TO_ADDR_OUT(ep_log_nbr) ((ep_log_nbr) | SL_USBD_ENDPOINT_DIR_OUT) |
#define | SL_USBD_ENDPOINT_IS_IN(ep_addr) ((((ep_addr) & SL_USBD_ENDPOINT_DIR_MASK) != 0u) ? true : false) |
Typedefs | |
typedef void(* | sl_usbd_async_function_t) (uint8_t ep_addr, void *p_buf, uint32_t buf_len, uint32_t xfer_len, void *p_arg, sl_status_t status) |
Enumerations | |
enum | sl_usbd_device_speed_t { SL_USBD_DEVICE_SPEED_INVALID = 0u , SL_USBD_DEVICE_SPEED_LOW , SL_USBD_DEVICE_SPEED_FULL , SL_USBD_DEVICE_SPEED_HIGH } |
enum | sl_usbd_device_state_t { SL_USBD_DEVICE_STATE_NONE = 0 , SL_USBD_DEVICE_STATE_INIT , SL_USBD_DEVICE_STATE_ATTACHED , SL_USBD_DEVICE_STATE_DEFAULT , SL_USBD_DEVICE_STATE_ADDRESSED , SL_USBD_DEVICE_STATE_CONFIGURED , SL_USBD_DEVICE_STATE_SUSPENDED } |
enum | sl_usbd_bus_event_t { SL_USBD_EVENT_BUS_CONNECT = 0 , SL_USBD_EVENT_BUS_DISCONNECT , SL_USBD_EVENT_BUS_RESET , SL_USBD_EVENT_BUS_SUSPEND , SL_USBD_EVENT_BUS_RESUME } |
enum | sl_usbd_config_event_t { SL_USBD_EVENT_CONFIG_SET = 0 , SL_USBD_EVENT_CONFIG_UNSET } |
CONFIG EVENT DATA TYPE. |
Function Documentation
◆ sl_usbd_core_init()
sl_status_t sl_usbd_core_init | ( | void |
| ) |
Initialize the USB device stack.
sl_usbd_core_init()
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) sli_usbd_core_init_internals() MUST be called ... :
- (a) ONLY ONCE from a product's application;
- (b) With the following conditions:
- (1) AFTER the product's OS has been initialized.
- (2) BEFORE the product's application calls any USB device stack function(s).
◆ sl_usbd_core_start_device()
sl_status_t sl_usbd_core_start_device | ( | void |
| ) |
Start the device stack.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) Device stack can be only started if the device is in one of the following states:
- SL_USBD_DEVICE_STATE_NONE Device controller has not been initialized.
- SL_USBD_DEVICE_STATE_INIT Device controller is already initialized.
◆ sl_usbd_core_stop_device()
sl_status_t sl_usbd_core_stop_device | ( | void |
| ) |
Stop the device stack.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_core_get_device_state()
sl_status_t sl_usbd_core_get_device_state | ( | sl_usbd_device_state_t * | p_dev_state | ) |
Get the current device state.
- Parameters
-
p_dev_state
Pointer to device state to be returned. Set to current device state, if no errors are returned, or SL_USBD_DEVICE_STATE_NONE, if any errors are returned.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_core_get_device_speed()
sl_status_t sl_usbd_core_get_device_speed | ( | sl_usbd_device_speed_t * | p_dev_speed | ) |
Get device speed.
- Parameters
-
p_dev_speed
Pointer to the variable that will be set to device speed upon return. It will be set to current device speed, if successful, or SL_USBD_DEVICE_SPEED_INVALID, if unsuccessful.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_core_set_device_self_power()
sl_status_t sl_usbd_core_set_device_self_power | ( | bool | self_pwr | ) |
Set the device's current power source.
- Parameters
-
self_pwr
The power source of the device : - true device is self-powered.
- false device is bus-powered.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_core_get_device_configuration()
sl_status_t sl_usbd_core_get_device_configuration | ( | sl_usbd_device_config_t ** | p_dev_cfg | ) |
Set the device's Microsoft vendor code.
- Parameters
-
vendor_code
Microsoft vendor code.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) The vendor code used MUST be different from any vendor bRequest value.
Get the device configuration.
- Parameters
-
p_dev_cfg
Pointer to a variable of type (sl_usbd_device_config_t *) which will receive the memory address of device configuration structure upon return. The variable will be set to point to device configuration, if no errors are returned, or it will be set to NULL if any errors are returned.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_core_get_device_frame_number()
sl_status_t sl_usbd_core_get_device_frame_number | ( | uint16_t * | p_frame_nbr | ) |
Get the last frame number from the driver.
- Parameters
-
p_frame_nbr
Pointer to variable that will receive frame number.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) The frame number will always be in the range of 0-2047 (11 bits).
-
(2) Frame number returned to the caller contains the frame and microframe numbers. It is encoded following this 16-bit format:
* | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | * | 0 0 | microframe | frame | *
Caller must use the macros SL_USBD_FRAME_NBR_GET() or SL_USBD_MICROFRAME_NBR_GET() to get the frame or microframe number only.
◆ sl_usbd_core_add_configuration()
sl_status_t sl_usbd_core_add_configuration | ( | uint8_t | attrib, |
uint16_t | max_pwr, |
||
sl_usbd_device_speed_t | spd, |
||
const char * | p_name, |
||
uint8_t * | p_cfg_nbr |
||
) |
Add a configuration attribute to the device.
- Parameters
-
attrib
Available configuration attributes. - SL_USBD_DEV_ATTRIB_SELF_POWERED Power does not come from VBUS.
- SL_USBD_DEV_ATTRIB_REMOTE_WAKEUP Remote wakeup feature enabled.
max_pwr
Bus power required for this device (see Note #1). spd
Available configuration speeds. - SL_USBD_DEVICE_SPEED_FULL Configuration is added in the full-speed configuration set.
p_name
Pointer to string describing the configuration (see Note #2). p_cfg_nbr
Pointer to variable that will receive the configuration number. It will be set to the configuration number, if no errors are returned, otherwise it will be set to SL_USBD_CONFIG_NBR_NONE if any errors are returned.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) USB spec 2.0 (section 7.2.1.3/4) defines power constraints for bus-powered devices: "A low-power function draws up to one unit load from the USB cable when operational" "A function is high-power if, when fully powered, draws over one, but no more than five, unit loads from the USB cable." A unit load is defined as 100mA, so 'max_pwr' argument should be between 0 mA and 500mA
- (2) String support is optional: 'p_name' can be a NULL string pointer.
-
(3) Configuration can only be added when the device is in the following states:
- SL_USBD_DEVICE_STATE_NONE Device controller has not been initialized.
- SL_USBD_DEVICE_STATE_INIT Device controller is already initialized.
◆ sl_usbd_core_add_interface()
sl_status_t sl_usbd_core_add_interface | ( | uint8_t | cfg_nbr, |
sl_usbd_class_driver_t * | p_class_drv, |
||
void * | p_if_class_arg, |
||
void * | p_if_alt_class_arg, |
||
uint8_t | class_code, |
||
uint8_t | class_sub_code, |
||
uint8_t | class_protocol_code, |
||
const char * | p_name, |
||
uint8_t * | p_if_nbr |
||
) |
Associate a configuration with its alternative-speed counterpart.
- Parameters
-
config_nbr
Configuration number. config_other
Other-speed configuration number.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) Configurations from high- and full-speed can be associated with each other to provide comparable functionality regardless of speed.
-
(2) Configuration can ONLY be associated when the device is in the following states:
- SL_USBD_DEVICE_STATE_NONE Device controller has not been initialized.
- SL_USBD_DEVICE_STATE_INIT Device controller is already initialized.
Add an interface to a specific configuration.
- Parameters
-
cfg_nbr
Configuration index to add the interface. p_class_drv
Pointer to interface driver. p_if_class_arg
Pointer to interface driver argument. p_if_alt_class_arg
Pointer to alternate interface argument. class_code
Class code assigned by the USB-IF. class_sub_code
Subclass code assigned by the USB-IF. class_protocol_code
protocol code assigned by the USB-IF. p_name
Pointer to string describing the Interface. p_if_nbr
Pointer to a variable that will receive interface number after creation. The variable will be set to the interface number, if no errors are returned, otherwise it is set to SL_USBD_INTERFACE_NBR_NONE.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) USB Spec 2.0 Interface (section 9.6.5) states: "An interface may include alternate settings that allow the endpoints and/or their characteristics to be varied after the device has been configured. The default setting for an interface is always an alternate setting of zero."
◆ sl_usbd_core_add_alt_interface()
sl_status_t sl_usbd_core_add_alt_interface | ( | uint8_t | config_nbr, |
uint8_t | if_nbr, |
||
void * | p_class_arg, |
||
const char * | p_name, |
||
uint8_t * | p_if_alt_nbr |
||
) |
Add an alternate setting to a specific interface.
- Parameters
-
config_nbr
Configuration number. if_nbr
Interface number. p_class_arg
Pointer to alternate interface argument. p_name
Pointer to alternate setting name. p_if_alt_nbr
Pointer to variable that will receive alternate setting number upon return. It will be set to interface alternate setting number if no error(s) are returned, or SL_USBD_ALT_INTERFACE_NBR_NONE if any errors are returned.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_core_add_interface_group()
sl_status_t sl_usbd_core_add_interface_group | ( | uint8_t | config_nbr, |
uint8_t | class_code, |
||
uint8_t | class_sub_code, |
||
uint8_t | class_protocol_code, |
||
uint8_t | if_start, |
||
uint8_t | if_cnt, |
||
const char * | p_name, |
||
uint8_t * | p_if_grp_num |
||
) |
Create an interface group.
- Parameters
-
config_nbr
Configuration number. class_code
Class code assigned by the USB-IF. class_sub_code
Subclass code assigned by the USB-IF. class_protocol_code
protocol code assigned by the USB-IF. if_start
Interface number of the first interface that is associated with this group. if_cnt
Number of consecutive interfaces that are associated with this group. p_name
Pointer to the string that describes the interface group. p_if_grp_num
Pointer to the variable that will receive interface group number upon return. The variable is set to interface group number if no errors are returned, or SL_USBD_INTERFACE_GROUP_NBR_NONE if any errors are returned.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_core_get_device_descriptor()
sl_status_t sl_usbd_core_get_device_descriptor | ( | uint8_t * | p_buf, |
uint8_t | max_len, |
||
uint8_t * | p_desc_len |
||
) |
Get the device descriptor.
- Parameters
-
p_buf
Pointer to the destination buffer. max_len
Maximum number of bytes to write in destination buffer. p_desc_len
Pointer to a variable that will receive the actual size of the descriptor. The variable is set to number of bytes actually in the descriptor if no errors are returned, or set to 0 if any errors are returned.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) This function should be used by drivers that supporting the standard requests auto-reply, (during the initialization process).
◆ sl_usbd_core_get_configuration_descriptor()
sl_status_t sl_usbd_core_get_configuration_descriptor | ( | uint8_t * | p_buf, |
uint16_t | max_len, |
||
uint8_t | config_ix, |
||
uint16_t * | p_desc_len |
||
) |
Get a configuration descriptor.
- Parameters
-
p_buf
Pointer to the destination buffer. max_len
Maximum number of bytes to write in the destination buffer. config_ix
Index of the desired configuration descriptor. p_desc_len
Pointer to a variable that will receive the actual size of the descriptor. The variable is set to number of bytes actually in the descriptor if no errors are returned, or set to 0 if any errors are returned.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) This function should be used by drivers supporting a standard request's auto-reply, during the initialization process.
◆ sl_usbd_core_get_string_descriptor()
sl_status_t sl_usbd_core_get_string_descriptor | ( | uint8_t * | p_buf, |
uint8_t | max_len, |
||
uint8_t | str_ix, |
||
uint8_t * | p_desc_len |
||
) |
Get a string descriptor.
- Parameters
-
p_buf
Pointer to the destination buffer. max_len
Maximum number of bytes to write in destination buffer. str_ix
Index of the desired string descriptor. p_desc_len
Pointer to a variable that will receive the actual size of the descriptor. The variable is set to number of bytes actually in the descriptor if no errors are returned, or set to 0 if any errors are returned.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) This function should be used by drivers supporting a standard request's auto-reply, during the initialization process.
◆ sl_usbd_core_add_string()
sl_status_t sl_usbd_core_add_string | ( | const char * | p_str | ) |
Add string to USB device.
- Parameters
-
p_str
Pointer to string to add (see Note #1).
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) USB spec 2.0 chapter 9.5 states: "Where appropriate, descriptors contain references to string descriptors that provide displayable information describing a descriptor in human-readable form. The inclusion of string descriptors is optional. However, the reference fields within descriptors are mandatory. If a device does not support string descriptors, string reference fields must be reset to zero to indicate no string descriptor is available". Since string descriptors are optional, 'p_str' could be a NULL pointer.
◆ sl_usbd_core_get_string_index()
sl_status_t sl_usbd_core_get_string_index | ( | const char * | p_str, |
uint8_t * | p_str_ix |
||
) |
Get string index corresponding to a given string.
- Parameters
-
p_str
Pointer to string. p_str_ix
Pointer to variable where string index will be returned.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_core_write_08b_to_descriptor_buf()
sl_status_t sl_usbd_core_write_08b_to_descriptor_buf | ( | uint8_t | val | ) |
Write an 8-bit value to the descriptor buffer.
- Parameters
-
val
8-bit value to write in the descriptor buffer.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) USB classes may use this function to append class-specific descriptors to the configuration descriptor.
◆ sl_usbd_core_write_16b_to_descriptor_buf()
sl_status_t sl_usbd_core_write_16b_to_descriptor_buf | ( | uint16_t | val | ) |
Write a 16-bit value in the descriptor buffer.
- Parameters
-
val
16-bit value.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) USB classes may use this function to append class-specific descriptors to the configuration descriptor.
- (2) USB descriptors are in little-endian format.
◆ sl_usbd_core_write_24b_to_descriptor_buf()
sl_status_t sl_usbd_core_write_24b_to_descriptor_buf | ( | uint32_t | val | ) |
Write a 24-bit value to the descriptor buffer.
- Parameters
-
val
32-bit value containing 24 useful bits to write in the descriptor buffer.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) USB classes may use this function to append class-specific descriptors to the configuration descriptor.
- (2) USB descriptors are in little-endian format.
◆ sl_usbd_core_write_32b_to_descriptor_buf()
sl_status_t sl_usbd_core_write_32b_to_descriptor_buf | ( | uint32_t | val | ) |
Write a 32-bit value to the descriptor buffer.
- Parameters
-
val
32-bit value to write in the descriptor buffer.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) USB classes may use this function to append class-specific descriptors to the configuration descriptor.
- (2) USB descriptors are in little-endian format.
◆ sl_usbd_core_write_buf_to_descriptor_buf()
sl_status_t sl_usbd_core_write_buf_to_descriptor_buf | ( | const uint8_t * | p_buf, |
uint16_t | len |
||
) |
Write a buffer into the descriptor buffer.
- Parameters
-
p_buf
Pointer to the buffer to write into the descriptor buffer. len
Length of the buffer.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) USB classes may use this function to append class-specific descriptors to the configuration descriptor.
◆ sl_usbd_core_write_control_sync()
sl_status_t sl_usbd_core_write_control_sync | ( | void * | p_buf, |
uint32_t | buf_len, |
||
uint16_t | timeout_ms, |
||
bool | end, |
||
uint32_t * | p_xfer_len |
||
) |
Send data on the Control IN endpoint.
- Parameters
-
p_buf
Pointer to the buffer of data that will be sent (see Note #2). buf_len
Number of octets to transmit. timeout_ms
Timeout in milliseconds. end
End-of-transfer flag (see Note #1). p_xfer_len
Pointer to a variable that will be set to the number of octets transmitted. The variable is set to the number of octets transmitted if no errors are returned, otherwise it is set to 0.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) If end-of-transfer is set and transfer length is multiple of maximum packet size, a zero-length packet is transferred to indicate a short transfer to the host.
- (2) Transmit buffer must be 32 bits aligned.
◆ sl_usbd_core_read_control_sync()
sl_status_t sl_usbd_core_read_control_sync | ( | void * | p_buf, |
uint32_t | buf_len, |
||
uint16_t | timeout_ms, |
||
uint32_t * | p_xfer_len |
||
) |
Receive data on the Control OUT endpoint.
- Parameters
-
p_buf
Pointer to the destination buffer to receive data (see Note #1). buf_len
Number of octets to receive. timeout_ms
Timeout in milliseconds. p_xfer_len
Pointer to a variable that will be set to the number of octets received. The variable is set to the number of octets received if no errors are returned, otherwise it is set to 0.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) Receive buffer must be 32 bits aligned.
◆ sl_usbd_core_add_bulk_endpoint()
sl_status_t sl_usbd_core_add_bulk_endpoint | ( | uint8_t | config_nbr, |
uint8_t | if_nbr, |
||
uint8_t | if_alt_nbr, |
||
bool | dir_in, |
||
uint16_t | max_pkt_len, |
||
uint8_t * | p_ep_addr |
||
) |
Add a bulk endpoint to alternate setting interface.
- Parameters
-
config_nbr
Configuration number. if_nbr
Interface number. if_alt_nbr
Interface alternate setting number. dir_in
Endpoint direction. - true IN direction.
- false OUT direction.
max_pkt_len
Endpoint maximum packet length (see Note #1) p_ep_addr
Pointer to a variable that will receive the new endpoint address. The variable will be set to endpoint address if no errors are returned, otherwise it will be set to SL_USBD_ENDPOINT_ADDR_NONE.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) If the 'max_pkt_len' argument is '0', the stack will allocate the first available BULK endpoint, regardless its maximum packet size.
◆ sl_usbd_core_read_bulk_sync()
sl_status_t sl_usbd_core_read_bulk_sync | ( | uint8_t | ep_addr, |
void * | p_buf, |
||
uint32_t | buf_len, |
||
uint16_t | timeout_ms, |
||
uint32_t * | p_xfer_len |
||
) |
Receive data on Bulk OUT endpoint.
- Parameters
-
ep_addr
Endpoint address. p_buf
Pointer to the destination buffer to receive data (see Note #1). buf_len
Number of octets to receive. timeout_ms
Timeout in milliseconds. p_xfer_len
Pointer to a variable that will be set to the number of octets received. The variable is set to the number of octets received if no errors are returned, otherwise it is set to 0.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) Receive buffer must be 32 bits aligned.
◆ sl_usbd_core_read_bulk_async()
sl_status_t sl_usbd_core_read_bulk_async | ( | uint8_t | ep_addr, |
void * | p_buf, |
||
uint32_t | buf_len, |
||
sl_usbd_async_function_t | async_fnct, |
||
void * | p_async_arg |
||
) |
Receive data on Bulk OUT endpoint asynchronously.
- Parameters
-
ep_addr
Endpoint address. p_buf
Pointer to the destination buffer to receive data (see Note #1). buf_len
Number of octets to receive. async_fnct
Function that will be invoked upon completion of receive operation. p_async_arg
Pointer to the argument that will be passed as parameter of 'async_fnct'.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) Receive buffer must be 32 bits aligned.
◆ sl_usbd_core_write_bulk_sync()
sl_status_t sl_usbd_core_write_bulk_sync | ( | uint8_t | ep_addr, |
void * | p_buf, |
||
uint32_t | buf_len, |
||
uint16_t | timeout_ms, |
||
bool | end, |
||
uint32_t * | p_xfer_len |
||
) |
Send data on a Bulk IN endpoint.
- Parameters
-
ep_addr
Endpoint address. p_buf
Pointer to buffer of data that will be transmitted (see Note #2). buf_len
Number of octets to transmit. timeout_ms
Timeout in milliseconds. end
End-of-transfer flag (see Note #3). p_xfer_len
Pointer to a variable that will receive the number of octets transmitted. The variable is set to the number of octets transmitted if no errors are returned, otherwise it is set to 0.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) This function SHOULD NOT be called from interrupt service routine (ISR).
- (2) Transmit buffer must be 32 bits aligned.
- (3) If end-of-transfer is set and transfer length is multiple of maximum packet sizes, a zero-length packet is transferred to indicate a short transfer to the host.
◆ sl_usbd_core_write_bulk_async()
sl_status_t sl_usbd_core_write_bulk_async | ( | uint8_t | ep_addr, |
void * | p_buf, |
||
uint32_t | buf_len, |
||
sl_usbd_async_function_t | async_fnct, |
||
void * | p_async_arg, |
||
bool | end |
||
) |
Send data on the Bulk IN endpoint asynchronously.
- Parameters
-
ep_addr
Endpoint address. p_buf
Pointer to the buffer of data that will be transmitted (see Note #1). buf_len
Number of octets to transmit. async_fnct
Function that will be invoked upon completion of transmit operation. p_async_arg
Pointer to the argument that will be passed as parameter of 'async_fnct'. end
End-of-transfer flag (see Note #2).
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) Transmit buffer must be 32 bits aligned.
- (2) If end-of-transfer is set and transfer length is multiple of maximum packet size, a zero-length packet is transferred to indicate a short transfer to the host.
◆ sl_usbd_core_add_interrupt_endpoint()
sl_status_t sl_usbd_core_add_interrupt_endpoint | ( | uint8_t | config_nbr, |
uint8_t | if_nbr, |
||
uint8_t | if_alt_nbr, |
||
bool | dir_in, |
||
uint16_t | max_pkt_len, |
||
uint16_t | interval, |
||
uint8_t * | p_ep_addr |
||
) |
Add an interrupt endpoint to an alternate setting interface.
- Parameters
-
config_nbr
Configuration number. if_nbr
Interface number. if_alt_nbr
Interface alternate setting number. dir_in
Endpoint Direction. - true IN direction.
- false OUT direction.
max_pkt_len
Endpoint maximum packet length. (see Note #1) interval
Endpoint interval in frames or microframes. p_ep_addr
Pointer to a variable that will receive the new endpoint address. The variable will be set to endpoint address if no errors are returned, otherwise it will be set to SL_USBD_ENDPOINT_ADDR_NONE.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) If the 'max_pkt_len' argument is '0', the stack will allocate the first available INTERRUPT endpoint, regardless its maximum packet size.
◆ sl_usbd_core_read_interrupt_sync()
sl_status_t sl_usbd_core_read_interrupt_sync | ( | uint8_t | ep_addr, |
void * | p_buf, |
||
uint32_t | buf_len, |
||
uint16_t | timeout_ms, |
||
uint32_t * | p_xfer_len |
||
) |
Receive data on the Interrupt OUT endpoint.
- Parameters
-
ep_addr
Endpoint address. p_buf
Pointer to the destination buffer to receive data (see Note #2). buf_len
Number of octets to receive. timeout_ms
Timeout in milliseconds. p_xfer_len
Pointer to a variable that will be set to the number of octets received. The variable is set to the number of octets received if no errors are returned, otherwise it is set to 0.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) This function SHOULD NOT be called from interrupt service routine (ISR).
- (2) Receive buffer must be 32 bits aligned.
◆ sl_usbd_core_read_interrupt_async()
sl_status_t sl_usbd_core_read_interrupt_async | ( | uint8_t | ep_addr, |
void * | p_buf, |
||
uint32_t | buf_len, |
||
sl_usbd_async_function_t | async_fnct, |
||
void * | p_async_arg |
||
) |
Receive data on Interrupt OUT endpoint asynchronously.
- Parameters
-
ep_addr
Endpoint address. p_buf
Pointer to the destination buffer to receive data (see Note #1). buf_len
Number of octets to receive. async_fnct
Function that will be invoked upon completion of receive operation. p_async_arg
Pointer to argument that will be passed as parameter of 'async_fnct'.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) Receive buffer must be 32 bits aligned.
◆ sl_usbd_core_write_interrupt_sync()
sl_status_t sl_usbd_core_write_interrupt_sync | ( | uint8_t | ep_addr, |
void * | p_buf, |
||
uint32_t | buf_len, |
||
uint16_t | timeout_ms, |
||
bool | end, |
||
uint32_t * | p_xfer_len |
||
) |
Send data on Interrupt IN endpoint.
- Parameters
-
ep_addr
Endpoint address. p_buf
Pointer to the buffer of data that will be transmitted (see Note #2). buf_len
Number of octets to transmit. timeout_ms
Timeout in milliseconds. end
End-of-transfer flag (see Note #3). p_xfer_len
Pointer to a variable that will be set to the number of octets transmitted. The variable is set to the number of octets transmitted if no errors are returned, otherwise it is set to 0.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) This function SHOULD NOT be called from interrupt service routine (ISR).
- (2) Transmit buffer must be 32 bits aligned.
- (3) If end-of-transfer is set and transfer length is multiple of maximum packet size, a zero-length packet is transferred to indicate a short transfer to the host.
◆ sl_usbd_core_write_interrupt_async()
sl_status_t sl_usbd_core_write_interrupt_async | ( | uint8_t | ep_addr, |
void * | p_buf, |
||
uint32_t | buf_len, |
||
sl_usbd_async_function_t | async_fnct, |
||
void * | p_async_arg, |
||
bool | end |
||
) |
Send data on the Interrupt IN endpoint asynchronously.
- Parameters
-
ep_addr
Endpoint address. p_buf
Pointer to the buffer of data that will be transmitted (see Note #1). buf_len
Number of octets to transmit. async_fnct
Function that will be invoked upon completion of transmit operation. p_async_arg
Pointer to the argument that will be passed as parameter of 'async_fnct'. end
End-of-transfer flag (see Note #2).
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) Transmit buffer must be 32 bits aligned.
- (2) If end-of-transfer is set and transfer length is multiple of maximum packet size, a zero-length packet is transferred to indicate a short transfer to the host.
◆ sl_usbd_core_endpoint_write_zlp()
sl_status_t sl_usbd_core_endpoint_write_zlp | ( | uint8_t | ep_addr, |
uint16_t | timeout_ms |
||
) |
Add an isochronous endpoint to alternate setting interface.
- Parameters
-
config_nbr
Configuration number. if_nbr
Interface number. if_alt_nbr
Interface alternate setting number. dir_in
Endpoint Direction : - true, IN direction.
- false, OUT direction.
attrib
Isochronous endpoint synchronization and usage type attributes. max_pkt_len
Endpoint maximum packet length (see Note #1). transaction_frame
Endpoint transactions per (micro)frame (see Note #2). interval
Endpoint interval in frames or microframes. p_ep_addr
Pointer to a variable that will receive the new endpoint address. The variable will be set to endpoint address if no errors are returned, otherwise it will be set to SL_USBD_ENDPOINT_ADDR_NONE.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) If the 'max_pkt_len' argument is '0', the stack allocates the first available ISOCHRONOUS endpoint regardless of its maximum packet size.
- (2) For full-speed endpoints, 'transaction_frame' must be set to 1 since there is no support for high-bandwidth endpoints.
- (3) For full-/high-speed isochronous endpoints, bInterval value must be in the range from 1 to 16. The bInterval value is used as the exponent for a 2^(bInterval-1) value. Maximum polling interval value is 2^(16-1) = 32768 frames in full-speed and 32768 microframes (i.e., 4096 frames) in high-speed.
Receive data on an isochronous OUT endpoint asynchronously.
- Parameters
-
ep_addr
Endpoint address. p_buf
Pointer to the destination buffer to receive data (see Note #1). buf_len
Number of octets to receive. async_fnct
Function that will be invoked upon completion of a receive operation. p_async_arg
Pointer to the argument that will be passed as parameter of 'async_fnct'.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) Receive buffer must be 32 bits aligned.
Send data on an isochronous IN endpoint asynchronously.
- Parameters
-
ep_addr
Endpoint address. p_buf
Pointer to the buffer of data that will be transmitted (see Note #1). buf_len
Number of octets to transmit. async_fnct
Function that will be invoked upon completion of transmit operation. p_async_arg
Pointer to the argument that will be passed as parameter of 'async_fnct'.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) Transmit buffer must be 32 bits aligned.
Set synchronization feedback rate on synchronization isochronous endpoint.
- Parameters
-
config_nbr
Configuration number. if_nbr
Interface number. if_alt_nbr
Interface alternate setting number. synch_ep_addr
Synchronization endpoint address. sync_refresh
Exponent of synchronization feedback rate (see Note #3).
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) Synchronization endpoints can ONLY be associated when the device is in the following states:
- SL_USBD_DEVICE_STATE_NONE Device controller has not been initialized.
- SL_USBD_DEVICE_STATE_INIT Device controller is already initialized.
- (2) For audio class 1.0, the interface class code must be SL_USBD_CLASS_CODE_AUDIO and protocol 'zero'
- (3) If explicit synchronization mechanism is needed to maintain synchronization during transfers, the information carried over the synchronization path must be available every 2 ^ (10 - P) frames, with P ranging from 1 to 9 (512 ms down to 2 ms).
- (4) Table 4-22 "Standard AS Isochronous Synch Endpoint Descriptor" of Audio 1.0 specification indicates for bmAttributes field no usage type for bits 5..4. But USB 2.0 specification, Table 9-13 "Standard Endpoint Descriptor" indicates several types of usage. When an explicit feedback is defined for a asynchronous isochronous endpoint, the associated synch feedback should use the Usage type 'Feedback endpoint'.
Associate synchronization endpoint to isochronous endpoint.
- Parameters
-
config_nbr
Configuration number. if_nbr
Interface number. if_alt_nbr
Interface alternate setting number. data_ep_addr
Data endpoint address. sync_addr
Associated synchronization endpoint.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) Synchronization endpoints can ONLY be associated when the device is in the following states:
- SL_USBD_DEVICE_STATE_NONE Device controller has not been initialized.
- SL_USBD_DEVICE_STATE_INIT Device controller is already initialized.
- (2) For audio class 1.0, interface class code must be SL_USBD_CLASS_CODE_AUDIO and protocol 'zero'.
Send zero-length packet to the host.
- Parameters
-
ep_addr
Endpoint address. timeout_ms
Timeout in milliseconds.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) This function should only be called during a synchronous transfer.
◆ sl_usbd_core_endpoint_read_zlp()
sl_status_t sl_usbd_core_endpoint_read_zlp | ( | uint8_t | ep_addr, |
uint16_t | timeout_ms |
||
) |
Receive zero-length packet from the host.
- Parameters
-
ep_addr
Endpoint address. timeout_ms
Timeout in milliseconds.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) This function should only be called during a synchronous transfer.
◆ sl_usbd_core_abort_endpoint()
sl_status_t sl_usbd_core_abort_endpoint | ( | uint8_t | ep_addr | ) |
Abort I/O transfer on the endpoint.
- Parameters
-
ep_addr
Endpoint address.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_core_endpoint_read_complete()
sl_status_t sl_usbd_core_endpoint_read_complete | ( | uint8_t | ep_log_nbr | ) |
Notify USB stack that packet receive has completed.
- Parameters
-
ep_log_nbr
Endpoint logical number.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_core_endpoint_write_complete()
sl_status_t sl_usbd_core_endpoint_write_complete | ( | uint8_t | ep_log_nbr | ) |
Notify USB stack that packet transmit has completed.
- Parameters
-
ep_log_nbr
Endpoint logical number.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_core_endpoint_write_complete_extended()
sl_status_t sl_usbd_core_endpoint_write_complete_extended | ( | uint8_t | ep_log_nbr, |
sl_status_t | xfer_err |
||
) |
Notify USB stack that packet transmit has completed (see Note #1).
- Parameters
-
ep_log_nbr
Endpoint logical number. xfer_err
Error code returned by the USB driver.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
- Note
- (1) This function is an alternative to the function sl_usbd_core_endpoint_write_complete() so that a USB device driver can return to the core an error code upon the Tx transfer completion.
◆ sl_usbd_core_stall_endpoint()
sl_status_t sl_usbd_core_stall_endpoint | ( | uint8_t | ep_addr, |
bool | state |
||
) |
Stall the non-control endpoint.
- Parameters
-
ep_addr
Endpoint address. state
Endpoint stall state.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_core_is_endpoint_stalled()
sl_status_t sl_usbd_core_is_endpoint_stalled | ( | uint8_t | ep_addr, |
bool * | p_ep_stall |
||
) |
Get the stall status of a non-control endpoint.
- Parameters
-
ep_addr
Endpoint address. p_ep_stall
Pointer to a boolean that will receive the endpoint stalled status. The boolean variable is set to true if endpoint is stalled, or is set to false if endpoint is not stalled.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_core_get_max_endpoint_packet_size()
sl_status_t sl_usbd_core_get_max_endpoint_packet_size | ( | uint8_t | ep_addr, |
uint16_t * | p_max_size |
||
) |
Retrieve the endpoint maximum packet size.
- Parameters
-
ep_addr
Endpoint address. p_max_size
Pointer to a variable that will receive the maximum packet size upon return. The variable is set to the maximum packet size if no errors are returned, otherwise it is set to 0.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
◆ sl_usbd_core_get_max_phy_endpoint_number()
sl_status_t sl_usbd_core_get_max_phy_endpoint_number | ( | uint8_t * | p_ep_phy_nbr | ) |
Get the maximum physical endpoint number.
- Parameters
-
p_ep_phy_nbr
Pointer to variable where maximum physical endpoint number will be returned. If no errors are returned, the variable will be set to maximum physical endpoint number, otherwise it will be set to SL_USBD_ENDPOINT_PHY_NONE.
- Returns
- Returns SL_STATUS_OK on success or another SL_STATUS code on failure.
Macro Definition Documentation
◆ SL_USBD_FRAME_NBR_MAX
#define SL_USBD_FRAME_NBR_MAX 2047u |
FRAME
Note(s) : (1) Section 8.3.3 of USB spec 2.0 describes the frame number as: "The frame number field is an 11-bit field that is incremented by the host on a per-frame basis. The frame number field rolls over upon reaching its maximum value of 7FFH and is sent only in SOF tokens at the start of each (micro)frame."
◆ SL_USBD_REQ_DIR_MASK
#define SL_USBD_REQ_DIR_MASK 0x80u |
REQUEST CHARACTERISTICS
Note(s) : (1) Request types are defined in USB spec 2.0, section 9.3, Table 9-2, 'RequestType' field.
◆ SL_USBD_REQ_GET_STATUS
#define SL_USBD_REQ_GET_STATUS 0u |
STANDARD REQUESTS
Note(s) : (1) Request types are defined in USB spec 2.0, section 9.4, Table 9-4, 'RequestType' field.
◆ SL_USBD_DESC_TYPE_DEVICE
#define SL_USBD_DESC_TYPE_DEVICE 1u |
DESCRIPTOR TYPES
Note(s) : (1) Descriptors types are defined in the USB spec 2.0 section 9.2.6, Table 9-5.
◆ SL_USBD_LANG_ID_ARABIC_SAUDI_ARABIA
#define SL_USBD_LANG_ID_ARABIC_SAUDI_ARABIA 0x0401u |
LANGUAGE IDENTIFIERS
Note(s) : (1) Languages identifier are defined in "http://www.usb.org/developers/docs/USB_LANGIDs.pdf".
◆ SL_USBD_CLASS_CODE_USE_IF_DESC
#define SL_USBD_CLASS_CODE_USE_IF_DESC 0x00u |
CLASS CODES
Note(s) : (1) Class codes are defined in "http://www.usb.org/developers/defined_class".
(2) Class code information can be placed in the Device descriptor or in the Interface descriptor. Some defined class code are allowed to be used only in the Device descriptor, others can used in both Device and Interface descriptors and come can only be used in Interface Descriptors. (3) Subclass & protocol codes are defined in the relevant class drivers.
◆ SL_USBD_FRAME_NBR_DIFF_GET
#define SL_USBD_FRAME_NBR_DIFF_GET | ( | frame_nbr1, |
|
frame_nbr2 |
|||
) |
◆ SL_USBD_ENDPOINT_PHY_TO_ADDR
#define SL_USBD_ENDPOINT_PHY_TO_ADDR | ( | ep_phy_nbr | ) |
◆ SL_USBD_ENDPOINT_ADDR_TO_PHY
#define SL_USBD_ENDPOINT_ADDR_TO_PHY | ( | ep_addr | ) |
Enumeration Type Documentation
◆ sl_usbd_device_speed_t
USB DEVICE SPEED DATA TYPE
- Note
- (1) 'Universal Serial Bus Specification Rev 2.0', section 4.2.1 defines three data rates:
- (a) The USB Low-Speed (LS) signaling bit rate is 1.5 Mb/s.
- (b) The USB Full-Speed (FS) signaling bit rate is 12 Mb/s.
- (c) The USB High-Speed (HS) signaling bit rate is 480 Mb/s.
Enumerator | |
---|---|
SL_USBD_DEVICE_SPEED_LOW | Low-Speed (see Note #1a). |
SL_USBD_DEVICE_SPEED_FULL | Full-Speed (see Note #1b). |
SL_USBD_DEVICE_SPEED_HIGH | High-Speed (see Note #1c). |
◆ sl_usbd_device_state_t
USB DEVICE STATES DATA TYPE
- Note
- (1) 'Universal Serial Bus Specification Rev 2.0', section 9.1.1 defines seven visible device states:
- (a) SL_USBD_DEVICE_STATE_INIT : Device is not attached to the USB.
- (b) SL_USBD_DEVICE_STATE_ATTACHED : Device is attached to the USB, but not powered.
- (c) USBD_DEV_STATE_POWERED : Device is attached to the USB and powered, but has not been reset.
- (d) SL_USBD_DEVICE_STATE_DEFAULT : Device is attached to the USB and powered and has been reset, but has not been assigned a unique address. Device responds at the default address.
- (e) SL_USBD_DEVICE_STATE_ADDRESSED : Device is attached to the USB, powered, has been reset, and a unique device address has been assigned. Device is not configured.
- (f) SL_USBD_DEVICE_STATE_CONFIGURED : Device is attached to the USB, powered, has been reset, has a unique address, is configured, and is not suspended. The host may now use the function provided by the device.
- (g) SL_USBD_DEVICE_STATE_SUSPENDED : Device is, at minimum, attached to the USB and is powered and has not seen bus activity for 3 ms. It may also have a unique address and be configured for use. However, because the device is suspended, the host may not use the device's function.
- (2) An additional state is added (USBD_DEV_STATE_START) to determine if the device controller has been initialized.
◆ sl_usbd_config_event_t
CONFIG EVENT DATA TYPE.