sl_usbd_cdc_subclass_driver_t Struct Reference
CDC Subclass Driver.
#include <sl_usbd_class_cdc.h>
Data Fields | |
void(* | enable )(void *p_subclass_arg) |
Callback for enable event. | |
void(* | disable )(void *p_subclass_arg) |
Callback for disable event. | |
bool(* | mgmt_req )(const sl_usbd_setup_req_t *p_setup_req, void *p_subclass_arg) |
Callback to handle management requests. | |
void(* | notify_cmpl )(void *p_subclass_arg) |
Callback to handle notification completion. | |
void(* | fnct_descriptor )(void *p_subclass_arg, uint8_t first_dci_if_nbr) |
Callback to build functional desc. | |
uint16_t(* | fnct_get_descriptor_size )(void *p_subclass_arg) |
Callback to get the size of the functional desc. |
CDC Subclass Driver.
Field Documentation
◆ enable
void(* sl_usbd_cdc_subclass_driver_t::enable) (void *p_subclass_arg) |
Callback for enable event.
◆ disable
void(* sl_usbd_cdc_subclass_driver_t::disable) (void *p_subclass_arg) |
Callback for disable event.
◆ mgmt_req
bool(* sl_usbd_cdc_subclass_driver_t::mgmt_req) (const sl_usbd_setup_req_t *p_setup_req, void *p_subclass_arg) |
Callback to handle management requests.
◆ notify_cmpl
void(* sl_usbd_cdc_subclass_driver_t::notify_cmpl) (void *p_subclass_arg) |
Callback to handle notification completion.
◆ fnct_descriptor
void(* sl_usbd_cdc_subclass_driver_t::fnct_descriptor) (void *p_subclass_arg, uint8_t first_dci_if_nbr) |
Callback to build functional desc.
◆ fnct_get_descriptor_size
uint16_t(* sl_usbd_cdc_subclass_driver_t::fnct_get_descriptor_size) (void *p_subclass_arg) |
Callback to get the size of the functional desc.