Introduction#

This guide provides detailed and comprehensive instructions for setting up the SiWT917 Single Band Wi-Fi + Bluetooth Low Energy Development Kit using a Raspberry Pi board.

The primary goal is to enable Wi-Fi functionality on the development kit. The guide includes step-by-step procedures for flashing the RPI4 OS image onto the Raspberry Pi, ensuring that the operating system is correctly installed and ready for use.

Additionally, it covers the configuration of the SiWT917 in Wi-Fi Station (STA) mode, which allows the device to connect to a Wi-Fi router. This setup enables seamless wireless communication and enhances the overall functionality of the development kit.