Appendix C: Troubleshooting#
Make sure the third-party AP is up while connecting to it. Also make sure to add the valid credentials depending on security type in the
<system_path>/SiWT917.x.x.x.x/release/sta_settings.conffile while running the supplicant.Make sure that the AP should be brought in same channel in which the STA is connected to the third-party AP.