Prerequisites#
Following are the details for the prerequisties required for both hardware and software.
Hardware#
Following are the details for hardware requirements.
| S.N. | Hardware Components | Quantity | Description |
|---|---|---|---|
| 1. |
SiWT917 RCP Wi-Fi 6 Single Band + BLE 5.4 Wireless Radio.
Radio board: BRD4346A Adapter board: BRD8045B |
1 |
|
| 2. | PC/Laptop/Embedded Platform with Linux OS | 1 | Raspberry Pi 4 with SiWT917 RPi image |
| 3. | Standard WLAN Access Point | 1 | For example, TP-Link AX1500 Wi-Fi 6 Router |
| 4. | Third party Station | 1 | Note: Use third-party stations such as phones, tablets, PCs, or laptops capable of connecting to Wi-Fi 6 access points. Example: OnePlus Nord mobile was used for this test. |
| 5. | Monitor, mouse, and keyboard | 1 | To access the console or UI of Raspberry Pi 4 |
| 6. | Ethernet/H0DMI cables | 1 | To connect Raspberry Pi 4 with the monitor |
Note: For more information, follow the: Getting Started Guide.
Software#
Following are the details for software requirements.
| S.N. | Software Components | Description |
|---|---|---|
| 1. | SiWT917 RCP Driver | si91x-rcp-driver |
| 2. | Kernel Version from 3.18 to 6.1 | For example, in this test case, the system's kernel version is 6.1. |
| 3. | wpa supplicant | For example, wpa_supplicant 2.10. |
| 4. | hostapd |
Note:
Command: apt install hostapd |