Prerequisites#
Readers of this document are expected to be familiar with the Standard WLAN AP configuration, iperf tools, IP addressing, and DHCP.
Hardware#
Following are the details for hardware requirements.
| S.N. | Hardware Components | Quantity | Description |
|---|---|---|---|
| 1. |
SiWT917 RCP Wi-Fi 6 Single Band + BLE 5.4 Wireless Radio.
Radio boards: BRD4346A Adapter board: BRD8045B |
1 |
|
| 2. | PC/Laptop/Embedded Platform with Linux OS | 2 |
|
| 3. | Standard WLAN Access Point | 1 | To connect with Raspberry Pi 4 |
| 4. | Monitor, mouse, and keyboard | 1 | To connect Raspberry Pi 4 with the monitor |
| 5. | Ethernet/HDMI cables | 1 | ASUS TUF Gaming AX5400 Dual-band Wi-Fi 6 |
Note: For more information, refer to Getting Started Guide.
Software#
Following are the details for software requirements.
S.N. | Software Components | Description |
|---|---|---|
1. | SiWT917 RCP Driver | |
2. | Kernel Version from 3.18 to 6.1 | For example, In this test case, the system's kernel version is 6.1 |
3. | For example, wpa_supplicant 2.10. | |
4. | Measurement Tool - iperf | Refer to the section Configure iperf and test. |