Wi-Fi Commander Tool Overview#
Introduction#
The Wi-Fi Commander tool provides a command-line interface for configuring, controlling, and validating Wi-Fi functionality on Silicon Labs devices. It is designed to support developers during bring-up, testing, debugging, and automation workflows by exposing commonly used Wi-Fi operations through a structured command set.
The tool enables users to interact with Wi-Fi features without requiring custom application code for every operation. It provides a consistent interface for executing commands, inspecting device state, and validating connectivity behavior during development.
Key Features#
The Wi-Fi Commander tool supports high-level control of Wi-Fi functionality, including:
Device and interface initialization
Wi-Fi scanning and network discovery
Connection and disconnection management
Access point (AP) and station mode configuration
Network parameter configuration
Security and credential management
Status reporting and diagnostics
Basic connectivity validation
Scriptable command execution for testing and automation workflows
The available command set may vary depending on the device, firmware version, software development kit (SDK) version, and enabled feature set.
Intended Use Cases#
The Wi-Fi Commander tool is intended for the following use cases:
Bringing up Wi-Fi functionality on supported Silicon Labs platforms
Validating Wi-Fi behavior during development
Running repeatable test sequences from scripts
Debugging connection, configuration, and network discovery issues
Demonstrating Wi-Fi features without writing additional application code
Supporting engineering, QA, and field troubleshooting workflows
Scope#
This documentation describes the purpose, supported usage model, and high-level capabilities of the Wi-Fi Commander tool. It provides guidance on how the tool is used, the feature areas it covers, and its role within the Silicon Labs Wi-Fi development workflow.
The scope of this documentation includes:
Overview of the Wi-Fi Commander tool
Supported feature categories
Command usage concepts
Typical workflows
Expected inputs and outputs
Tool limitations and assumptions
References to related Silicon Labs documentation, where applicable
Out of Scope#
This documentation does not provide a detailed explanation of Wi-Fi protocol behavior, radio frequency (RF) theory, or low-level driver implementation details. It also does not replace product-specific datasheets, SDK documentation, security guidance, or certification documentation.
The following topics are considered out of scope:
Detailed IEEE 802.11 protocol descriptions
Hardware design guidelines
RF performance tuning
Regulatory certification procedures
Internal firmware architecture
Complete API reference documentation for underlying Wi-Fi libraries
Platform-specific bring-up procedures not directly related to the Wi-Fi Commander tool
Audience#
This documentation is intended for embedded software developers, validation engineers, field application engineers (FAEs), and other technical users who need to configure, test, or debug Wi-Fi functionality on Silicon Labs platforms.
Users are expected to have a basic understanding of embedded development workflows, command-line tools, and general Wi-Fi networking concepts.
Limitations#
The Wi-Fi Commander tool is intended primarily for development, validation, and diagnostic workflows. It may not expose every Wi-Fi capability supported by the underlying device or SDK.
Feature availability can depend on:
Device family
Firmware configuration
SDK version
Build-time feature flags
Security mode support
Network environment
Host platform support
For product development, verify final behavior using the target application and production firmware configuration.
Compatibility with WiseConnect#
Wi-Fi Commander version v1.x.x is compatible with WiseConnect v3.5.0 and Trusted Application (TA) version 2.14.5.
Relationship to Other Tools and Documentation#
The Wi-Fi Commander tool is one part of the Silicon Labs Wi-Fi development workflow. Use it together with the relevant SDK documentation, example applications, API references, release notes, and device-specific documentation.
When a command or feature depends on platform-specific behavior, refer to the corresponding Silicon Labs documentation for the target device and SDK version.
Summary#
The Wi-Fi Commander tool provides a practical, command-driven interface for exercising Wi-Fi functionality on Silicon Labs devices. It helps simplify development, validation, and debugging by enabling users to perform common Wi-Fi operations from a consistent command-line environment.
This overview defines the tool's purpose, intended usage, and documentation scope. Detailed command descriptions, examples, and workflow-specific guidance are provided in the following sections.