Wi-Fi Memory Calculator#

The Wi-Fi Memory Calculator is a configuration-analysis tool included in Simplicity Studio v6.

Use this tool to evaluate and validate combinations of Wi-Fi stack features before building firmware.

This calculator helps you understand how selected features affect memory usage and whether a configuration is supported on the target device.

You can use the Wi-Fi Memory Calculator to:

  • Enable or disable SiWx917 features

  • Automatically resolve feature dependencies

  • View memory consumption in real time (RAM and ROM)

  • Determine the feasibility for the target device

OverviewOverview

Practical Use Cases#

Use the Wi-Fi Memory Calculator to:

  • Validate the feasibility of a planned feature set

  • Optimize memory usage

  • Plan and compare feature configurations before firmware development

Key Advantages#

The Wi-Fi Memory Calculator provides the following benefits:

  • Does not require hardware

  • Does not require a firmware build

  • Provides immediate feedback as features are selected

  • Allows safe experimentation

Prerequisites#

Software#

  • Simplicity Studio v6 (Full Install)