BLE Gain Table#
To program region-based maximum power for the BLE device, follow the steps below.
See the Region-based Maximum Power section for more details.
Compile and insert the driver as described in the Compilation Steps and Installing the Driver sections.
Navigate to the rsi/release folder.
Run the following command:
# ./bt_ble_gain_table_update <protocol ID>For example:
# ./bt_ble_gain_table_update 0In this case, 0 is the Protocol ID value for BLE.
The commands above start the table programming and should display the following logs.
******************Successfully completed programming n gain tables*****************In this case,
nis the number of structures given in wlan_gain_table.txt file.Below is the reference Gain table structure format while updating the file
//!************************************************************ //! INSTRUCTIONS SHOULD BE FOLLOWED TO EDIT BELOW GAIN TABLES: //!************************************************************ //! 1. Each value should be seperated by ',' and space characters. //! 2. Multi-line comments not supported. (e.g. /* comment */) //! 3. A space before comment is needed, for inline comments. (e.g. <Data> //<Comment>) //! 4. Hexadecimal numbers not supported. //! 5. No space between value and ',' character. //! 6. Max power gain table with size more than 10 bytes is not supported. //! 6. Offset gain table with size more than 128 bytes is not supported. //! 7. Supported table names and their maximum supported size are //! For BLE Max Power Table --- RS9116_BLE_REGION_BASED_MAXPOWER_XX MAX_LENGTH = 10 //! For BLE Offset Table --- RS9116_BLE_REGION_BASED_MAXPOWER_VS_OFFSET_XX MAX_LENGTH = 128 //! NOTE: No support for other table names. //! 8. Update above mentioned respected generic tables with the required data //! 9. Max Power Gain table Format: //! <TABLE NAME>[] = { //<COMMENTS if any> //! <REGION NAME 1>, <MAX POWER>, //! <REGION NAME 2>, <MAX POWER>, //! . //! . //! <REGION NAME N>, <MAX POWER>, //! }; //<COMMENTS if any> //! //! 10. Offset Gain table Format: //! <TABLE NAME>[] = { //<COMMENTS if any> //! <NO.of Regions>, //! <REGION NAME 1>, <NO.OF CHANNELS IN THIS REGION>, //! <CHANNEL NUMBER 1>, <TX POWER OFFSET FOR PHY RATE = 1M>, <TX POWER OFFSET FOR PHY RATE = 2M>, <TX POWER OFFSET FOR PHY RATE = 125kbps>, <TX POWER OFFSET FOR PHY RATE = 500kbps>, //! <CHANNEL NUMBER 2>, <TX POWER OFFSET FOR PHY RATE = 1M>, <TX POWER OFFSET FOR PHY RATE = 2M>, <TX POWER OFFSET FOR PHY RATE = 125kbps>, <TX POWER OFFSET FOR PHY RATE = 500kbps>, //! . //! . //! <CHANNEL NUMBER m-1>, <TX POWER OFFSET FOR PHY RATE = 1M>, <TX POWER OFFSET FOR PHY RATE = 2M>, <TX POWER OFFSET FOR PHY RATE = 125kbps>, <TX POWER OFFSET FOR PHY RATE = 500kbps>, //! <CHANNEL NUMBER m>, <TX POWER OFFSET FOR PHY RATE = 1M>, <TX POWER OFFSET FOR PHY RATE = 2M>, <TX POWER OFFSET FOR PHY RATE = 125kbps>, <TX POWER OFFSET FOR PHY RATE = 500kbps>, //! <REGION NAME 2>, <NO.OF CHANNELS IN THIS REGION>, //! <CHANNEL NUMBER 1>, <TX POWER OFFSET FOR PHY RATE = 1M>, <TX POWER OFFSET FOR PHY RATE = 2M>, <TX POWER OFFSET FOR PHY RATE = 125kbps>, <TX POWER OFFSET FOR PHY RATE = 500kbps>, //! <CHANNEL NUMBER 2>, <TX POWER OFFSET FOR PHY RATE = 1M>, <TX POWER OFFSET FOR PHY RATE = 2M>, <TX POWER OFFSET FOR PHY RATE = 125kbps>, <TX POWER OFFSET FOR PHY RATE = 500kbps>, //! . //! . //! <CHANNEL NUMBER m-1>, <TX POWER OFFSET FOR PHY RATE = 1M>, <TX POWER OFFSET FOR PHY RATE = 2M>, <TX POWER OFFSET FOR PHY RATE = 125kbps>, <TX POWER OFFSET FOR PHY RATE = 500kbps>, //! <CHANNEL NUMBER m>, <TX POWER OFFSET FOR PHY RATE = 1M>, <TX POWER OFFSET FOR PHY RATE = 2M>, <TX POWER OFFSET FOR PHY RATE = 125kbps>, <TX POWER OFFSET FOR PHY RATE = 500kbps>, //! <REGION NAME 3>, <NO.OF CHANNELS IN THIS REGION>, //! . //! . //! <REGION NAME y>, <NO.OF CHANNELS IN THIS REGION>, //! }; //<COMMENTS if any> //! 11. Supported Region names: //! FCC, ETSI, TELEC, WORLDWIDE, KCC //! For example: RS9116_BLE_REGION_BASED_MAXPOWER_XX[] = { // REGION_NAME MAX_POWER FCC, 16, ETSI, 8, TELEC, 10, WORLDWIDE, 16, KCC, 10, }; RS9116_BLE_REGION_BASED_MAXPOWER_VS_OFFSET_XX[] = { 5, //NUM_OF_REGIONS FCC, 4, //NUM_OF_CHANNELS //chan_num 1M 2M 125 kbps 500 kbps 255, 0, 0, 6, 0, 0, 0, 0, 6, 0, 38, 0, 2, 6, 0, 39, 0, 16, 6, 0, ETSI, 4, //NUM_OF_CHANNELS //chan_num 1M 2M 125 kbps 500 kbps 255, 0, 0, 0, 0, 0, 0, 0, 0, 0, 19, 0, 0, 0, 0, 39, 0, 0, 0, 0, TELEC, 4, //NUM_OF_CHANNELS //chan_num 1M 2M 125 kbps 500 kbps 255, 0, 0, 0, 0, 0, 0, 0, 0, 0, 19, 0, 0, 0, 0, 39, 0, 0, 0, 0, WORLDWIDE, 4, //NUM_OF_CHANNELS //chan_num 1M 2M 125 kbps 500 kbps 255, 0, 0, 0, 0, 0, 0, 0, 0, 0, 19, 0, 0, 0, 0, 39, 0, 0, 0, 0, KCC, 4, //NUM_OF_CHANNELS //chan_num 1M 2M 125 kbps 500 kbps 255, 0, 0, 0, 0, 0, 0, 0, 0, 0, 19, 0, 0, 0, 0, 39, 0, 0, 0, 0, };