BLE PER Mode#
SiWx91x RCP Driver Supports BLE PER Mode Transmit and Receive functionality. Follow the steps below to verify both functionalities.
Follow the Compilation Steps in the above section and compile the driver as follows.
# make clean; makeNavigate to the release folder and run the following command to set the driver to PER mode:
# cd release # insmod rsi_91x.ko dev_oper_mode=8 driver_mode_value=2 rsi_zone_enabled=0x601 # insmod rsi_sdio.ko sdio_clock=50
BLE PER Transmit#
Run the following command to check the BLE PER transmit:
# ./ble_transmit <Access_Addr> <pkt_length> <ble_rate> <rx_channel_index><tx_channel_index> <scrambler_seed> <no_of_packets> <payload_type><le_channel_type> <tx_power_index> <tx_mode> <hopping_type> <ant_sel><inter_pkt_gap> <pll_mode> <rf_type> <rf_chain>
Description of each field:
SI No | Parameters | Description | Values |
|---|---|---|---|
1 | Access Address | It is a 32-bit address in hexadecimal format | 00112233 |
2 | pkt_length | Length of the packet, in bytes, to be transmitted. | |
3 | ble_rate | 1Mbps - 1 ,2Mbps - 2 , 125Kbps - 4, 500Kbps - 8 | |
4 | rx_channel_index | Receive channel index, as per the Bluetooth standard | 0 to 39 |
5 | tx_channel_index | Transmit channel index, as per the Bluetooth standard. | 0 to 39 |
6 | scrambler_seed | Initial seed to be used for whitening. It should be set to ‘0’ in order to disable whitening. In order toenable the whitening scrambler seed should be given, which is used on the receive side. | |
7 | no_of_packets | Number of packets to be transmitted | It is valid only when the is set to Burst mode. |
8 | payload_type | Type of payload to be transmitted | ‘0’ – Payload consists of all zeros ‘1’ – Payload consists of all 0xFF’s ‘2’ – Payload consists of all 0x55’s ‘3’ – Payload consists of all 0xF0’s |
9 | le_channel_type | advertising channel - 0 data channel - 1 | |
10 | tx_power_index | This field corresponds to the transmit power index,The range for tx_power_index is 1 to 63(0 and 32 are invalid) | - If rf_chain is BT_HP_CHAIN o 1 -12 BLE HP Mode o 127 magic number for selecting maximum possible power output - If rf_chain is BT_LP_CHAIN o 1 - 31 BLE- 0 dBm mode o 33 - 63 BLE- 10 dBm Mode |
11 | tx_mode | Burst mode - 0 Continuous mode - 1 | |
12 | hopping_type | no hopping -0 fixed hopping - 1 random hopping - 2 | |
13 | ant_sel | onchip antenna - 2 u.f.l - 3 | |
14 | inter_pkt_gap | Number of slots to be skipped between two packets - Each slot will be 1250usec | |
15 | pll_mode | PLL_MODE0 – 0 PLL_MODE1 – 1 PLL_MODE2 – 2 | |
16 | rf_chain | WLAN_HP_CHAIN - 0 BT_HP_CHAIN - 2 BT_LP_CHAIN - 3 |
Example
Continuous Mode :
#./ble_transmit 71764129 250 1 38 38 2 0 0 1 10 1 0 3 0 0 1 3
Transmit a BLE-1Mbps advertising packet with access address of 0x71764129 and packet length of 250 bytes on 2478 MHz with the following parameters. Access_Addr - 71764129 pkt_length - 250 ble_rate -1 rx_channel_index -38 tx_channel_index -38 scrambler_seed - 2 no_of_packets - 0 payload_type - 0 le_channel_type -1 tx_power_index -10 tx_mode - 1 hopping_type - 0 ant_sel -3 inter_pkt_gap -0 pll_mode -0 rf_type - 1 rf_chain - 3
Burst Mode:
#./ble_transmit 71764129 250 1 38 38 0 0 0 1 10 0 0 3 0 0 1 3
Transmit a BLE-1Mbps advertising packet with access address of 0x71764129 and packet length of 250 bytes on 247 8MHz with the following parameters. Access_Addr - 71764129 pkt_length - 250 ble_rate - 1 rx_channel_index -38 tx_channel_index -38 scrambler_seed - 0 no_of_packets - 0 payload_type - 0 le_channel_type -1 tx_power_index - 10 tx_mode - 0 hopping_type - 0 ant_sel -3 inter_pkt_gap -0 pll_mode -0 rf_type - 1 rf_chain - 3
Run the following command to stop BLE PER transmit:
#./ble_transmit 0
BLE PER Receive#
Run the following command to keep the device in BLE PER receive mode:
#./ble_receive <access_addr> <data_legth_indication> <scrambler_seed> <ble_rate> <rx_channel_index> <tx_channel_index> <le_channel_type> <hopping_type> <ant_sel> <loop_back_mode><pwrsave_options> <pll_mode> <rf_type> <rf_chain>
Description of each field:
SI No | Parameters | Description | Values |
|---|---|---|---|
1 | Access Address | It is a 32-bit address in hexadecimal format | 00112233 |
2 | data_length_ind ication | 0 – Disable(37 Bytes) 1 –Enable(255 Bytes) | |
3 | scrambler_seed | Initial seed to be used for whitening. It should be set to ‘0’ in order to disable whitening. | |
4 | ble_rate | 1Mbps - 1 , 2Mbps - 2 , Long Range(LR) - 4 | |
5 | rx_channel_index | Receive channel index, as per the Bluetooth standard | 0 to 39 |
6 | tx_channel_index | Transmit channel index, as per the Bluetooth standard | 0 to 39 |
7 | le_channel_type | advertising channel – 0 data channel – 1 | |
8 | hopping_type | no hopping -0 fixed hopping - 1 random hopping - 2 | |
9 | ant_sel | onchip antenna - 2 u.f.l – 3 | |
10 | oop_back_mode | Disable – 0 Enable – 1 | |
11 | pwrsave_options | Disable – 0 Enable – 1 | |
12 | pll_mode | PLL_MODE0 – 0 PLL_MODE1 – 1 PLL_MODE2 – 2 | |
13 | rf_type | External RF – 0 Internal RF – 1 | |
14 | rf_chain | WLAN_HP_CHAIN - 0 WLAN_LP_CHAIN - 1 BT_HP_CHAIN - 2 BT_LP_CHAIN - 3 |
Example
#./ble_receive 71764129 0 0 1 37 37 0 0 3 0 0 0 1 3
Receive a BLE-1 Mbps advertising packet with 0x71764129 access address and 250byte packet length on 2478 MHz with the following parameters. scrambler_seed : 0 hopping_type: disable ant_sel : u.f.l loop_back_mode : Disabled pwrsave_options : Disabled pll_mode : PLL_MODE0 rf_type : Internal RF rf_chain: BT_LP_CHAIN
To get the receive stats, run the following command:
#./bt_util bt_stats <file name > < Number of Pkt> Ex: #./bt_util bt_stats aa 0
The following command can be given to stop the reception.
#./ble_receive 0