Using the hciconfig and hcitool Commands#
The hcitool and hciconfig commands are used to control and configure parameters for the Bluetooth interface. The most frequently used HCI commands are explained here. For other HCI commands, see the Bluetooth specification, Volume 2, Part E, Chapter 7, from www.bluetooth.org.
Reset  | |
|---|---|
Description  | This command is used to issue a soft reset to the Bluetooth module  | 
Default Value  | -  | 
Input Parameters  | None  | 
Output Parameter  | None  | 
Reset Required  | No.  | 
Usage  | hcitool -i <hciX> cmd 0x03 0x03  | 
Read Local Version Information  | |
|---|---|
Description  | This command is used to read the local version information  | 
Default Value  | -  | 
Input Parameters  | None  | 
Output Parameter  | Run the   | 
Reset Required  | No.  | 
Usage  | hcitool -i <hciX> cmd 0x04 0x01  | 
Read Local Supported Commands  | |
|---|---|
Description  | This command is used to read the local controller supported HCI commands.  | 
Default Value  | -  | 
Input Parameters  | None  | 
Output Parameter  | List of supported commands (64 bytes of bit field)  | 
Reset Required  | No.  | 
Usage  | hcitool -i <hciX> cmd 0x04 0x02  | 
Get Local BD Address  | |
|---|---|
Description  | This command is used to get the local BD Address  | 
Default Value  | -  | 
Input Parameters  | None  | 
Output Parameter  | 6 Byte BD Address  | 
Reset Required  | No.  | 
Usage  | hcitool -i <hciX> cmd 0x04 0x09  | 
List of supported HCI commands#
For OGF 0x02#
HCI Commands(OCF)  | Supported  | Comments(Macro's Defined in the source code)  | 
|---|---|---|
HCI_Hold_Mode  | Yes  | /* HCI link policy command OCF types */HCI_OP_HOLD_MODE  | 
HCI_Sniff_Mode  | Yes  | HCI_OP_SNIFF_MODE  | 
HCI_Exit_Sniff_Mode  | Yes  | HCI_OP_EXIT_SNIFF_MODE  | 
HCI_QoS_Setup  | Yes  | HCI_OP_QOS_SETUP  | 
HCI_Role_Discovery  | Yes  | HCI_OP_ROLE_DISCOVERY  | 
HCI_Switch_Role  | Yes  | HCI_OP_SWITCH_ROLE  | 
HCI_Read_Link_Policy_Settings  | Yes  | HCI_OP_READ_LINK_POLICY  | 
HCI_Write_Link_Policy_Settings  | Yes  | HCI_OP_WRITE_LINK_POLICY  | 
HCI_Read_Default_Link_Policy_Settings  | Yes  | HCI_OP_READ_DEF_LINK_POLICY  | 
HCI_Write_Default_Link_Policy_Settings  | Yes  | HCI_OP_WRITE_DEF_LINK_POLICY  | 
HCI_Flow_Specification  | Yes  | HCI_OP_FLOW_SPECIFICATION  | 
HCI_Sniff_Subrating  | Yes  | HCI_OP_SNIFF_SUBRATING  | 
For OGF 0x03#
HCI Commands(OCF)  | Supported  | Comments(Macro's Defined in the source code)  | 
|---|---|---|
HCI_Set_Event_Mask  | Yes  | HCI_OP_SET_EVENT_MASK  | 
For OGF 0x04#
HCI Commands(OCF)  | Supported  | Comments(Macro's Defined in the source code)  | 
|---|---|---|
HCI_Reset  | Yes  | HCI_OP_RESET  | 
HCI_Set_Event_Filter  | Yes  | HCI_OP_SET_EVENT_FLT  | 
HCI_Flush  | Yes  | HCI_OP_FLUSH  | 
HCI_Read_PIN_Type  | Yes  | HCI_OP_READ_PIN_TYPE  | 
HCI_Write_PIN_Type  | Yes  | HCI_OP_WRITE_PIN_TYPE  | 
HCI_Create_New_Unit_Key  | Yes  | HCI_OP_CREATE_NEW_UNIT_KEY  | 
HCI_Read_Stored_Link_Key  | Yes  | HCI_OP_READ_STORED_LINK_KEY  | 
HCI_Write_Stored_Link_Key  | Yes  | HCI_OP_WRITE_STORED_LINK_KEY  | 
HCI_Delete_Stored_Link_Key  | Yes  | HCI_OP_DELETE_STORED_LINK_KEY  | 
HCI_Read_Local_Name  | Yes  | HCI_OP_READ_LOCAL_NAME  | 
HCI_Write_Local_Name  | Yes  | HCI_OP_WRITE_LOCAL_NAME  | 
HCI_Read_Connection_Accept_Timeout  | Yes  | HCI_OP_READ_CA_TIMEOUT  | 
HCI_Write_Connection_Accept_Timeout  | Yes  | HCI_OP_WRITE_CA_TIMEOUT  | 
HCI_Read_Page_Timeout  | Yes  | HCI_OP_READ_PAGE_TIMEOUT  | 
HCI_Write_Page_Timeout  | yes  | HCI_OP_WRITE_PAGE_TIMEOUT  | 
HCI_Read_Scan_Enable  | yes  | HCI_OP_READ_SCAN_ENABLE  | 
HCI_Write_Scan_Enable  | yes  | HCI_OP_WRITE_SCAN_ENABLE  | 
HCI_Read_Page_Scan_Activity  | Yes  | HCI_OP_READ_PAGE_SCAN_ACTIVITY  | 
HCI_Write_Page_Scan_Activity  | Yes  | HCI_OP_WRITE_PAGE_SCAN_ACTIVITY  | 
HCI_Read_Inquiry_Scan_Activity  | Yes  | HCI_OP_READ_INQUIRY_SCAN_ACTIVITY  | 
HCI_Write_Inquiry_Scan_Activity  | Yes  | HCI_OP_WRITE_INQUIRY_SCAN_ACTIVITY  | 
HCI_Read_Authentication_Enable  | Yes  | HCI_OP_READ_AUTH_ENABLE  | 
HCI_Write_Authentication_Enable  | Yes  | HCI_OP_WRITE_AUTH_ENABLE  | 
HCI_Read_Class_of_Device  | Yes  | HCI_OP_READ_CLASS_OF_DEVICE  | 
HCI_Write_Class_of_Device  | Yes  | HCI_OP_WRITE_CLASS_OF_DEVICE  | 
HCI_Read_Voice_Setting  | Yes  | HCI_OP_READ_VOICE_SETTING  | 
HCI_Write_Voice_Setting  | Yes  | HCI_OP_WRITE_VOICE_SETTING  | 
HCI_Read_Automatic_Flush_Timeout  | Yes  | HCI_OP_READ_AUTO_FLUSH_TOUT  | 
HCI_Write_Automatic_Flush_Timeout  | Yes  | HCI_OP_WRITE_AUTO_FLUSH_TOUT  | 
HCI_OP_READ_NUM_BROADCAST_RETRY  | NO  | |
HCI_OP_WRITE_NUM_BROADCAST_RETRY  | NO  | |
HCI_Read_Hold_Mode_Activity  | NO  | HCI_OP_READ_HOLD_MODE_ACTIVITY → Not defined in the code  | 
HCI_Write_Hold_Mode_Activity  | No  | |
HCI_Read_Transmit_Power_Level  | Yes  | HCI_OP_READ_TX_PWR_LEVEL  | 
HCI_Read_Synchronous_Flow_Control_Enable  | No  | HCI_OP_READ_SYNCHRONOUS_FLOW_CTRL_EN  | 
HCI_Write_Synchronous_Flow_Control_Enable  | No  | |
HCI_Set_Controller_To_Host_Flow_Control  | No  | HCI_OP_SET_CNTRLER_TO_HOST_FLOW_CTRL  | 
HCI_Host_Buffer_Size  | Yes  | HCI_OP_HOST_BUFFER_SIZE  | 
HCI_Host_Number_Of_Completed_Packets  | No  | HCI_OP_HOST_NUM_COMPLETED_PKTS  | 
HCI_Read_Link_Supervision_Timeout  | Yes  | HCI_OP_READ_LINK_SUPERVISION_TOUT  | 
HCI_Write_Link_Supervision_Timeout  | Yes  | HCI_OP_WRITE_LINK_SUPERVISION_TOUT  | 
HCI_Read_Number_Of_Supported_IAC  | Yes  | HCI_OP_READ_NUM_SUPPORTED_IAC  | 
Set_AFH_Host_Channel_Classification  | Yes  | HCI_OP_SET_AFH_HOST_CH_CLASSIFICATION  | 
HCI_Read_Inquiry_Scan_Type  | Yes  | HCI_OP_READ_INQUIRY_SCAN_TYPE  | 
HCI_Write_Inquiry_Scan_Type  | Yes  | HCI_OP_WRITE_INQUIRY_SCAN_TYPE  | 
HCI_Read_Inquiry_Mode  | Yes  | HCI_OP_READ_INQUIRY_MODE  | 
HCI_Write_Inquiry_Mode  | Yes  | HCI_OP_WRITE_INQUIRY_MODE  | 
HCI_Read_Page_Scan_Type  | Yes  | HCI_OP_READ_PAGE_SCAN_TYPE  | 
HCI_Write_Page_Scan_Type  | Yes  | HCI_OP_WRITE_PAGE_SCAN_TYPE  | 
Read_AFH_Channel_Assessment_Mode  | Yes  | HCI_OP_READ_AFH_CH_ASSESSMENT_MODE  | 
Write_AFH_Channel_Assessment_Mode  | Yes  | HCI_OP_WRITE_AFH_CH_ASSESSMENT_MODE  | 
HCI_Read_Extended_Inquiry_Response  | Yes  | HCI_OP_READ_EXT_INQUIRY_RESP  | 
HCI_Write_Extended_Inquiry_Response  | Yes  | HCI_OP_WRITE_EXT_INQUIRY_RESP  | 
HCI_Refresh_Encryption_Key  | yes  | HCI_OP_REFRESH_ENCRYPTION_KEY  | 
HCI_Read_Simple_Pairing_Mode  | Yes  | HCI_OP_READ_SIMPLE_PAIRING_MODE  | 
HCI_Write_Simple_Pairing_Mode  | Yes  | HCI_OP_WRITE_SIMPLE_PAIRING_MODE  | 
HCI_Read_Local_OOB_Data  | Yes  | HCI_OP_READ_LOCAL_OOB_DATA  | 
HCI_Read_Inquiry_Response_Transmit_Power_Leve  | Yes  | HCI_OP_READ_INQUIRY_RESP_TX_PWR_LEVEL  | 
HCI_Write_Inquiry_Transmit_Power_Level  | Yes  | HCI_OP_WRITE_INQUIRY_RESP_TX_PWR_LEVEL  | 
HCI_Send_Keypress_Notification  | Yes  | HCI_OP_SEND_KEY_PRESS_NOTIFICATION  | 
HCI_Read_Default_Erroneous_Data_Reporting  | NO  | HCI_OP_READ_DEF_ERRONEOUS_DATA_REP  | 
HCI_Write_Default_Erroneous_Data_Reporting  | No  | HCI_OP_WRITE_DEF_ERRONEOUS_DATA_REP  | 
HCI_Enhanced_Flush  | Yes  | HCI_OP_ENHANCED_FLUSH  | 
HCI_Read_Logical_Link_Accept_Timeout  | No  | HCI_OP_READ_LOGICAL_LINK_ACCEPT_TOUT  | 
HCI_Write_Logical_Link _Accept_Timeout  | No  | HCI_OP_WRITE_LOGICAL_LINK_ACCEPT_TOUT  | 
HCI_Set_Event_Mask_Page_2  | Yes  | HCI_OP_SET_EVENT_MASK_PAGE_2  | 
HCI_Read_Location_Data  | No  | HCI_OP_READ_LOCATION_DATA  | 
HCI_Write_Location_Data  | No  | HCI_OP_WRITE_LOCATION_DATA  | 
HCI_Read_Flow_Control_Mode  | ||
HCI_Write_Flow_Control_Mode  | ||
HCI_Read_Enhanced_Transmit_Power_Level  | Yes  | HCI_OP_READ_ENHANCED_TX_PWR_LEVEL  | 
HCI_Read_Best_Effort_Flush_Timeout  | No  | HCI_OP_READ_BE_FLUSH_TOUT  | 
HCI_Write_Best_Effort_Flush_Timeout  | No  | HCI_OP_WRITE_BE_FLUSH_TOUT  | 
HCI_Short_Range_Mode  | No  | HCI_OP_SHORT_RANGE_MODE  | 
HCI_Read_LE_Host_Support  | No  | HCI_OP_READ_LE_HOST_SUPPORT  | 
HCI_Write_LE_Host_Support  | No  | HCI_OP_WRITE_LE_HOST_SUPPORT  | 
HCI_Set_MWS_Channel_Parameters  | No  | |
HCI_ Set_ External_Frame_Configuration  | No  | |
HCI_Set_MWS_Transport_Layer  | No  | |
HCI_Set_MWS_Scan_Frequency_Table  | No  | |
HCI_Set_MWS_PATTERN_Configuration  | No  | |
HCI_Set_Reserved_LT_ADDR  | No  | |
HCI_Read_Local_Version_Information  | No  | |
HCI_Read_Local_Supported_Commands  | No  | |
HCI_Read_Local_Supported_Features  | No  | |
HCI_Read_Local_Extended_Features  | No  | |
HCI_Read_Buffer_Size  | No  | |
HCI_Read_BD_ADDR  | No  | |
HCI_Read_Data_Block_Size  | No  | |
HCI_Read_Local_Supported_Codecs  | No  | 
For OGF 0x05#
HCI Commands(OCF)  | Supported  | Comments(Macro's Defined in the source code)  | 
|---|---|---|
HCI_Read_Failed_Contact_Counter  | Yes  | HCI_OP_READ_FAILED_CONTACT_COUNTER  | 
HCI_Reset_Failed_Contact_Counter  | Yes  | HCI_OP_RESET_FAILED_CONTACT_COUNTER  | 
HCI_Read_Link_Quality 0  | Yes  | HCI_OP_READ_LINK_QUALITY  | 
HCI_Read_RSSI  | Yes  | HCI_OP_READ_RSSI  | 
HCI_Read_AFH_Channel_Map  | Yes  | HCI_OP_READ_AFH_CH_MAP  | 
HCI_Read_Clock  | Yes  | HCI_OP_READ_CLK  | 
HCI_Read_Encryption_Key_Size  | Yes  | HCI_OP_READ_ENCRYPTION_KEY_SIZE  | 
HCI_Read_Local_AMP_Info  | No  | HCI_OP_READ_LOCAL_AMP_INFO  | 
HCI_Write_Local_AMP_Info  | No  | |
HCI_Read_Local_AMP_ASSOC  | NO  | |
HCI_OP_READ_LOCAL_AMP_ASSOC  | ||
HCI_Write_Remote_AMP_ASSOC  | No  | HCI_OP_WRITE_REMOTE_AMP_ASSOC  | 
For OGF 0x06#
HCI Commands(OCF)  | Supported  | Comments(Macro's Defined in the source code)  | 
|---|---|---|
HCI_Read_Loopback_Mode  | No  | |
HCI_Write_Loopback_Mode  | No  | |
HCI_Enable_Device_Under_Test_Mode  | Yes  | HCI_OP_ENABLE_DEV_UNDER_TEST_MODE  | 
HCI_Write_Simple_Pairing_Debug_Mode  | Yes  | HCI_OP_WRITE_PAIRING_DBG_MODE  | 
HCI_Enable_AMP_Receiver_Reports  | No  | |
HCI_AMP_Test_End  | No  | |
HCI_AMP_Test  | No  | |
HCI_Write_Secure_Connections_Test_Mode  | No  |