Debug Prints#
You can enable debug prints (observed in dmesg) in the driver in the following two ways:
By assigning module param while installing the driver.
Through debugfs after installing the driver.
Both are explained below.
Assigning module param:
# insmod rsi_91x.ko rsi_zone_enabled=0x601In this case,
rsi_zone_enabledis a bitmap value which is explained below.Through debugfs:
# echo <value> > /sys/kernel/debug/phy<X>/debug_zone
rsi_zone_enabled and \<value\> are bitmap values as explained below.
BIT | ZONE |
|---|---|
BIT(0) | ERROR ZONE |
BIT(1) | INFO ZONE |
BIT(2) | INIT ZONE |
BIT(3) | MGMT TX ZONE |
BIT(4) | MGMT RX ZONE |
BIT(5) | DATA TX ZONE |
BIT(6) | DATA RX ZONE |
BIT(7) | FSM ZONE |
BIT(8) | ISR ZONE |
BIT(9) | INT MGMT ZONE |
BIT(10) | MGMT DEBUG ZONE |
For example, to enable both INFO ZONE and ERROR ZONE, set BIT(1) and BIT(0) to arrive at a bitmap value of 0x03.