Check the Software Version#
Run the following command to check the driver and LMAC version:
# cat /sys/kernel/debug/phy<X>/version
You can expect results similar to those below.
Driver : SiWT917.2.10.0.5 LMAC : 1711.2.10.0.0.5
Driver version :
Driver : SiWT917.w.x.y.z [Ex : SiWT917.2.10.0.5] where the naming convention is as follows: 'w' is Major version 'x' is Minor version 'y' is Patch number 'z' is Build number
LMAC Version :
LMAC : ab.w.x.y.c.z [Ex : 1711.2.10.0.0.5] where the naming convention is as follows: 'a' is CHIP ID 'b' is Rom Version (Reserved) 'w' is Major version 'x' is Minor version 'y' is Patch number 'c' is customer ID 'z' is Build number