Enabling Wireless Extension Tools#
Wireless Extension tools, such as 'iwconfig' and 'iwpriv' are required for configuring the driver. Make sure that the wireless extensions are enabled in the Linux kernel configuration file.
Enable these options in the kernel configuration file, re-compile the kernel, and cross compile the driver.
CONFIG_WIRELESS CONFIG_WIRELESS_EXT CONFIG_WEXT_PRIV CONFIG_WEXT_SPY CONFIG_WEXT_PROC CONFIG_WEXT_CORE CONFIG_HOSTAP
See the Kernel Configuration section for the commands to compile the kernel.