Get SDIO Stats#
Run the following command to get the SDIO-specific information, such as the number of interrupts or the buffer full status.
   # cat /sys/kernel/debug/phy<X>/sdio_statsYou can expect results similar to those below.
   total_sdio_interrupts: 1855
   sdio_msdu_pending_intr_count: 1890
   sdio_buff_full_count: 0
   sdio_buff_semi_full_count: 0
   sdio_unknown_intr_count: 0
   BUFFER FULL STATUS : 0
   SEMI BUFFER FULL STATUS : 0
   MGMT BUFFER FULL STATUS : 0
   BUFFER FULL COUNTER : 0
   BUFFER SEMI FULL COUNTER : 0
   MGMT BUFFER FULL COUNTER : 0