Get Wi-Fi Station Stats#
Run the following command to check the driver status, management packet stats, and data packet stats:
# cat /sys/kernel/debug/phy<X>/statsYou can expect results similar to those below.
   ==> RSI STA DRIVER STATUS <==
   DRIVER_FSM_STATE: (9)
   total_mgmt_pkt_send :        114        total_mgmt_pkt_queued :         0          total_mgmt_pkt_freed :         0
   total_data_vo_pkt_send:        4        total_data_vo_pkt_queued:         0          total_data_vo_pkt_freed:        4
   total_data_vi_pkt_send:        0        total_data_vi_pkt_queued:         0          total_data_vi_pkt_freed:        0
   total_data_be_pkt_send:        230      total_data_be_pkt_queued:         0          total_data_be_pkt_freed:        230
   total_data_bk_pkt_send:        0        total_data_bk_pkt_queued:         0          total_data_bk_pkt_freed:        0 In this case, the value of DRIVER_FSM_STATE is shown in the table below:
DRIVER_FSM_STATE  | Value  | 
|---|---|
FSM_FW_NOT_LOADED  | 0  | 
FSM_CARD_NOT_READY  | 1  | 
FSM_COMMON_DEV_PARAMS_SENT  | 2  | 
FSM_BOOT_PARAMS_SENT  | 3  | 
FSM_EEPROM_READ_MAC_ADDR  | 4  | 
FSM_EEPROM_READ_RF_TYPE  | 5  | 
FSM_RESET_MAC_SENT  | 6  | 
FSM_RADIO_CAPS_SENT  | 7  | 
FSM_BB_RF_PROG_SENT  | 8  | 
FSM_MAC_INIT_DONE  | 9  |