Functional Description SiWT917_EB4346B with Raspberry Pi 4 Platform#

Setup DiagramSetup Diagram

In the figure above, the user needs to connect the SiWT917 RCP module to a Raspberry Pi 4 running Raspberry Pi 4 OS through the Raspberry Pi connector (40 PIN header) . The Raspberry Pi should have a kernel version installed between 3.18 to 6.12. To evaluate concurrent mode, an external third-party AP and STA are needed.

Use Cases#

  • We can use this feature in devices that need wireless third-party access point for internet access and need an admin interface to control and configure the services provided by it.

  • Create a bridge/hub with internet access to provide internet access to multiple IoT devices like a Wi-Fi extender.