Public Attributes#

uint8_t

remote device address

uint8_t

attribute handle

uint8_t

attribute value offset

uint16_t

length of attribute value

uint8_t

This contains the attribute value.

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_prepare_write_resp_s::dev_addr[RSI_DEV_ADDR_LEN]

remote device address


handle#

uint8_t rsi_ble_prepare_write_resp_s::handle[2]

attribute handle


offset#

uint8_t rsi_ble_prepare_write_resp_s::offset[2]

attribute value offset


length#

uint16_t rsi_ble_prepare_write_resp_s::length

length of attribute value


att_value#

uint8_t rsi_ble_prepare_write_resp_s::att_value[RSI_DEV_ATT_LEN]

This contains the attribute value.

The maximum value is 240, please refer RSI_DEV_ATT_LEN Macro