Monitor Mode#
Functions#
sl_status_t
sl_wifi_enable_monitor_mode(sl_wifi_interface_t interface)
Enable monitor (promiscuous) mode on the Wi-Fi device.
sl_status_t
sl_wifi_disable_monitor_mode(sl_wifi_interface_t interface)
Disable monitor mode on the Wi-Fi interface.
Function Documentation#
sl_wifi_enable_monitor_mode#
sl_status_t sl_wifi_enable_monitor_mode (sl_wifi_interface_t interface)
Enable monitor (promiscuous) mode on the Wi-Fi device.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_interface_t | [in] | interface | Wi-Fi interface as identified by sl_wifi_interface_t |
In this mode, all types of Wi-Fi frames will be forwarded to the host. Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
Note
This API is not yet implemented.
sl_wifi_disable_monitor_mode#
sl_status_t sl_wifi_disable_monitor_mode (sl_wifi_interface_t interface)
Disable monitor mode on the Wi-Fi interface.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_interface_t | [in] | interface | Wi-Fi interface as identified by sl_wifi_interface_t |
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
Note
This API is not yet implemented.