Client#
Functions#
Connect to the given Wi-Fi AP.
Disconnect the Wi-Fi client interface.
Get current Wi-Fi client's signal strength (RSSI).
Set the Wi-Fi roaming configuration.
Get the Wi-Fi roaming configuration.
Verify the Wi-Fi client configuration is valid and available.
Load the certificate into the device.
Load the certificate into the device.
Set the advanced configuration options of a client interface.
Function Documentation#
sl_wifi_connect#
sl_status_t sl_wifi_connect (sl_wifi_interface_t interface, const sl_wifi_client_configuration_t * access_point, uint32_t timeout_ms)
Connect to the given Wi-Fi AP.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_interface_t | [in] | interface | Wi-Fi client interface as identified by sl_wifi_interface_t |
| const sl_wifi_client_configuration_t * | [in] | access_point | sl_wifi_client_configuration_t object that contains the details of Access Point. |
| uint32_t | [in] | timeout_ms | Timeout value in milliseconds. The function will abort and return when the timeout timer expires. A value of 0 indicates an asynchronous action. TBD: asynchronous action page. |
sl_wifi_init should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
Note
If channel, band, and BSSID are provided, this API will attempt to connect without scanning.
sl_wifi_disconnect#
sl_status_t sl_wifi_disconnect (sl_wifi_interface_t interface)
Disconnect the Wi-Fi client interface.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_interface_t | [in] | interface | Wi-Fi client interface as identified by sl_wifi_interface_t |
sl_wifi_connect should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
sl_wifi_get_signal_strength#
sl_status_t sl_wifi_get_signal_strength (sl_wifi_interface_t interface, int32_t * rssi)
Get current Wi-Fi client's signal strength (RSSI).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_interface_t | [in] | interface | Wi-Fi interface as identified by sl_wifi_interface_t |
| int32_t * | [in] | rssi | signal strength (RSSI) in dBm. |
sl_wifi_connect should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
sl_wifi_set_roam_configuration#
sl_status_t sl_wifi_set_roam_configuration (sl_wifi_interface_t interface, sl_wifi_roam_configuration_t * roam_configuration)
Set the Wi-Fi roaming configuration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_interface_t | [in] | interface | Wi-Fi interface as identified by sl_wifi_interface_t |
| sl_wifi_roam_configuration_t * | [in] | roam_configuration | sl_wifi_roam_configuration_t object to store Wi-Fi roaming configuration. |
sl_wifi_set_advanced_scan_configuration should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
Note
For si91x chips, following ranges are valid: trigger_level: [-10, -100] , trigger_level_change: [0, 90]
sl_wifi_get_roam_configuration#
sl_status_t sl_wifi_get_roam_configuration (sl_wifi_interface_t interface, sl_wifi_roam_configuration_t * roam_configuration)
Get the Wi-Fi roaming configuration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_interface_t | [in] | interface | Wi-Fi interface as identified by sl_wifi_interface_t |
| sl_wifi_roam_configuration_t * | [out] | roam_configuration | @sl_wifi_roam_configuration_t object that will contain the current roam configuration. |
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
Note
This API is not yet implemented.
sl_wifi_test_client_configuration#
sl_status_t sl_wifi_test_client_configuration (sl_wifi_interface_t interface, const sl_wifi_client_configuration_t * ap, uint32_t timeout_ms)
Verify the Wi-Fi client configuration is valid and available.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_interface_t | [in] | interface | Wi-Fi interface as identified by sl_wifi_interface_t |
| const sl_wifi_client_configuration_t * | [in] | ap | sl_wifi_client_configuration_t object that contains the details of Access Point. |
| uint32_t | [in] | timeout_ms | Timeout value in milliseconds. The function will abort and return when the timeout timer expires. A value of 0 indicates an asynchronous action. |
sl_wifi_init should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
sl_wifi_set_certificate#
sl_status_t sl_wifi_set_certificate (uint8_t certificate_type, const uint8_t * buffer, uint32_t certificate_length)
Load the certificate into the device.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | certificate_type | Certificate type being set |
| const uint8_t * | [in] | buffer | Pointer to buffer containing the certificate. |
| uint32_t | [in] | certificate_length | Length of certificate buffer data. |
sl_wifi_init should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
sl_wifi_set_certificate_with_index#
sl_status_t sl_wifi_set_certificate_with_index (uint8_t certificate_type, uint8_t certificate_index, uint8_t * buffer, uint32_t certificate_length)
Load the certificate into the device.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | certificate_type | Certificate type being set. |
| uint8_t | [in] | certificate_index | Certificate to be loaded in specified index. |
| uint8_t * | [in] | buffer | Pointer to buffer containing the certificate. |
| uint32_t | [in] | certificate_length | Length of certificate buffer data. |
sl_wifi_init should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
sl_wifi_set_advanced_client_configuration#
sl_status_t sl_wifi_set_advanced_client_configuration (sl_wifi_interface_t interface, const sl_wifi_advanced_client_configuration_t * configuration)
Set the advanced configuration options of a client interface.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_interface_t | [in] | interface | Wi-Fi interface as identified by sl_wifi_interface_t |
| const sl_wifi_advanced_client_configuration_t * | [in] | configuration | Wi-Fi client advanced configuration. See sl_wifi_advanced_client_configuration_t |
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.