Scanning#

Functions#

sl_status_t
sl_wifi_start_scan(sl_wifi_interface_t interface, const sl_wifi_ssid_t *optional_ssid, const sl_wifi_scan_configuration_t *configuration)

Start scanning for Wi-Fi networks.

sl_status_t
sl_wifi_stop_scan(sl_wifi_interface_t interface)

Stop Wi-Fi scan.

sl_status_t
sl_wifi_set_advanced_scan_configuration(const sl_wifi_advanced_scan_configuration_t *configuration)

Set advanced scan configuration.

sl_status_t
sl_wifi_get_advanced_scan_configuration(sl_wifi_advanced_scan_configuration_t *configuration)

Get advanced scan configuration.

sl_status_t
sl_wifi_wait_for_scan_results(sl_wifi_scan_result_t **scan_result_array, uint32_t max_scan_result_count)

Wait for current scan to complete and stores the results in the provided array.

Function Documentation#

sl_wifi_start_scan#

sl_status_t sl_wifi_start_scan (sl_wifi_interface_t interface, const sl_wifi_ssid_t * optional_ssid, const sl_wifi_scan_configuration_t * configuration)

Start scanning for Wi-Fi networks.

Parameters
[in]interface

Wi-Fi interface as identified by sl_wifi_interface_t

[in]optional_ssid

Optional SSID of type sl_wifi_ssid_t can be used to scan for a particular Wi-Fi network

[in]configuration

sl_wifi_scan_configuration_t

Returns

Note

  • For 911x, Advanced scan results are not populated to user.


Definition at line 378 of file components/protocol/wifi/inc/sl_wifi.h

sl_wifi_stop_scan#

sl_status_t sl_wifi_stop_scan (sl_wifi_interface_t interface)

Stop Wi-Fi scan.

Parameters
[in]interface

Wi-Fi interface as identified by sl_wifi_interface_t

Returns

Note

  • For 911x, sl_wifi_stop_scan is ONLY supported for advanced scan


Definition at line 394 of file components/protocol/wifi/inc/sl_wifi.h

sl_wifi_set_advanced_scan_configuration#

sl_status_t sl_wifi_set_advanced_scan_configuration (const sl_wifi_advanced_scan_configuration_t * configuration)

Set advanced scan configuration.

Parameters
[in]configuration

Set advanced scan configuration as identified by sl_wifi_advanced_scan_configuration_t

Returns


Definition at line 406 of file components/protocol/wifi/inc/sl_wifi.h

sl_wifi_get_advanced_scan_configuration#

sl_status_t sl_wifi_get_advanced_scan_configuration (sl_wifi_advanced_scan_configuration_t * configuration)

Get advanced scan configuration.

Parameters
[out]configuration

sl_wifi_advanced_scan_configuration_t object that will contain the current advanced scan configuration.

Returns


Definition at line 418 of file components/protocol/wifi/inc/sl_wifi.h

sl_wifi_wait_for_scan_results#

sl_status_t sl_wifi_wait_for_scan_results (sl_wifi_scan_result_t ** scan_result_array, uint32_t max_scan_result_count)

Wait for current scan to complete and stores the results in the provided array.

Parameters
[in]scan_result_array

Array of sl_wifi_scan_result_t objects to store the scan results.

[in]max_scan_result_count

The maximum number of scan result objects that can fit in the scan result array.

  • This function also returns when the scan result array is full.

  • Once the scan result array is full, any further scan results will be lost.

Returns

Note

  • This API is not supported in the current release.


Definition at line 436 of file components/protocol/wifi/inc/sl_wifi.h