Application Components#
WiSeConnectâ„¢ SDK v3.x has revamped the component organization such that almost none of the v2.x components remain in v3.x.
The following sections provide a list of v3.x components.
The component category path is listed for each component, specifying how to navigate to the component in the SOFTWARE COMPONENTS tab of Simplicity Studio. Components are listed in alphabetical order of the component category path.


BLE#
Component Name | Component Category Path |
|---|---|
BLE Core | BLE |
Wi-Fi#
Component Name | Component Category Path |
|---|---|
Wi-Fi resources | Resources |
Si91x Support Library | Wi-Fi |
Wi-Fi Core | Wi-Fi |
Network Management#
Component Name | Component Category Path |
|---|---|
Network Manager | Networking > Core |
Basic Data Manager | Networking > Data Management |
NVM3 Data Manager | Networking > Data Management |
BSD Sockets | Networking > Sockets |
Si91x Driver#
Component Name | Component Category Path |
|---|---|
Si91x Core | Devices > Si91x |
Si91x Driver | Devices > Si91x |
Si91x SoC | Devices > Si91x |
Basic buffers | Devices > Si91x > Memory |
Hosted LwIP Network Stack | Devices > Si91x > Networking |
Network Offload | Devices > Si91x > Networking |
Si91x Platform#
Component Name | Component Category Path |
|---|---|
BRD4325A | Platform > Board > Radio Board |
BRD4325B | Platform > Board > Radio Board |
BRD4325C | Platform > Board > Radio Board |
BRD4325G | Platform > Board > Radio Board |
si917_memory_default_config | Platform > Board > si91x > core |
SL CALENDAR | Platform > Board > si91x > Drivers |
SL CONFIG TIMER | Platform > Board > si91x > Drivers |
SL DMA | Platform > Board > si91x > Drivers |
SL GPIO | Platform > Board > si91x > Drivers |
SL GSPI | Platform > Board > si91x > Drivers |
SL I2C | Platform > Board > si91x > Drivers |
SL IOSTREAM USART | Platform > Board > si91x > Drivers |
SL SIO | Platform > Board > si91x > Drivers |
SL SSI | Platform > Board > si91x > Drivers |
SL ULP | Platform > Board > si91x > Drivers |
SL USART | Platform > Board > si91x > Drivers |
SL WDT | Platform > Board > si91x > Drivers |
ULP Timer Instance | Platform > Board > si91x > Drivers |
Toolchain for ARM | Platform > Board > si91x > Toolchain |
Memory LCD with 917's SPI driver | Platform > si91x > core |
Protocols and Services#
Component Name | Component Category Path |
|---|---|
HTTP Client Library | Networking > Protocol |
MQTT Client Library | Networking > Protocol |
SNTP Client Library | Networking > Protocol |
AWS IoT Library | Third Party |