Public Attributes#

uint8_t
uint8_t

uint8_t, Advertising SID subfield in the ADI field used to identify the Periodic Advertising.

uint8_t

uint8_t, Advertiser Address Type, this parameter indicates the type of address being used in the connection request packets

uint8_t

uint8_t, Advertiser Address[6]

uint16_t

uint16_t, Skip,The maximum number of periodic advertising events that can be skipped after a successful receive Range : 0x0000 to 0x01F3

uint16_t

uint16_t, Sync Timeout, Synchronization timeout for the periodic advertising train Range : 0x000A to 0x4000

uint8_t

Public Attribute Documentation#

fil_policy#

uint8_t rsi_ble_ae_set_periodic_adv_create_sync_s::fil_policy

adv_sid#

uint8_t rsi_ble_ae_set_periodic_adv_create_sync_s::adv_sid

uint8_t, Advertising SID subfield in the ADI field used to identify the Periodic Advertising.

Range : 0x00 to 0x0F, All other bits - Reserved for future use


adv_addr_type#

uint8_t rsi_ble_ae_set_periodic_adv_create_sync_s::adv_addr_type

uint8_t, Advertiser Address Type, this parameter indicates the type of address being used in the connection request packets

      0x00          Public Device Address or Public Identity Address
      0x01          Random Device Address or Random (static) Identity Address

All other values Reserved for future use


adv_addr#

uint8_t rsi_ble_ae_set_periodic_adv_create_sync_s::adv_addr[RSI_DEV_ADDR_LEN]

uint8_t, Advertiser Address[6]


skip#

uint16_t rsi_ble_ae_set_periodic_adv_create_sync_s::skip

uint16_t, Skip,The maximum number of periodic advertising events that can be skipped after a successful receive Range : 0x0000 to 0x01F3


sync_timeout#

uint16_t rsi_ble_ae_set_periodic_adv_create_sync_s::sync_timeout

uint16_t, Sync Timeout, Synchronization timeout for the periodic advertising train Range : 0x000A to 0x4000


reserved#

uint8_t rsi_ble_ae_set_periodic_adv_create_sync_s::reserved