Public Attributes#

uint8_t

address of remote device

uint8_t

Device input output capability 0x00 - Display Only 0x01 - Display Yes/No 0x02 - Keyboard Only 0x03 - No Input No Output 0x04 - Keyboard Display.

uint8_t

Out Of the Band data.

uint8_t

Authentication Request contains bonding type MITM Request - BIT(2) Secure Connections - BIT(3) Keypress - BIT(4) CT2 - BIT(5)

uint8_t

Minimum required key size.

uint8_t

Initiator generates/requires the no .of keys after successful paring BIT(0) - EncKey: Initiator distributes the LTK followed by EDIV and Rand BIT(1) - IdKey : Initiator distributes the IRK followed by its address BIT(2) - Sign : Initiator distributes the CSRK BIT(3) - BIT(7): Reserved for future use.

uint8_t

Responder generates/requires the no .of keys after successful paring BIT(0) - EncKey: Responder distributes the LTK followed by EDIV and Rand BIT(1) - IdKey : Responder distributes the IRK followed by its address BIT(2) - Sign : Responder distributes the CSRK BIT(3) - BIT(7): Reserved for future use.

Public Attribute Documentation#

dev_addr#

uint8_t rsi_bt_event_smp_resp_s::dev_addr[6]

address of remote device


io_cap#

uint8_t rsi_bt_event_smp_resp_s::io_cap

Device input output capability 0x00 - Display Only 0x01 - Display Yes/No 0x02 - Keyboard Only 0x03 - No Input No Output 0x04 - Keyboard Display.


oob_data#

uint8_t rsi_bt_event_smp_resp_s::oob_data

Out Of the Band data.


auth_req#

uint8_t rsi_bt_event_smp_resp_s::auth_req

Authentication Request contains bonding type MITM Request - BIT(2) Secure Connections - BIT(3) Keypress - BIT(4) CT2 - BIT(5)


min_req_key_size#

uint8_t rsi_bt_event_smp_resp_s::min_req_key_size

Minimum required key size.


ini_key_distrb#

uint8_t rsi_bt_event_smp_resp_s::ini_key_distrb

Initiator generates/requires the no .of keys after successful paring BIT(0) - EncKey: Initiator distributes the LTK followed by EDIV and Rand BIT(1) - IdKey : Initiator distributes the IRK followed by its address BIT(2) - Sign : Initiator distributes the CSRK BIT(3) - BIT(7): Reserved for future use.


resp_key_distrb#

uint8_t rsi_bt_event_smp_resp_s::resp_key_distrb

Responder generates/requires the no .of keys after successful paring BIT(0) - EncKey: Responder distributes the LTK followed by EDIV and Rand BIT(1) - IdKey : Responder distributes the IRK followed by its address BIT(2) - Sign : Responder distributes the CSRK BIT(3) - BIT(7): Reserved for future use.