Public Attributes#

uint8_t

uint8_t, enable, If this parameter is set Periodic Advertising starts 0 - Enable Periodic Advertising 1 - Include the ADI field in AUX_SYNC_IND PDUs

uint8_t

uint8_t, Advertising Handle, Used to identify an advertising set Range : 0x00 to 0xEF

Public Attribute Documentation#

enable#

uint8_t ae_periodic_adv_enable::enable

uint8_t, enable, If this parameter is set Periodic Advertising starts 0 - Enable Periodic Advertising 1 - Include the ADI field in AUX_SYNC_IND PDUs


adv_handle#

uint8_t ae_periodic_adv_enable::adv_handle

uint8_t, Advertising Handle, Used to identify an advertising set Range : 0x00 to 0xEF