Public Attributes#

uint8_t

uint8_t AE_ADV_DATA_TYPE 1, AE_PERIODIC_ADV_DATA_TYPE 2, AE_SCAN_RSP_DATA_TYPE 3

uint8_t

uint8_t Advertising Handle, used to identify an Advertising set, Ranges from 0x00 to 0xEF

uint8_t

uint8_t Operation 0x00 - Intermediate fragment of fragmented extended advertising data 0x01 - First fragment of fragmented extended advertising data 0x02 - Last fragment of fragmented extended advertising data 0x03 - Complete extended advertising data 0x04 - Unchanged data (just update the Advertising DID)

uint8_t

uint8_t Fragment_Preference, Specifies the controller on where to fragment the Host advertising Data 0x00 - The Controller may fragment all Host advertising data 0x01 - The Controller should not fragment or should minimize fragmentation of Host advertising data

uint8_t

uint8_t Data Length, Specifies Advertising_Data_Length , This parameter ranges from 0 to 251

uint8_t

uint8_t Data ,Specifies Advertising_Data.

Public Attribute Documentation#

type#

uint8_t rsi_ble_ae_data_s::type

uint8_t AE_ADV_DATA_TYPE 1, AE_PERIODIC_ADV_DATA_TYPE 2, AE_SCAN_RSP_DATA_TYPE 3


Definition at line 1261 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

adv_handle#

uint8_t rsi_ble_ae_data_s::adv_handle

uint8_t Advertising Handle, used to identify an Advertising set, Ranges from 0x00 to 0xEF


Definition at line 1263 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

operation#

uint8_t rsi_ble_ae_data_s::operation

uint8_t Operation 0x00 - Intermediate fragment of fragmented extended advertising data 0x01 - First fragment of fragmented extended advertising data 0x02 - Last fragment of fragmented extended advertising data 0x03 - Complete extended advertising data 0x04 - Unchanged data (just update the Advertising DID)


Definition at line 1271 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

frag_pref#

uint8_t rsi_ble_ae_data_s::frag_pref

uint8_t Fragment_Preference, Specifies the controller on where to fragment the Host advertising Data 0x00 - The Controller may fragment all Host advertising data 0x01 - The Controller should not fragment or should minimize fragmentation of Host advertising data


Definition at line 1277 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

data_len#

uint8_t rsi_ble_ae_data_s::data_len

uint8_t Data Length, Specifies Advertising_Data_Length , This parameter ranges from 0 to 251


Definition at line 1279 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

data#

uint8_t rsi_ble_ae_data_s::data[0xC8]

uint8_t Data ,Specifies Advertising_Data.


Definition at line 1281 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h