Network Interface#
Functions#
Initialize a network interface.
De-initialize a network interface.
Bring a network interface up.
Bring a network interface down.
Resolve given host name to IP address.
Function Documentation#
sl_net_init#
sl_status_t sl_net_init (sl_net_interface_t interface, const void * configuration, void * network_context, sl_net_event_handler_t event_handler)
Initialize a network interface.
Type | Direction | Argument Name | Description | ||||||
---|---|---|---|---|---|---|---|---|---|
sl_net_interface_t | [in] | interface | Interface identified by sl_net_interface_t | ||||||
const void * | [in] | configuration | Configuration object specific to network interface of type sl_wifi_device_configuration_t. If configuration = NULL, then following configuration is used internally by SDK
| ||||||
void * | [in] | network_context | Runtime context specific to network interface. | ||||||
sl_net_event_handler_t | [in] | event_handler | Processes all network events related to network interface as identified by sl_net_event_handler_t |
This API should be called before calling any sl_net API. Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.4
Note
For Wi-Fi events, sl_net uses the wifi callback framework. Register the corresponding Wi-Fi event handlers using sl_wifi_set_callback API.
Parameter
network_context
is only being used when module is acting as station in external stack mode[lwIP]. In such case,network_context
is supposed to refer a valid sl_net_wifi_lwip_context_t variable.
sl_net_deinit#
sl_status_t sl_net_deinit (sl_net_interface_t interface)
De-initialize a network interface.
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_net_interface_t | [in] | interface | Interface identified by sl_net_interface_t |
Pre-conditions:
sl_net_init should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
sl_net_up#
sl_status_t sl_net_up (sl_net_interface_t interface, sl_net_profile_id_t profile_id)
Bring a network interface up.
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_net_interface_t | [in] | interface | Interface identified by sl_net_interface_t |
sl_net_profile_id_t | [in] | profile_id | Network profile identifier for specific interface of type sl_net_profile_id_t |
Pre-conditions:
sl_net_init should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
Note
By default, profile and credential configurations in sl_net_defaults.h are used by SDK. User can define their profile and credential configurations for an interface, by calling sl_net_set_profile and sl_net_set_credentials APIs before calling sl_net_up API".
sl_net_down#
sl_status_t sl_net_down (sl_net_interface_t interface)
Bring a network interface down.
Type | Direction | Argument Name | Description |
---|---|---|---|
sl_net_interface_t | [in] | interface | Interface identified by sl_net_interface_t |
Pre-conditions:
sl_net_up should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
sl_net_host_get_by_name#
sl_status_t sl_net_host_get_by_name (const char * host_name, const uint32_t timeout, const sl_net_dns_resolution_ip_type_t dns_resolution_ip, sl_ip_address_t * ip_address)
Resolve given host name to IP address.
Type | Direction | Argument Name | Description |
---|---|---|---|
const char * | [in] | host_name | Host name which needs to be resolved. |
const uint32_t | [in] | timeout | timeout in millisecs. |
const sl_net_dns_resolution_ip_type_t | [in] | dns_resolution_ip | DNS resolution by IP of type sl_net_dns_resolution_ip_type_t |
sl_ip_address_t * | [out] | ip_address | IP address object to store resolved IP address of type sl_ip_address_t |
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
Note
If timeout value is greater than zero, caller would be blocked till timeout milliseconds to get the response. If the values is equal's to zero, response would sent through sl_net_event_handler_t.