Network Credential#
Functions#
Set a network credential including client credentials, certificates, and keys.
Retrieve a stored network credential.
Delete a stored network credential.
Function Documentation#
sl_net_set_credential#
sl_status_t sl_net_set_credential (sl_net_credential_id_t id, sl_net_credential_type_t type, const void * credential, uint32_t credential_length)
Set a network credential including client credentials, certificates, and keys.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_net_credential_id_t | [in] | id | Network credential identifier as identified by sl_net_credential_id_t |
| sl_net_credential_type_t | [in] | type | Network credential type as identified by sl_net_credential_type_t |
| const void * | [in] | credential | Pointer to the credential data object. |
| uint32_t | [in] | credential_length | Length of the credential data object. |
Pre-conditions:
sl_net_init should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
sl_net_get_credential#
sl_status_t sl_net_get_credential (sl_net_credential_id_t id, sl_net_credential_type_t * type, void * credential, uint32_t * credential_length)
Retrieve a stored network credential.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_net_credential_id_t | [in] | id | Network credential identifier as identified by sl_net_credential_id_t |
| sl_net_credential_type_t * | [out] | type | Network credential type as identified by sl_net_credential_type_t |
| void * | [out] | credential | Pointer to location where credential data is stored. |
| uint32_t * | [inout] | credential_length | in: Number of bytes available at credential, out: Number of bytes written. |
Pre-conditions:
sl_net_init should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
sl_net_delete_credential#
sl_status_t sl_net_delete_credential (sl_net_credential_id_t id, sl_net_credential_type_t type)
Delete a stored network credential.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_net_credential_id_t | [in] | id | Network credential identifier as identified by sl_net_credential_id_t |
| sl_net_credential_type_t | [out] | type | Network credential type as identified by sl_net_credential_type_t |
Pre-conditions:
sl_net_init should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.