Structure to hold the parameters of clock calibration, trigger time macros can be used to fill trigger time.

Public Attributes#

boolean_t

true to enable and false to disable rc calibration

boolean_t

true to enable and false to disable rc periodic calibration

uint8_t

rc trigger time, 5 sec, 10 sec, 15 sec, 30 sec, 1 min, 2 min

boolean_t

true to enable and false to disable ro calibration

boolean_t

true to enable and false to disable periodic calibration

uint8_t

ro trigger time, 1 sec, 2 sec, 4 sec, 8 sec

Public Attribute Documentation#

rc_enable_calibration#

boolean_t clock_calibration_config_t::rc_enable_calibration

true to enable and false to disable rc calibration


Definition at line 83 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_calendar.h

rc_enable_periodic_calibration#

boolean_t clock_calibration_config_t::rc_enable_periodic_calibration

true to enable and false to disable rc periodic calibration


Definition at line 84 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_calendar.h

rc_trigger_time#

uint8_t clock_calibration_config_t::rc_trigger_time

rc trigger time, 5 sec, 10 sec, 15 sec, 30 sec, 1 min, 2 min


Definition at line 85 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_calendar.h

ro_enable_calibration#

boolean_t clock_calibration_config_t::ro_enable_calibration

true to enable and false to disable ro calibration


Definition at line 86 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_calendar.h

ro_enable_periodic_calibration#

boolean_t clock_calibration_config_t::ro_enable_periodic_calibration

true to enable and false to disable periodic calibration


Definition at line 87 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_calendar.h

ro_trigger_time#

uint8_t clock_calibration_config_t::ro_trigger_time

ro trigger time, 1 sec, 2 sec, 4 sec, 8 sec


Definition at line 88 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_calendar.h