Structure to hold port and pin of sio spi.

Public Attributes#

uint8_t

SIO SPI CS port.

uint8_t

SIO SPI CS pin.

uint8_t

SIO SPI CS mux.

uint8_t

SIO SPI CS pad.

uint8_t

SIO SPI CLK port.

uint8_t

SIO SPI CLK pin.

uint8_t

SIO SPI CLK mux.

uint8_t

SIO SPI CLK pad.

uint8_t

SIO SPI MOSI port.

uint8_t

SIO SPI MOSI pin.

uint8_t

SIO SPI MOSI mux.

uint8_t

SIO SPI MOSI pad.

uint8_t

SIO SPI MISO port.

uint8_t

SIO SPI MISO pin.

uint8_t

SIO SPI MISO mux.

uint8_t

SIO SPI MISO pad.

Public Attribute Documentation#

spi_cs_port#

uint8_t sl_sio_spi_t::spi_cs_port

SIO SPI CS port.


Definition at line 145 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

spi_cs_pin#

uint8_t sl_sio_spi_t::spi_cs_pin

SIO SPI CS pin.


Definition at line 146 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

spi_cs_mux#

uint8_t sl_sio_spi_t::spi_cs_mux

SIO SPI CS mux.


Definition at line 147 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

spi_cs_pad#

uint8_t sl_sio_spi_t::spi_cs_pad

SIO SPI CS pad.


Definition at line 148 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

spi_clk_port#

uint8_t sl_sio_spi_t::spi_clk_port

SIO SPI CLK port.


Definition at line 149 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

spi_clk_pin#

uint8_t sl_sio_spi_t::spi_clk_pin

SIO SPI CLK pin.


Definition at line 150 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

spi_clk_mux#

uint8_t sl_sio_spi_t::spi_clk_mux

SIO SPI CLK mux.


Definition at line 151 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

spi_clk_pad#

uint8_t sl_sio_spi_t::spi_clk_pad

SIO SPI CLK pad.


Definition at line 152 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

spi_mosi_port#

uint8_t sl_sio_spi_t::spi_mosi_port

SIO SPI MOSI port.


Definition at line 153 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

spi_mosi_pin#

uint8_t sl_sio_spi_t::spi_mosi_pin

SIO SPI MOSI pin.


Definition at line 154 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

spi_mosi_mux#

uint8_t sl_sio_spi_t::spi_mosi_mux

SIO SPI MOSI mux.


Definition at line 155 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

spi_mosi_pad#

uint8_t sl_sio_spi_t::spi_mosi_pad

SIO SPI MOSI pad.


Definition at line 156 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

spi_miso_port#

uint8_t sl_sio_spi_t::spi_miso_port

SIO SPI MISO port.


Definition at line 157 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

spi_miso_pin#

uint8_t sl_sio_spi_t::spi_miso_pin

SIO SPI MISO pin.


Definition at line 158 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

spi_miso_mux#

uint8_t sl_sio_spi_t::spi_miso_mux

SIO SPI MISO mux.


Definition at line 159 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

spi_miso_pad#

uint8_t sl_sio_spi_t::spi_miso_pad

SIO SPI MISO pad.


Definition at line 160 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h