typedef for SSI clock config struct

Public Attributes#

uint16_t

Clock Division Factor.

uint16_t

intf PLL control value

uint32_t

intf PLL clock frequency

uint32_t

intf PLL reference clock frequency

uint32_t

SoC PLL Clock frequency.

uint32_t

SoC PLL reference clock frequency.

uint8_t

SoC PLL count value.

Public Attribute Documentation#

division_factor#

uint16_t sl_ssi_clock_config_t::division_factor

Clock Division Factor.


Definition at line 108 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ssi.h

intf_pll_500_control_value#

uint16_t sl_ssi_clock_config_t::intf_pll_500_control_value

intf PLL control value


Definition at line 109 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ssi.h

intf_pll_clock#

uint32_t sl_ssi_clock_config_t::intf_pll_clock

intf PLL clock frequency


Definition at line 110 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ssi.h

intf_pll_reference_clock#

uint32_t sl_ssi_clock_config_t::intf_pll_reference_clock

intf PLL reference clock frequency


Definition at line 111 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ssi.h

soc_pll_clock#

uint32_t sl_ssi_clock_config_t::soc_pll_clock

SoC PLL Clock frequency.


Definition at line 112 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ssi.h

soc_pll_reference_clock#

uint32_t sl_ssi_clock_config_t::soc_pll_reference_clock

SoC PLL reference clock frequency.


Definition at line 113 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ssi.h

soc_pll_mm_count_value#

uint8_t sl_ssi_clock_config_t::soc_pll_mm_count_value

SoC PLL count value.


Definition at line 114 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ssi.h