Structure to hold the parameters of sysrtc clock-source configurations.

Public Attributes#

uint8_t

input clock sources \refsl_clock_sources_t

uint32_t

clock division factor

Public Attribute Documentation#

clock_source#

uint8_t sl_sysrtc_clock_config_t::clock_source

input clock sources \refsl_clock_sources_t


Definition at line 85 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sysrtc.h

division_factor#

uint32_t sl_sysrtc_clock_config_t::division_factor

clock division factor


Definition at line 86 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sysrtc.h