Getting Started with the WiSeConnect™ SDK v3.x#
To get started with using the WiSeConnect™ SDK v3.x, download the latest version of Simplicity Studio and select one of the getting started guides in this section:
System-on-chip (SoC) mode - both the application and connectivity stack run on the SiWx91x™ chipset.
To run the out-of-the-box demo, see the Starting with SoC Mode section.
To set up software and hardware, create a project, configure and compile an application, and run an application, see the Developing for SiWx91x Host section.
Network co-processor (NCP) mode - application runs on external microcontroller unit (MCU) host, connectivity stack runs on the SiWx91x chipset. See the Starting with EFR32™ in NCP Mode section.
Note: If you are using an external MCU host other than EFR32, stay tuned. We will publish more guides soon.
Matter Quick-Start Guides provide steps to set up your first example application using the Matter protocol: