Functions#
This section provides a reference to the SHA Crypto API functions.
Functions#
sl_status_t
sl_si91x_sha(uint8_t sha_mode, uint8_t *msg, uint16_t msg_length, uint8_t *digest)
Decide whether the SHA message can be sent once or requires multiple calls to send.
Function Documentation#
sl_si91x_sha#
sl_status_t sl_si91x_sha (uint8_t sha_mode, uint8_t * msg, uint16_t msg_length, uint8_t * digest)
Decide whether the SHA message can be sent once or requires multiple calls to send.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | sha_mode |
|
| uint8_t * | [in] | msg | - Pointer to message |
| uint16_t | [in] | msg_length | - Total message length |
| uint8_t * | [out] | digest | - Output parameter to hold computed digest from SHA |
This is a blocking API. Returns
The following values are returned:
0 - Success
Non-Zero Value - Failure
Note
Refer Error Codes section for above error codes error-codes.