Functions#
This section provides a reference to the TRNG Crypto API functions.
Functions#
This API Initializes the TRNG hardware engine.
This API checks the Entropy of TRNG and verifies TRNG functioning.
This API initializes and programs the key required for TRNG hardware engine.
This API generates random number of desired length.
This API checks if there are any repeating elements in the Array.
Function Documentation#
sl_si91x_trng_init#
sl_status_t sl_si91x_trng_init (sl_si91x_trng_config_t * config, uint32_t * output)
This API Initializes the TRNG hardware engine.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_si91x_trng_config_t * | [in] | config | Configuration object of type sl_si91x_trng_config_t |
| uint32_t * | [out] | output | Buffer to store the output. |
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
sl_si91x_trng_entropy#
sl_status_t sl_si91x_trng_entropy (void )
This API checks the Entropy of TRNG and verifies TRNG functioning.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
sl_si91x_trng_program_key#
sl_status_t sl_si91x_trng_program_key (uint32_t * trng_key, uint16_t key_length)
This API initializes and programs the key required for TRNG hardware engine.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t * | [in] | trng_key | - Pointer to trng_key |
| uint16_t | [in] | key_length | - key_length - key length in Dwords (uint32_t) |
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
sl_si91x_trng_get_random_num#
sl_status_t sl_si91x_trng_get_random_num (uint32_t * random_number, uint16_t length)
This API generates random number of desired length.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t * | [in] | random_number | - Address for Random number |
| uint16_t | [in] | length | - length of random number in bytes |
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
sl_si91x_duplicate_element#
sl_status_t sl_si91x_duplicate_element (uint32_t * dword, uint32_t length_in_dwords)
This API checks if there are any repeating elements in the Array.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t * | [in] | dword | |
| uint32_t | [in] | length_in_dwords | of the Array |
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.