Types#
This section provides a reference to the MQTT API data types.
Modules#
sl_mqtt_client_last_will_message_t
sl_mqtt_client_configuration_t
sl_mqtt_client_topic_subscription_info_t
Typedefs#
Handler for MQTT client Events.
Handler for MQTT client RX message.
Typedef Documentation#
sl_mqtt_client_event_handler_t#
sl_mqtt_client_event_handler_t )(void *client, sl_mqtt_client_event_t event, void *event_data, void *context)
Handler for MQTT client Events.
N/A | client | Client on which the event occurred. |
N/A | event | Event occurred of type sl_mqtt_client_event_t |
N/A | event_data | Event data for the data. This parameter would be non-null only for MQTT_CLIENT_MESSAGED_RECEIVED and MQTT_CLIENT_ERROR. |
N/A | context | Context provided by user at the time of API call. The caller must ensure that the lifecycle of the context is retained until the callback is invoked. The deallocation of context is also the responsibility of the caller. |
169
of file components/service/mqtt/inc/sl_mqtt_client_types.h
sl_mqtt_client_message_received_t#
sl_mqtt_client_message_received_t )(void *client, sl_mqtt_client_message_t *message_to_be_published, void *context)
Handler for MQTT client RX message.
N/A | client | Client which has received message. |
N/A | message_to_be_published | Message received of type sl_mqtt_client_message_t |
N/A | context | Context provided by user at the time of Subscribe API call. The caller must ensure that the lifecycle of the context is retained until the callback is invoked. The deallocation of context is also the responsibility of the caller. |
Note
Due to the constraints from the firmware, is_retained, qos_level, packet_identifier, duplicate_message of sl_mqtt_client_message_t are not populated and shall be ignored while processing the message.
187
of file components/service/mqtt/inc/sl_mqtt_client_types.h