MQTT Client Topic Subscription Info structure.
Public Attributes#
sl_slist_node_t
Next node in the linked list.
A function pointer to message handler.
Quality of subscription.
uint16_t
Length of the subscribed topic. Length should not exceed 202 bytes including NULL termination character.
uint8_t
A flexible array to store the topic.
Public Attribute Documentation#
next_subscription#
sl_slist_node_t sl_mqtt_client_topic_subscription_info_t::next_subscription
Next node in the linked list.
Definition at line
193
of file components/service/mqtt/inc/sl_mqtt_client_types.h
topic_message_handler#
sl_mqtt_client_message_received_t sl_mqtt_client_topic_subscription_info_t::topic_message_handler
A function pointer to message handler.
Definition at line
194
of file components/service/mqtt/inc/sl_mqtt_client_types.h
qos_of_subscription#
sl_mqtt_qos_t sl_mqtt_client_topic_subscription_info_t::qos_of_subscription
Quality of subscription.
Definition at line
195
of file components/service/mqtt/inc/sl_mqtt_client_types.h
topic_length#
uint16_t sl_mqtt_client_topic_subscription_info_t::topic_length
Length of the subscribed topic. Length should not exceed 202 bytes including NULL termination character.
Definition at line
197
of file components/service/mqtt/inc/sl_mqtt_client_types.h
topic#
uint8_t sl_mqtt_client_topic_subscription_info_t::topic[]
A flexible array to store the topic.
Definition at line
198
of file components/service/mqtt/inc/sl_mqtt_client_types.h