Wi-Fi Access Point configuration.

Public Attributes#

Optional flags for AP configuration.

ID of secure credentials.

uint8_t

Keep alive type of the access point. One of the values from sl_si91x_ap_keepalive_type_t

uint16_t

Beacon interval of the access point in milliseconds.

uint32_t

Duration in milliseconds to kick idle client.

uint16_t

How many beacons per DTIM.

uint8_t

Maximum number of associated clients.

uint8_t

Stop beaconing when there are no associated clients.

To enable Transition Disable Indication (TDI). One of the values from sl_wifi_tdi_t.

uint8_t

A flag to enable 11n.

Public Attribute Documentation#

ssid#

sl_wifi_ssid_t sl_wifi_ap_configuration_t::ssid

SSID.


Definition at line 154 of file components/protocol/wifi/inc/sl_wifi_types.h

security#

sl_wifi_security_t sl_wifi_ap_configuration_t::security

Security mode.


Definition at line 155 of file components/protocol/wifi/inc/sl_wifi_types.h

encryption#

sl_wifi_encryption_t sl_wifi_ap_configuration_t::encryption

Encryption mode.


Definition at line 156 of file components/protocol/wifi/inc/sl_wifi_types.h

channel#

sl_wifi_channel_t sl_wifi_ap_configuration_t::channel

Channel.


Definition at line 157 of file components/protocol/wifi/inc/sl_wifi_types.h

rate_protocol#

sl_wifi_rate_protocol_t sl_wifi_ap_configuration_t::rate_protocol

Rate protocol.


Definition at line 158 of file components/protocol/wifi/inc/sl_wifi_types.h

options#

sl_wifi_ap_flag_t sl_wifi_ap_configuration_t::options

Optional flags for AP configuration.


Definition at line 159 of file components/protocol/wifi/inc/sl_wifi_types.h

credential_id#

sl_wifi_credential_id_t sl_wifi_ap_configuration_t::credential_id

ID of secure credentials.


Definition at line 160 of file components/protocol/wifi/inc/sl_wifi_types.h

keepalive_type#

uint8_t sl_wifi_ap_configuration_t::keepalive_type

Keep alive type of the access point. One of the values from sl_si91x_ap_keepalive_type_t


Definition at line 162 of file components/protocol/wifi/inc/sl_wifi_types.h

beacon_interval#

uint16_t sl_wifi_ap_configuration_t::beacon_interval

Beacon interval of the access point in milliseconds.


Definition at line 163 of file components/protocol/wifi/inc/sl_wifi_types.h

client_idle_timeout#

uint32_t sl_wifi_ap_configuration_t::client_idle_timeout

Duration in milliseconds to kick idle client.


Definition at line 164 of file components/protocol/wifi/inc/sl_wifi_types.h

dtim_beacon_count#

uint16_t sl_wifi_ap_configuration_t::dtim_beacon_count

How many beacons per DTIM.


Definition at line 165 of file components/protocol/wifi/inc/sl_wifi_types.h

maximum_clients#

uint8_t sl_wifi_ap_configuration_t::maximum_clients

Maximum number of associated clients.


Definition at line 166 of file components/protocol/wifi/inc/sl_wifi_types.h

beacon_stop#

uint8_t sl_wifi_ap_configuration_t::beacon_stop

Stop beaconing when there are no associated clients.


Definition at line 167 of file components/protocol/wifi/inc/sl_wifi_types.h

tdi_flags#

sl_wifi_tdi_t sl_wifi_ap_configuration_t::tdi_flags

To enable Transition Disable Indication (TDI). One of the values from sl_wifi_tdi_t.


Definition at line 168 of file components/protocol/wifi/inc/sl_wifi_types.h

is_11n_enabled#

uint8_t sl_wifi_ap_configuration_t::is_11n_enabled

A flag to enable 11n.


Definition at line 169 of file components/protocol/wifi/inc/sl_wifi_types.h