Wi-Fi max transmit power.
Public Attributes#
uint8_t
Transmit power during scan. Valid input range: 1dBm to 31dBm.
uint8_t
Transmit power during join. Valid input range: 1dBm to 31dBm.
Public Attribute Documentation#
scan_tx_power#
uint8_t sl_wifi_max_tx_power_t::scan_tx_power
Transmit power during scan. Valid input range: 1dBm to 31dBm.
Definition at line
398
of file components/protocol/wifi/inc/sl_wifi_types.h
join_tx_power#
uint8_t sl_wifi_max_tx_power_t::join_tx_power
Transmit power during join. Valid input range: 1dBm to 31dBm.
Definition at line
399
of file components/protocol/wifi/inc/sl_wifi_types.h