HTTP server request URI parameters.

Public Attributes#

char *

URI path.

uint16_t

Number of query parametrs received in uri.

Public Attribute Documentation#

path#

char* sl_http_server_request_uri_t::path

URI path.


Definition at line 168 of file components/service/sl_http_server/inc/sl_http_server_types.h

query_parameters#

sl_http_server_uri_query_parameter_t sl_http_server_request_uri_t::query_parameters[MAX_QUERY_PARAMETERS]

Array of query parameters.


Definition at line 169 of file components/service/sl_http_server/inc/sl_http_server_types.h

query_parameter_count#

uint16_t sl_http_server_request_uri_t::query_parameter_count

Number of query parametrs received in uri.


Definition at line 170 of file components/service/sl_http_server/inc/sl_http_server_types.h