Wi-Fi performance profile.
Public Attributes#
Performance profile of type sl_si91x_performance_profile_t.
Set DTIM alignment required. DTIM Alignment Types.
Default value to be used is 0.
Listen interval.
Monitor interval will be in millisecs, Default interval 50 milli secs is used if monitor_interval is set to 0. This is only valid when performance profile is set to ASSOCIATED_POWER_SAVE_LOW_LATENCY.
twt request.
twt selection request
Public Attribute Documentation#
profile#
sl_si91x_performance_profile_t sl_wifi_performance_profile_t::profile
Performance profile of type sl_si91x_performance_profile_t.
974
of file components/device/silabs/si91x/wireless/inc/sl_wifi_device.h
dtim_aligned_type#
uint8_t sl_wifi_performance_profile_t::dtim_aligned_type
Set DTIM alignment required. DTIM Alignment Types.
975
of file components/device/silabs/si91x/wireless/inc/sl_wifi_device.h
num_of_dtim_skip#
uint8_t sl_wifi_performance_profile_t::num_of_dtim_skip
Default value to be used is 0.
976
of file components/device/silabs/si91x/wireless/inc/sl_wifi_device.h
listen_interval#
uint16_t sl_wifi_performance_profile_t::listen_interval
Listen interval.
977
of file components/device/silabs/si91x/wireless/inc/sl_wifi_device.h
monitor_interval#
uint16_t sl_wifi_performance_profile_t::monitor_interval
Monitor interval will be in millisecs, Default interval 50 milli secs is used if monitor_interval is set to 0. This is only valid when performance profile is set to ASSOCIATED_POWER_SAVE_LOW_LATENCY.
979
of file components/device/silabs/si91x/wireless/inc/sl_wifi_device.h
twt_request#
sl_wifi_twt_request_t sl_wifi_performance_profile_t::twt_request
twt request.
980
of file components/device/silabs/si91x/wireless/inc/sl_wifi_device.h
twt_selection#
sl_wifi_twt_selection_t sl_wifi_performance_profile_t::twt_selection
twt selection request
981
of file components/device/silabs/si91x/wireless/inc/sl_wifi_device.h