Functions#
This section provides a reference to Wi-Fi API functions:
Common functions to initialize and configure Wi-Fi features.
Radio functions to configure the Wi-Fi radio.
Scanning functions to scan for Wi-Fi Access Points (APs) in the local area network (LAN).
Client functions to implement a Wi-Fi client, otherwise known as a station (STA).
Access Point functions to implement a Wi-FI Access Point (AP).
Power and Performance functions to configure Wi-Fi connectivity performance.
Wi-Fi Protected Setup functions to implement Wi-Fi Protected Setup (WPS).
Debugging functions for debugging the Wi-Fi APIs.